Wireless LAN (WLAN) Access Point

Overview

NXP® Wireless LAN Access Point block diagram

NXP<sup>&#174;</sup> Wireless LAN Access Point block diagram

Community Demo

ZigBee/Wi-Fi Connectivity Gateway for the Smart Home

(00:56min)

In brief, the Android application running in the tablet connects via Wi-Fi to the gateway, which translates every command to both ZigBee HA 1.2 and TCP/IP networks, thus enabling any Wi-Fi enabled device to control several devices even if using different communication protocols.

See more demos at the nxp.community >