IR controller module implements functions to command different TVs using an infrared transmitter. IR Controller Driver uses CMT to modulate the IR signal. Timing parameters and controller command codes are defined using the structures on IR Controller Parameters.
Modules | |
| IR Controller Parameters | |
| IR Controller Driver | |
Files | |
| file | controller_parameter_list.h |
| file | ir_controller.h |