Freescale SemiconductorMSE9S12XEQ512_3M25J
Mask Set ErrataRev. April 16, 2012



MC9S12XEQ512, Mask 3M25J


Introduction
This errata sheet applies to the following devices:

MC9S12XEQ512, MC9S12XEQ384, MC9S12XEG384, MC9S12XES384



MCU Device Mask Set Identification

The mask set is identified by a 5-character code consisting of a version number, a letter, two numerical digits, and a letter, for example 1K79X. All standard devices are marked with a mask set number and a date code.



MCU Device Date Codes

Device markings indicate the week of manufacture and the mask set used. The date is coded as four numerical digits where the first two digits indicate the year and the last two digits indicate the work week. For instance, the date code "0201" indicates the first week of the year 2002.



MCU Device Part Number Prefixes

Some MCU samples and devices are marked with an SC, PC, or XC prefix. An SC prefix denotes special/custom device. A PC prefix indicates a prototype device which has undergone basic testing only. An XC prefix denotes that the device is tested but is not fully characterized or qualified over the full range of normal manufacturing process variations. After full characterization and qualification, devices will be marked with the MC or SC prefix.



Errata System Tracking Numbers

MUCtsXXXXX is the tracking number for device errata. It can be used with the mask set and date code to identify a specific erratum.



Errata Summary


Errata NumberModule affectedBrief DescriptionWork-
around
MUCts03731 s12x_dbg DBG: State flags and counter corrupted by simultaneous arm and disarm YES
MUCts03868 s12_cpu_xe CPU: Breakpoint missed at simultaneous taghits YES
MUCts03934 s12x_bdm BDM: Incomplete Memory Access on misaligned access due to BDM features YES
MUCts03977 pwm_8b8c PWM: Emergency shutdown input can be overruled YES
MUCts04083 pim_xe_q512 PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetch YES
MUCts04104 ect_16b8c ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1 YES
MUCts04135 pwm_8b8c PWM: Wrong output level after shutdown restart in 16bit concatenated channel mode YES
MUCts04136 pwm_8b8c PWM: Wrong output value after restart from stop or wait mode YES
MUCts04156 ect_16b8c ECT_16B8C: Output compare pulse is inaccurate YES
MUCts04177 s12xe_crg s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instruction YES
MUCts04244 sci SCI: RXEDGIF occurs more times than expected in IR mode YES



DBG: State flags and counter corrupted by simultaneous arm and disarmMUCts03731

Description

Simultaneous disarming (hardware) and arming (software) results in 

status, flag and counter register (DBGSR, DBGMFR, DBGCNT) corruption.

Hardware disarming initiated by an internal trigger or by tracing
completion takes 2 clock cycles. If a write to DBGC1 with the ARM bit
set occurs in the final clock cycle of this disarming process, arming
is suppressed but the DBGSR register is initialized to state1 and
DBGMFR/DBGCNT are initialized to zero.

The result is that the DBG module is disarmed by hardware but DBGSR
indicates state1.

NOTE: DBGC1 is typically only written to whilst armed to set the TRIG
bit or update the COMRV bits to map different registers to the address
map window.

Generally during debugging, after arming the DBG module and returning
to application code a further write access of DBGC1 over the BDM
interface requires considerable time relative to application code
execution, therefore in many cases the breakpoint may be reached before
a DBGC1 update is attempted. Furthermore the probability of hitting the
same cycle is seen to be very low.


Workaround


If the fault condition is caused by writing to DBGC1 to set the TRIG 

bit (to request an immediate breakpoint), then the application code may
be rerun again without the attempted setting of TRIG. The software
trigger (TRIG) is unnecessary in any case at the same point point in
time as an internal hardware trigger occurs.

Development tool vendors should avoid COMRV updates while the DBG is
armed.

Users that observe the problem due to development tool COMRV updates
can add a NOP to code and rerun to shift the disarm cycle, thereby
preventing a collision with the COMRV updates.



CPU: Breakpoint missed at simultaneous taghitsMUCts03868

Description

The CPU execution priority encoder evaluates taghits and then 

generates a breakpoint if a taghit must lead to an immediate
breakpoint as determined by the DBG module.

If the DBG module indicates that this taghit leads to an immediate
breakpoint then the CPU loads the execution stage with SWI or BGND thus
generating the breakpoint.

At simultaneous taghits the lowest channel has priority.
If taghits on 2 channels simultaneously, whereby the lower channel tag
must be ignored, but the higher channel tag must cause a breakpoint,
then the breakpoint request is erroneously missed.
Thus if channel[1:0] taghits occur simultaneously whereby channel[0]
must be ignored but channel[1] must cause a breakpoint, then the
breakpoint request on channel[1] is erroneously missed and no
breakpoint generated.

The DBG module recognises the taghit and the state sequencer
transitions accordingly. Furthermore the taghit causes the DBG module
to request a forced breakpoint, which means that a late CPU breakpoint
occurs. If the tagged instruction is a single cycle instruction, the
breakpoint occurs at the second instruction following the tagged
instruction.
Otherwise the breakpoint occurs at the instruction immediately
following the tagged instruction.

This bug requires that separate tags are placed on the same
instruction. This is not a typical case when using exact tag addresses.
It is more relevant in debugging environments using range modes, where
tags may cover a whole range. In this case a tagged range may cover a
tag or another tagged range, making simultaneous taghits possible.

This is a debugging issue only.

Workaround


Do not attach multiple tags to the same exact address. 

When attaching multiple tags to the same address by overlapping tag
ranges in range modes, or covering a tag with a tag range in range
modes, then the missed tag can be avoided by mapping the final state
change to the lower channel number.

For example the case
Channel[0] tags a range; channel[3] tags an instruction within that
range.
From DBG State1 Taghit[0] leads to State2. (DBGSCR1=$6)
From DBG State2 Taghit[3] leads to FinalState.(DBGSCR2=$5)
In State2 a simultaneous Taghit[3,0] scenario would miss the breakpoint.

This can be avoided by using the alternative DBG configuration
Channel[2] tags a range; channel[0] tags an instruction within that
range.
From DBG State1 Taghit[2] leads to State2. (DBGSCR1=$3)
From DBG State2 Taghit[0] leads to FinalState.(DBGSCR2=$7)



BDM: Incomplete Memory Access on misaligned access due to BDM featuresMUCts03934

Description

If a misaligned word write access is directly followed by an attempted

entry into active BDM, then the second byte access may be performed on a
different target due to the memory map switching for BDM active.

Depending on the type of access this can lead to the following situations...
1. When writing in the address range from $7F_FEFF to $7F_FFFD in the
external space the MMC splits the accesses into two 8-bit accesses. It
is able to complete the first access, but just before the second access
the BDM firmware becomes mapped into this address location and the
second byte access goes to the firmware.
This can only occur if the last cycle of the access instruction is a
word write to an odd address AND the instruction is followed by BGND or
a tagged breakpoint.

This can only occur on devices featuring an External Bus Interface.

2. On a misaligned word write with a global store (GSTD,GSTS,GSTX,GSTY)
in the address range $XX_0FFF to $XX_3FFD, the first split access is
performed correctly in the external space, but in the second byte cycle
the MMC is instructed to interpret the address coming from the CPU as a
local address, which is the internal RAM. Since accesses to the RAM are
not split, the MMC enters an inconsistent state and never acknowledges
the CPU access. This causes the CPU flow to cease.
This can only occur if the CPU executes a global store instruction which
writes to an odd address in the last instruction cycle AND the
instruction is followed by BGND or a tagged breakpoint.

This can only occur on devices featuring an External Bus Interface.

3. Generally on a misaligned global store (GSTD,GSTS,GSTX,GSTY) the
lower 16-bits of the global address are interpreted as a local address
for the second byte access. This can result result in unintended
accesses to registers or external RAM.







Workaround


Do not set breakpoints or insert BGND after a GSTD.


Remove all instances of BGND from code when not debugging.








PWM: Emergency shutdown input can be overruledMUCts03977

Description

If the PWM emergency shutdown feature is enabled (PWM7ENA=1) and PWM

channel 7 is disabled (PWME7=0) another lower priority function
available on the related pin can take control over the data direction.
This does not lead to a problem if input mode is maintained. If the
alternative function switches to output mode the shutdown function may
unintentionally be triggered by the output data.


Workaround


When using the PWM emergency shutdown feature the GPIO function on the

pin associated with PWM channel 7 should be selected as an input.

In the case that this pin is selected as an output or where an
alternative function is enabled which could drive it as an output,
enable PWM channel 7 by setting the PWME7 bit. This prevents an
active shutdown level driven on the (output) pin from resulting in an
emergency shutdown of the enabled PWM channels.




PIM: Edge-sensitive mode of IRQ-pin may cause incorrect interrupt vector fetchMUCts04083

Description

Where the IRQ interrupt is being used in edge-sensitive mode and a 

lower priority interrupt is already pending when an IRQ edge event
occurs, if the IRQ edge event occurs inside a very narrow (<3ns) window
just as the pending interrupt vector is being fetched, then a different
vector other than that relating to either the pending interrupt or IRQ
will be taken.

In the case that a programmed interrupt vector is fetched both the
originally pending interrupt and the IRQ interrupt request will remain
pending and will be serviced once the erroneously called service
routine has completed (and RTI has been executed).

In the case that the incorrect vector fetch is from an unprogrammed
vector table entry (i.e. erased state = 0xFFFF) then erroneous
execution from the start of the register space will occur most often
resulting in an illegal memory access reset, COP reset or Unimplemented
Instruction Trap occurring.

In the less likely case that one of the three reset vectors is
incorrectly fetched then execution will jump to the appropriate reset
code.

The following vectors are not affected will not cause erroneous
behavior if pending:
$F0 - RTI
$F6 - SWI
$E2 – ECT channel 6
$B2 – CAN0 Rx
$72 – XGATE software trigger 0

This issue is limited to the edge-sensitive mode of the IRQ input only -
applications not using IRQ interrupts or configured for level-
sensitive IRQ input are not affected.

There is no issue where a pending interrupt has higher priority than
the IRQ request.

Workaround


Where using IRQ in edge-sensitive mode then configure the interrupt 

priority levels of all interrupts being used to ensure that the IRQ
request always has the lowest priority.

For new designs, where possible use the IRQ input in level-sensitive
mode or alternatively use a key-interrupt port.

There are a number of ‘best practices’ and features of the S12X which
can help minimize the impact of this errata in the case of it occurring:

1) As ‘best practice’ initialize all unused and unimplemented/reserved
interrupt vector table locations to point to a dummy interrupt service
routine (terminated with an RTI).

2) Where possible, check for appropriate asserted flags in interrupt
service routines and return / flag a system error if no request flag is
set.

3) Support is provided on the MCU for managing the following system
conditions:
* COP watchdog reset
* Illegal access reset
* Unimplemented instruction trap
For ‘best practice’ the application's software should be written to
recover from any of these conditions in a controlled manner.

4) In the case of erroneous code execution jumping to unused Flash the
typical practice of filling all unused Flash and RAM space with the op-
code for the SWI instruction will help manage this. SWI exception
routine should be written in this case to manage this event.




ECT: Channel 0 - 3 Input Capture interrupts inhibited when BUFEN=1, LATQ=0 and NOVWx=1MUCts04104

Description

Channel 0 – 3 Input Capture interrupts are inhibited when BUFEN=1, 

LATQ=0 and NOVWx=1 if an Input Capture edge occurs during or between a
read of TCx and TCxH or between a read of TCx/TCxH and clearing of CxF.


Details:

When any of the buffered input capture channels 0 - 3 are configured
for buffered/queue mode (BUFEN=1, LATQ=0) each of the channel’s input
capture holding registers and each channel’s associated pulse
accumulator and its holding register are enabled. When the input
capture channel is enabled by writing to a channel’s EDGxB and EDGxA
bits, both the input capture and input capture holding register are
considered empty. The first valid edge received after enabling a
channel will latch the ECT’s free running counter into the input
capture register (TCx) without setting the channel’s associated CxF
interrupt flag. The second valid edge received will transfer the value
of the input capture register, TCx, into the channel’s TCxH holding
register, latch the current value of the free running timer into the
input capture register and set the channel’s associated CxF interrupt
flag. In this condition, both the TCx and TCxH registers are
considered ‘full’.

If a corresponding channel’s NOVWx bit in the ICOVW register is set,
the capture register or its holding register cannot be written by a
valid edge at the input pin unless they are first emptied by reading
the TCx and TCxH registers. The act of reading the TCx and TCxH
registers and clearing the channel’s associated CxF interrupt flag
involves three separate operations. Two 16-bit read operations and an 8-
bit write operation.

If a channel’s associated CxF interrupt flag is cleared before reading
the TCx and TCxH registers and if a valid input edge occurs during or
between the reading of the capture and holding register, a channel’s
associated CxF interrupt flag will no longer be set as the result of
valid input edges. For example:

Clear CxF
|
|
V
Read TCx <----+
| |
|<--------+--- Valid Input Edge Occurs
V |
Read TCxH <---+

If the TCx and TCxH registers are read before a channel’s associated
CxF interrupt flag is cleared and if a valid input edge occurs between
the reading of TCx/TCxH and the clearing of a channel’s associated CxF
interrupt flag, a channel’s associated CxF interrupt flag will no
longer be set as the result of valid input edges. For example:

Clear CxF
|
|
V
Read TCx
|
|<------------ Valid Input Edge Occurs
V
Read TCxH


Systems that service the interrupt request and read the TCx and TCxH
registers before the next valid edge occurs at a channel’s associated
input pin will avoid the conditions under which the errata will occur.

Workaround


A simple workaround exists for this errata:


1. Clear the input capture channel’s associated CxF bit.
2. Disable the input capture function by writing 0:0 to a channel’s
EDGxB and EDGxA bits.
3. Read TCx
4. Read TCxH
5. Re-enable the input capture function by writing to a channel’s EDGxB
and EDGxA bits.


Code Example:

unsigned char ICSave;
unsigned int TC0Val;
unsigned int TC0HVal;

ICSave = TCTL4 & 0x03; /* save state of EDG0B and EDG0A */
TFLG1 = 0x01; /* clear ECT Channel 0 flag */
TCTL4 &= 0xfc; /* disable Channel 0 input capture function */
TC0Val = TC0; /* Read value of TC0 */
TC0HVal = TC0H; /* Read value of TC0H */
TCTL4 |= ICSave; /* Restore Channel 0 input capture function */



PWM: Wrong output level after shutdown restart in 16bit concatenated channel modeMUCts04135

Description

When the PWM is used in 16-bit (concatenation) channel and the emergency

shutdown feature is being used, after de-asserting PWM channel 7
(note:PWMRSTRT should be set) the PWM channels do
not show the state which is set by PWMLVL bit when the 16-bit counter is
non-zero.




Workaround


If emergency shutdown mode is required:


In 16-bit concatenation mode, user can disable the related PWM
channels and set the corresponding general-purpose IO to be the PWM
LVL value. After a intend period, restart the PWM channels.





PWM: Wrong output value after restart from stop or wait modeMUCts04136

Description

In low power modes (P-STOP/STOP/WAIT mode) and during PWM7

de-assert and when PWM counter reaching 0, the PWM channel outputs
cannot keep the state which is set by PWMLVL bit.






Workaround


Before entering low power modes, user can disable the related PWM 

channels and set the corresponding general-purpose IO to be the PWM
LVL value. After a intend period, restart the PWM channels.








ECT_16B8C: Output compare pulse is inaccurateMUCts04156

Description

The pulse width of an output compare (which resets the free running

counter when TCRE = 1) will measure one more bus clock cycle than
expected.



Workaround


The specification has been updated. Please refer to revision V03.08 (04

May 2010) or later.

In description of bitfield TCRE in register TSCR2,a note has been added:
TCRE=1 and TC7!=0, the TCNT cycle period will be TC7 x "prescaler
counter width" + "1 Bus Clock". When TCRE is set and TC7 is not equal to
0, then TCNT will cycle from 0 to TC7. When TCNT reaches TC7 value, it
will last only one bus cycle then reset to 0.







s12xe_crg: Possible PLL premature LOCK followed by an UN-LOCK in conjunction with STOP instructionMUCts04177

Description

If the PLL is manually turned off (PLLCTL_ PLLON = 0) before a STOP

instruction and the PLL is manually turned on (PLLCTL_PLLON=1) after
execution of the STOP instruction, the PLL might have a premature lock
condition in the case of a STOP instruction being executed with a
pending interrupt and the corresponding interrupt is enabled. In this
case the STOP is executed similar to NOP instruction.

Due to the manual control of the PLL, the VCO clock is switched on and
off. The PLL lock detection logic uses the VCO clock as well as the
reference clock (based on the external oscillator). The external
oscillator is not stopped because the STOP instruction is executed like
a NOP instruction, which keeps the reference clock running.

This causes the logic in the PLL lock detection being uncorrelated and
thus resulting in a possible premature LOCK condition (CRGFLG_LOCK=1).

After the next lock detection cycle the lock is lost (CRGFLG_LOCK=0)
because the VCO clock frequency has not reached the correct value. Some
lock detection cycles later the correct lock condition is reached (VCO
clock frequency reached the correct value) and the LOCK bit is set again
(CRGFLG_LOCK=1). Each transition of the LOCK bit is indicated by the
lock interrupt flag (CRGFLG_LOCKIF).

Workaround


Do not modify the PLLON bit around the STOP instruction. 


The clock control and power down/up sequencing is automatically done by
the device CRG module. Only the system clock source selection after exit
from STOP must be controlled by software (CLKSEL_PLLSEL bit) as
described in the Reference Manual.

Depending on the application if the fast wake-up feature is used the
software also needs to control the bit FSTWKP and bit SCME (both located
in the PLLCTL register) as described in the device Reference Manual when
STOP Mode is entered or exited.






SCI: RXEDGIF occurs more times than expected in IR modeMUCts04244

Description

Configured for Infrared Receive mode, the SCI may incorrectly set the 

RXEDGIF bit if there are consecutive '00' data bits. There are two
cases:

Case 1: due to re-sync of the RXD input, the received edge may be
delayed by one bus cycle. If an edge (bit = '0') is detected near
an SCI clock edge, the next edge (bit = '0') may be detected one
SCI clock later than expected due to re-sync logic.

Case 2: if external baud is slower than SCI receiver, the next edge
may be detected later than expected.

This glitch can be detected by the RXEDGIF circuit, but it does not
impact the final data result because the SCI receive and data recovery
logic takes samples at RT8, RT9, and RT10.




Workaround


Case 1 and case 2 may occurs at same time. To avoid those unexpected 

RXEDGIF at IR mode, the external baud should be kept a little bit
faster than receiver baud by:
P > (1/16)/(SBR)
or
(P)(SBR)(16)> 1

Where SBR is baud of receiver, P is external baud faster ratio.
For example:
1.- When SBR = 16, P = 0.4%, this means the external baud should be at
least 0.4% faster than receiver.
2.- When SBR = 4, P = 1.6%, this means the external baud should be at
least 1.6% faster than receiver.

Case 1 will cover case 2, i.e. case 1 is the worst case. If case1 is
solved, case 2 is also solved.


© Freescale Semiconductor, Inc., 2012. All rights reserved.