=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "AS1"       (component AsynchroSerial)
   - AS1_RecvChar -If any data is received, this method returns one character, otherwise it returns an error code (it does not 
                wait for data). This method is enabled only if the receiver property is enabled.  [Note:] Because the preferred 
                method to handle error and break exception in the interrupt mode is to use events <OnError> and <OnBreak> the 
                return value ERR_RXEMPTY has higher priority than other error codes. As a consequence the information about an 
                exception in interrupt mode is returned only if there is a valid character ready to be read. [ Version specific 
                information for Freescale 56800 derivatives ]   DMA mode:  If DMA controller is available on the selected CPU 
                and the receiver is configured to use DMA controller then this method only sets the selected DMA channel. Then 
                the status of the DMA transfer can be checked using GetCharsInRxBuf method. See an example of a typical usage 
                for details about the communication using DMA.
   - AS1_SendChar -Sends one character to the channel. If the component is temporarily disabled (Disable method) SendChar 
                method only stores data into an output buffer. In case of a zero output buffer size, only one character can be 
                stored. Enabling the component (Enable method) starts the transmission of the stored data. This method is 
                available only if the transmitter property is enabled.  [ Version specific information for Freescale 56800 
                derivatives ]   DMA mode:  If DMA controller is available on the selected CPU and the transmitter is configured 
                to use DMA controller then this method only sets selected DMA channel. Then the status of the DMA transfer can 
                be checked using GetCharsInTxBuf method. See an example of a typical usage for details about communication 
                using DMA.
   - AS1_RecvBlock -If any data is received, this method returns the block of the data and its length (and incidental error), 
                otherwise it returns an error code (it does not wait for data).  This method is available only if non-zero 
                length of the input buffer is defined and the receiver property is enabled.  If less than requested number of 
                characters is received only the available data is copied from the receive buffer to the user specified 
                destination. The value ERR_EXEMPTY is returned and the value of variable pointed by the Rcv parameter is set to 
                the number of received characters. [ Version specific information for Freescale 56800 derivatives ]   DMA mode: 
                If DMA controller is available on the selected CPU and the receiver is configured to use DMA controller then 
                this method only sets the selected DMA channel. Then the status of the DMA transfer can be checked using 
                GetCharsInRxBuf method. See an example of a typical usage for details about communication using DMA.
   - AS1_SendBlock -Sends a block of characters to the channel.  This method is available only if non-zero length of the output 
                buffer is defined and the transmitter property is enabled.  [ Version specific information for Freescale 56800 
                derivatives ]   DMA mode:  If DMA controller is available on the selected CPU and the transmitter is configured 
                to use DMA controller then this method only sets the selected DMA channel. Then the status of the DMA transfer 
                can be checked using GetCharsInTxBuf method. See typical usage for details about communication using DMA.
   - AS1_ClearRxBuf -Clears the receive buffer.  This method is available only if non-zero length of the input buffer is 
                defined and the receiver property is enabled. [ Version specific information for Freescale 56800 derivatives ]  
                DMA mode:  If DMA controller is available on the selected CPU and the receiver is configured to use DMA 
                controller then this method only stops selected DMA channel.
   - AS1_ClearTxBuf -Clears the transmit buffer.  This method is available only if non-zero length of the output buffer is 
                defined and the receiver property is enabled. [ Version specific information for Freescale 56800 derivatives ]  
                DMA mode:  If DMA controller is available on the selected CPU and the transmitter is configured to use DMA 
                controller then this method only stops selected DMA channel.
   - AS1_GetCharsInRxBuf -Returns the number of characters in the input buffer. This method is available only if the receiver 
                property is enabled. [ Version specific information for Freescale 56800 derivatives ]   DMA mode:  If DMA 
                controller is available on the selected CPU and the receiver is configured to use DMA controller then this 
                method returns the number of characters in the receive buffer.
   - AS1_GetCharsInTxBuf -Returns the number of characters in the output buffer. This method is available only if the 
                transmitter property is enabled. [ Version specific information for Freescale 56800 derivatives ]   DMA mode:  
                If DMA controller is available on the selected CPU and the transmitter is configured to use DMA controller then 
                this method returns the number of characters in the transmit buffer.
   - AS1_GetBreak -Tests the internal input break flag, returns it (whether the break has occurred or not) and clears it. This 
                method is available only if the property <Break signal> and the property receiver are enabled.
   - AS1_SetBreak -Sends the break sequence to the output line. This method is available only if the <Break signal> property 
                and the transmitter property are enabled.

Module "TEST1"     (component DSP_Test)
   - TEST1_testStart -The testStart function initializes the test_sRec data structure
   - TEST1_testFailed -The testFailed function indicates that one step of the test case has failed. The string pointed to by 
                pMsg denotes the cause of the failure.
   - TEST1_testComment -The testComment function records information about the current test. The testComment is independent on 
                the test result (if it fails or not).
   - TEST1_testEnd -The testEnd function declares the end of the test and determines whether the test case has passed or failed.
                If no call had been made to testFailed since testStart was called, the test case passes. If any call to 
                testFailed had been made, the test case fails.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.

===================================================================================