=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "TMR1"      (component TMR1cascade)
   - TMR1_Init -This method initializes registers of the TMR module according to this Peripheral Initialization settings.    
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the component for more details.

Module "TMR2"      (component TMR2cascade)
   - TMR2_Init -This method initializes registers of the TMR module according to this Peripheral Initialization settings.    
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the component for more details.

Module "TMR3"      (component TMR3cascade)
   - TMR3_Init -This method initializes registers of the TMR module according to this Peripheral Initialization settings.    
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the component for more details.

Module "TMR4"      (component TMR4cascade)
   - TMR4_Init -This method initializes registers of the TMR module according to this Peripheral Initialization settings.    
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the component for more details.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.

===================================================================================