=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "CAN1"      (component FreescaleCAN)
   - CAN1_SetAcceptanceCode -Sets the message ID of the given message buffer. Buffer ID is used for message filtering of 
                incoming frames.
   - CAN1_SetAcceptanceMask -Sets the acceptance mask registers. This method writes an acceptance mask directly to the 
                acceptance mask registers.
   - CAN1_SendFrame -Sends a frame via the CAN device. Using this method the user can send own message to the CAN bus. This 
                method allows to specify CAN buffer number, message ID, data to be sent, frame type (DATA_FRAME/REMOTE_FRAME) 
                and whether the message will be sent after the request comes.
   - CAN1_ReadFrame -Reads a frame from the CAN device. The user is informed about CAN reception through OnFullRxBuffer event 
                or GetStateRX method.
   - CAN1_GetStateTX -Returns the value of the transmission complete flags (register FCIFLAG1).
   - CAN1_GetStateRX -Returns the value of the reception complete flags (register FCIFLAG1).
   - CAN1_SetBufferCode -Sets up the message buffer code for the appropriate message buffer. This method is always enabled 
                because it is used internally.

Module "TEST1"     (component DSP_Test)
   - TEST1_testStart -The testStart function initializes the test_sRec data structure
   - TEST1_testFailed -The testFailed function indicates that one step of the test case has failed. The string pointed to by 
                pMsg denotes the cause of the failure.
   - TEST1_testComment -The testComment function records information about the current test. The testComment is independent on 
                the test result (if it fails or not).
   - TEST1_testEnd -The testEnd function declares the end of the test and determines whether the test case has passed or failed.
                If no call had been made to testFailed since testStart was called, the test case passes. If any call to 
                testFailed had been made, the test case fails.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.

===================================================================================