=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "SCI1"      (component Init_SCI_56800)
   - SCI1_Init -This method initializes registers of the SCI module according to this Peripheral Initialization settings.    
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the component for more details.

Module "TEST1"     (component DSP_Test)
   - TEST1_testStart -The testStart function initializes the test_sRec data structure
   - TEST1_testFailed -The testFailed function indicates that one step of the test case has failed. The string pointed to by 
                pMsg denotes the cause of the failure.
   - TEST1_testComment -The testComment function records information about the current test. The testComment is independent on 
                the test result (if it fails or not).
   - TEST1_testEnd -The testEnd function declares the end of the test and determines whether the test case has passed or failed.
                If no call had been made to testFailed since testStart was called, the test case passes. If any call to 
                testFailed had been made, the test case fails.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.

===================================================================================