=============================================================================
List of generated methods in project: ProcessorExpert

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "I2C1"      (component InternalI2C)
   - I2C1_SendChar -When working as a MASTER, this method writes one (7-bit addressing) or two (10-bit addressing) slave 
                address bytes inclusive of R/W bit = 0 to the I2C bus and then writes one character (byte) to the bus. The 
                slave address must be specified before, by the "SelectSlave" or "SelectSlave10" method or in the component 
                initialization section, "Target slave address init" property. If interrupt service is enabled and the method 
                returns ERR_OK, it doesn't mean that transmission was successful. The state of transmission is obtainable from 
                (OnTransmitData, OnError or OnArbitLost) events.   When working as a SLAVE, this method writes a character to 
                the internal output slave buffer and, after the master starts the communication, to the I2C bus. If no 
                character is ready for a transmission (internal output slave buffer is empty), the Empty character will be sent 
                (see "Empty character" property).
   - I2C1_RecvChar -When working as a MASTER, this method writes one (7-bit addressing) or two (10-bit addressing) slave 
                address bytes inclusive of R/W bit = 1 to the I2C bus, then reads one character (byte) from the bus and then 
                sends the stop condition. The slave address must be specified before, by the "SelectSlave" or "SelectSlave10" 
                method or in component initialization section, property "Target slave address init". If interrupt service is 
                enabled and the method returns ERR_OK, it doesn't mean that transmission was finished successfully. The state 
                of transmission must be tested by means of events (OnReceiveData, OnError or OnArbitLost). In case of 
                successful transmission, received data is ready after OnReceiveData event is called.   When working as a SLAVE, 
                this method reads a character from the input slave buffer.
   - I2C1_SendBlock -When working as a MASTER, this method writes one (7-bit addressing) or two (10-bit addressing) slave 
                address bytes inclusive of R/W bit = 0 to the I2C bus and then writes the block of characters to the bus. The 
                slave address must be specified before, by the "SelectSlave" or "SlaveSelect10" method or in component 
                initialization section, "Target slave address init" property. If interrupt service is enabled and the method 
                returns ERR_OK, it doesn't mean that transmission was successful. The state of transmission is detectable by 
                means of events (OnTransmitData, OnError or OnArbitLost). Data to be send is not copied to an internal buffer 
                and remains in the original location. Therefore the content of the buffer should not be changed until the 
                transmission is complete. Event OnTransmitData can be used to detect the end of the transmission.  When working 
                as a SLAVE, this method writes a block of characters to the internal output slave buffer and then, after the 
                master starts the communication, to the I2C bus. If no character is ready for a transmission (internal output 
                slave buffer is empty), the "Empty character" will be sent (see "Empty character" property). In SLAVE mode the 
                data are copied to an internal buffer, if specified by "Output buffer size" property.
   - I2C1_RecvBlock -When working as a MASTER, this method writes one (7-bit addressing) or two (10-bit addressing) slave 
                address bytes inclusive of R/W bit = 1 to the I2C bus, then reads the block of characters from the bus and then 
                sends the stop condition. The slave address must be specified before, by the "SelectSlave" or "SelectSlave10" 
                method or in component initialization section, "Target slave address init" property. If interrupt service is 
                enabled and the method returns ERR_OK, it doesn't mean that transmission was finished successfully. The state 
                of transmission must be tested by means of events (OnReceiveData, OnError or OnArbitLost). In case of 
                successful transmission, received data is ready after OnReceiveData event is called.   When working as a SLAVE, 
                this method reads a block of characters from the input slave buffer.
   - I2C1_GetCharsInTxBuf -Returns number of characters in the output buffer. In SLAVE mode returns the number of characters in 
                the internal slave output buffer. In MASTER mode returns number of characters to be sent from the user buffer 
                (passed by SendBlock method).  This method is not supported in polling mode.
   - I2C1_GetCharsInRxBuf -Returns number of characters in the input buffer. In SLAVE mode returns the number of characters in 
                the internal slave input buffer. In MASTER mode returns number of characters to be received into a user buffer 
                (passed by RecvChar or RecvBlock method).   This method is not supported in polling mode.
   - I2C1_SelectSlave -This method selects a new slave for communication by its 7-bit slave address value. Any send or receive 
                method directs to or from selected device, until a new slave device is selected by this method. This method is 
                not available for the SLAVE mode.
   - I2C1_CheckBus -This method returns the status of the bus. If the START condition has been detected, the method returns 
                'ComponentName'_BUSY. If the STOP condition has been detected, the method returns 'ComponentName'_IDLE.

Module "TEST1"     (component DSP_Test)
   - TEST1_testStart -The testStart function initializes the test_sRec data structure
   - TEST1_testFailed -The testFailed function indicates that one step of the test case has failed. The string pointed to by 
                pMsg denotes the cause of the failure.
   - TEST1_testComment -The testComment function records information about the current test. The testComment is independent on 
                the test result (if it fails or not).
   - TEST1_testEnd -The testEnd function declares the end of the test and determines whether the test case has passed or failed.
                If no call had been made to testFailed since testStart was called, the test case passes. If any call to 
                testFailed had been made, the test case fails.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.
   - Cpu_Delay100US -This method realizes software delay. The length of delay is at least 100 microsecond multiply input 
                parameter [us100]. As the delay implementation is not based on real clock, the delay time may be increased by 
                interrupt service routines processed during the delay. Adding read wait states for external program memory can 
                cause delay extension as well. The method is independent on selected speed mode.

===================================================================================