LPC5410x Group Interrupt example
===============================

Example description
-------------------
The Grouped GPIO interrupt example demonstrates the Grouped GPIO interrupt feature.

This example configures Grouped GPIO interrupt 0 to be invoked when both the buttons SW1-WAKE 
and SW2-ISP are pressed by the user. The interrupt toggles the state of LED 0. 

Special connection requirements
-------------------------------
There are no special connection requirements for this example.

Build procedures:
-----------------
Visit the at 'LPCOpen quickstart guides' [http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-v200-quickstart-guides]
to get started building LPCOpen projects.