/*
 *                   Copyright (c), NXP Semiconductors
 *
 *       All rights are reserved. Reproduction in whole or in part is
 *      prohibited without the written consent of the copyright owner.
 *  NXP reserves the right to make changes without notice at any time.
 * NXP makes no warranty, expressed, implied or statutory, including but
 * not limited to any implied warranty of merchantability or fitness for any
 *particular purpose, or that the use will not infringe any third party patent,
 * copyright or trademark. NXP must not be liable for any loss or damage
 *                          arising from its use.
 */

/** \file
 * Application specific selection of Reader Library Components
 *
 *
 * $Author: Purnank G (ing05193) $
 * $Revision: 6108 $
 * $Date: 2016-09-22 14:01:56 +0530 (Thu, 22 Sep 2016) $
 *
 *
 *
 */

#ifndef PH_NXPBUILD_APP_H_INC
#define PH_NXPBUILD_APP_H_INC


/** \defgroup ph_NxpBuild NXP Build
* \brief Controls the Inclusion of required components, Inclusion SRC/DATA within components and the Build Dependencies between the components
* @{
*/

/* NXPBUILD_DELETE: included code lines should be always removed from code */

/* NXP BUILD DEFINES */
/* use #define to include components            */
/* comment out #define to exclude components    */


/* DEBUG build mode */
/*#define NXPBUILD__PH_DEBUG*/                              /**< DEBUG build definition */


#define NXPRDLIB_REM_GEN_INTFS
/*********************************************************************************************************************************************************************************/

#define NXPBUILD__PH_PLATFORM                               /**< Embedded Platform Porting and Abstraction Component included. Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. */

#define NXPBUILD__PHNFCLIB                                  /**< Simplified API Interface, If enabling this the entry point should be this component in the application */

#ifdef NXPBUILD__PHNFCLIB
    #define NXPBUILD__PH_NFCLIB_ISO                             /* Enable the ISO profile of Simplified API */
    //#define NXPBUILD__PH_NFCLIB_EMVCO                           /* Enable the EMVCO profile of Simplified API */
    //#define NXPBUILD__PH_NFCLIB_NFC                             /* Enable the NFC profile of Simplified API */
#endif /* NXPBUILD__PHNFCLIB */


#ifdef NXPBUILD__PH_PLATFORM                                /**< If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required. */
    #ifdef CPU_MK82FN256VLL15
        #define NXPBUILD__PH_KINETIS_K82                    /**< K82 Freedom Board */
    #endif
    #if defined(__PN74XXXX__) || defined (__PN73XXXX__)
        #define NXPBUILD__PHHAL_HW_PN7462AU                   /**< NFC Controller PN7462AU HAL */
    #elif defined(__CODE_RED)
        #define NXPBUILD__PH_LPC1769                        /**< Host Controller LPC1769 */
        //#define NXPBUILD__PH_LPC11U68                     /**< Host Controller LPC11U68 */
    #endif
    //#define NXPBUILD__PH_RASPBERRY_PI                     /**< Host Controller RaspBerry Pi */
    //#define NXPBUILD__PH_UDOO_NEO                         /**< Host Controller udoo-neo */

    #if defined(NXPBUILD__PH_RASPBERRY_PI) || defined(NXPBUILD__PH_UDOO_NEO)
        #define NXPBUILD__PH_OSAL_LINUX                     /**< OSAL Implementation of POSIX is included. RdLib is executed as UM application in Linux */
    #else
        //#define NXPBUILD__PH_OSAL_NULLOS                  /**< OSAL Implementation of NULL OS is included. RdLib executed in Executive Loop. */
        #define NXPBUILD__PH_OSAL_FREERTOS                  /**< OSAL Implementation of Free RTOS is included. RdLib is linked to Free RTOS Library */
    #endif

    #if defined(NXPBUILD__PH_LPC1769) || defined(NXPBUILD__PH_LPC11U68)
        /* Host Controller SDK- Front End HAL Interface ie. Bus Abstraction Layer. Define only one of the below */
        #define NXPBUILD__PHBAL_REG_LPCOPEN_SPI             /**< LPCOpenStack SPI BAL Component is included. */
        //#define NXPBUILD__PHBAL_REG_LPCOPEN_I2C           /**< LPCOpenStack SPI I2C Component is included. */
    #endif

    #if defined (NXPBUILD__PH_KINETIS_K82)
        #define NXPBUILD__PHBAL_REG_KINETIS_SPI
        //#define NXPBUILD__PHBAL_REG_KINETIS_I2C
    #endif

    #ifdef NXPBUILD__PH_RASPBERRY_PI
        //#define NXPBUILD__PHBAL_REG_LINUX_KERNEL_SPI
        #define NXPBUILD__PHBAL_REG_LINUX_USER_SPI
        //#define NXPBUILD__PHBAL_REG_LINUX_USER_I2C
    #endif //NXPBUILD__PH_RASPBERRY_PI

#endif /* NXPBUILD__PH_PLATFORM */

#ifndef NXPBUILD__PHHAL_HW_PN7462AU                         /**< If the used NFC HW is not NFC Controller like PN7462AU, then include one of the front end HAL */
    //#define NXPBUILD__PHHAL_HW_RC523                      /**< RC523 HAL Component is included. */
    //#define NXPBUILD__PHHAL_HW_RC663                      /**< RC663 HAL Component is included */
    #define NXPBUILD__PHHAL_HW_PN5180                       /**< PN5180 HAL Component is included */
#endif /* NXPBUILD__PHHAL_HW_PN7462AU */

#if defined(NXPBUILD__PHHAL_HW_RC523) || \
    defined(NXPBUILD__PHHAL_HW_PN5180) || \
    defined(NXPBUILD__PHHAL_HW_PN7462AU)
//    #define NXPBUILD__PHHAL_HW_TARGET                     /**< Dependency checking if target mode macros should be enabled */
#endif

/*********************************************************************************************************************************************************************************/

#define NXPBUILD__PHPAL_I14443P3A_SW                        /**< PAL ISO 14443-3A SW Component is included. */

#define NXPBUILD__PHPAL_I14443P3B_SW                        /**< PAL ISO 14443-3B SW Component is included. */

#define NXPBUILD__PHPAL_I14443P4A_SW                        /**< PAL ISO 14443-4A SW Component is included. */

#define NXPBUILD__PHPAL_I14443P4_SW                         /**< PAL ISO 14443-4 SW Component is included. */

//#define NXPBUILD__PHPAL_MIFARE_SW                     /**< PAL MIFARE SW Component is included */
//#define NXPBUILD__PHPAL_MIFARE_STUB                   /**< PAL MIFARE STUB Component is included */

//#define NXPBUILD__PHPAL_FELICA_SW                         /**< PAL Felica SW Component is included. */

#ifndef NXPBUILD__PHHAL_HW_RC523                            /**< If FE HAL is RC523, then exclude ISO15693 & ISO18000p3m3 PAL, otherwise include as required. */
  #define NXPBUILD__PHPAL_SLI15693_SW                     /**< PAL SLI 15693 Component is included. */
  #define NXPBUILD__PHPAL_I18000P3M3_SW                   /**< PAL ISO 18000p3m3 Component is included. */
#endif /* NXPBUILD__PHHAL_HW_RC523 */

#ifdef NXPBUILD__PHHAL_HW_RC663                             /**< If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude. */
//  #define NXPBUILD__PHPAL_EPCUID_SW                       /**< PAL EPC UID SW Component is included. */
#endif

//#define NXPBUILD__PHPAL_I18092MPI_SW                      /**< PAL ISO18092 (P2P) SW Component is included. */

#ifndef NXPBUILD__PHHAL_HW_RC663                            /**< If FE HAL is RC663, then exclude ISO14443 Card Mode PAL & ISO18092 Target Mode PAL, otherwise include as required. */
    #ifdef NXPBUILD__PH_PLATFORM                            /**< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform. */
//      #define NXPBUILD__PHPAL_I14443P4MC_SW               /**< PAL ISO 14443-4 Card Mode SW Component is included. */
//      #define NXPBUILD__PHPAL_I18092MT_SW                 /**< PAL ISO 18092 Target Mode SW Component is included. */
    #endif /* NXPBUILD__PH_PLATFORM */
#endif /* NXPBUILD__PHHAL_HW_RC663 */

/*********************************************************************************************************************************************************************************/

#define NXPBUILD__PHAC_DISCLOOP_SW                          /**< Discovery Loop Activity SW Component is included. */

#ifdef NXPBUILD__PHAC_DISCLOOP_SW                           /**< If DiscLoop SW Component is included,  macros( & it's dependencies) to include/exclude SRC/DATA within Discloop is defined. */

    #if defined (NXPBUILD__PHHAL_HW_PN5180)   || \
            defined (NXPBUILD__PHHAL_HW_RC663) || \
            defined (NXPBUILD__PHHAL_HW_PN7462AU)
//              #define NXPBUILD__PHAC_DISCLOOP_LPCD       /**< SRC to enable LPCD is included. */
    #endif

    #ifdef  NXPBUILD__PHPAL_I14443P3A_SW
        #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS     /**< SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included. */
//      #define NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS    /**< SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included. */

        #if defined(NXPBUILD__PHPAL_I14443P4A_SW) && defined(NXPBUILD__PHPAL_I14443P4_SW)
            #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS  /**< SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included. */
        #endif
    #endif /* NXPBUILD__PHPAL_I14443P3A_SW */


    #if defined(NXPBUILD__PHPAL_I14443P3A_SW) && defined(NXPBUILD__PHPAL_I18092MPI_SW)
        #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS      /**< SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included. */
    #endif

    #ifdef NXPBUILD__PHPAL_I18092MPI_SW
        #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE   /**< SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included. */
        #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE/**< SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included. */
        #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE/**< SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included. */
    #endif /* NXPBUILD__PHPAL_I18092MPI_SW */

    #ifdef NXPBUILD__PHPAL_FELICA_SW
        #define NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS                /**< SRC/DATA to Detect FeliCa Cards is included. */
        #ifdef  NXPBUILD__PHPAL_I18092MPI_SW
            #define NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS         /**< SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included. */
        #endif /* NXPBUILD__PHPAL_I18092MPI_SW */
    #endif /* NXPBUILD__PHPAL_FELICA_SW */

    #ifdef NXPBUILD__PHPAL_I14443P3B_SW
        #define NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P3B_TAGS           /**< SRC/DATA to Detect Type B Cards that operate at Layer3 level is included */
        #ifdef NXPBUILD__PHPAL_I14443P4_SW
            #define NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P4B_TAGS       /**< SRC/DATA to Detect Type B Cards such as NFC Forum Type 4 Tags, EMVCo Type B Cards etc is included */
        #endif /* NXPBUILD__PHPAL_I14443P4_SW */
    #endif /* NXPBUILD__PHPAL_I14443P3B_SW */

    #ifdef NXPBUILD__PHPAL_SLI15693_SW
        #define NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS                 /**< SRC/DATA to Detect Type V Cards such as ICODE SLI/SLIX/SLI2/Tesa Cards is included*/
    #endif /* NXPBUILD__PHPAL_SLI15693_SW */

    #ifdef NXPBUILD__PHPAL_I18000P3M3_SW
        #define NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS            /**< SRC/DATA to Detect ICODE ILT Cards such as  SMARTRAC StackIt Cards is included*/
    #endif /* NXPBUILD__PHPAL_I18000P3M3_SW */


    #ifndef NXPBUILD__PHHAL_HW_RC663                               /**< If FE HAL is RC663, target mode is not supported at all, hence exclude those SRC, otherwise include as required */
        #ifdef NXPBUILD__PHHAL_HW_TARGET
            #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE   /**< SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included. */
            #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE    /**< SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included. */
            #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE/**< SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included. */
            #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE /**< SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included. */
            #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE/**< SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included. */
            #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE /**< SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included. */
        #endif /* NXPBUILD__PHHAL_HW_TARGET */
    #endif

#endif /* NXPBUILD__PHAC_DISCLOOP_SW */

/*********************************************************************************************************************************************************************************/

#ifdef NXPBUILD__PH_NFCLIB_ISO

    #ifdef NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS
        #define NXPBUILD__PH_NFCLIB_ISO_MFC
        #define NXPBUILD__PH_NFCLIB_ISO_MFUL
    #endif /* NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS */

    #ifdef NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS
        #define NXPBUILD__PH_NFCLIB_ISO_MFDF
    #endif /* NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS */

    #ifdef NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS
         #define NXPBUILD__PH_NFCLIB_ISO_15693
    #endif /* NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS*/

   #ifdef NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS
      #define NXPBUILD__PH_NFCLIB_ISO_18000
   #endif /* NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS */

#endif /* NXPBUILD__PH_NFCLIB_ISO*/
/*********************************************************************************************************************************************************************************/

//#define NXPBUILD__PH_CIDMANAGER_SW                            /**< CID Manager SW Component is included. */

#define NXPBUILD__PH_KEYSTORE_SW                                  /**< SW KeyStore Component is included. */

#if defined(NXPBUILD__PHHAL_HW_RC663) && !defined(NXPBUILD__PH_KEYSTORE_SW)
//  #define NXPBUILD__PH_KEYSTORE_RC663                         /**< RC663 KeyStore Component is included. */
#endif
//#define NXPBUILD__PH_NDA_MFDF                                 /**< Mifare DESFire */
//#define NXPBUILD__PH_CRYPTOSYM_SW                             /**< Crypto Symbols SW Component is included. */
//#define NXPBUILD__PH_CRYPTORNG_SW                             /**< Crypto RNG SW Component is included. */

/*********************************************************************************************************************************************************************************/

#ifdef NXPBUILD__PHPAL_FELICA_SW
    #define NXPBUILD__PHAL_FELICA_SW                            /**< AL FeliCa SW Component is included */
#endif /* NXPBUILD__PHPAL_FELICA_SW */

#ifdef NXPBUILD__PHPAL_MIFARE_SW
    #if defined(NXPBUILD__PH_KEYSTORE_SW) || defined(NXPBUILD__PH_KEYSTORE_RC663)
        #define NXPBUILD__PHAL_MFC_SW                           /**< AL Mifare Classic SW Component is included */
    #endif
    #define NXPBUILD__PHAL_MFUL_SW                              /**< AL Mifare Ultrlight SW Component is included */
    #define NXPBUILD__PHAL_MFDF_SW                              /**< AL Mifare DesFire SW Component is included */
#endif /* NXPBUILD__PHPAL_MIFARE_SW */

//#define NXPBUILD__PHAL_T1T_SW                                     /**< AL Type T1 Tag SW Component is included */

#ifdef NXPBUILD__PHPAL_SLI15693_SW
    //#define NXPBUILD__PHAL_I15693_SW                            /**< AL ISO 15693  SW Component is included */
//  #define NXPBUILD__PHAL_SLI_SW                               /**< AL SLI SW Component is included */
#endif /* NXPBUILD__PHPAL_SLI15693_SW */

//#define NXPBUILD__PHAL_TOP_SW                                     /**< AL for TagOps Mapping SW Component is included.Required for NDEF operations */

#ifdef NXPBUILD__PHPAL_I18000P3M3_SW
    #define NXPBUILD__PHAL_I18000P3M3_SW                        /**< AL ISO18000p3m3 SW Component is included */
#endif /* NXPBUILD__PHPAL_I18000P3M3_SW */

#ifdef NXPBUILD__PHPAL_I14443P4MC_SW
    #if !defined(NXPBUILD__PH_OSAL_NULLOS) && defined(NXPBUILD__PH_PLATFORM)
        #define NXPBUILD__PHCE_T4T_SW                           /**< AL HCE T2AT SW Component is included */
        //#define NXPBUILD__PHCE_T4T_PROPRIETARY                /**< SRC to handle HCE T4AT Proprietary Commands is included */
        /*#define NXPBUILD__PHCE_T4T_EXT_NDEF */                /**< SRC to handle Extended NDEF Support as per T4T spec 3.0 is included */
    #endif
#endif /* NXPBUILD__PHPAL_I14443P4MC_SW */

/* LLCP Components */
#if defined(NXPBUILD__PHPAL_I18092MPI_SW) || defined(NXPBUILD__PHPAL_I18092MT_SW)
    #if !defined(NXPBUILD__PH_OSAL_NULLOS) && defined(NXPBUILD__PH_PLATFORM)
        #define NXPBUILD__PHLN_LLCP_SW                           /**< Link LLCP SW Component is included */
    #endif
#endif

/* SNEP components */
#ifdef NXPBUILD__PHLN_LLCP_SW
    #define NXPBUILD__PHNP_SNEP_SW                               /**< Protocol SNEP SW Component is included */
#endif /* NXPBUILD__PHLN_LLCP_SW */

/* Enable/disable Debugging */
/*#define NXPBUILD__PH_DEBUG*/                                   /**< TODO: To be checked if required */

/** @}
* end of ph_NxpBuild
*/

#endif /* PH_NXPBUILD_APP_H_INC */