|
NXP NFC Reader Library
v4.040.05.011646
|
SNEP parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY!. More... | |
| void * | plnLlcpDataParams |
| LLCP Data Parameters structure pointer. More... | |
| void * | psSocket |
| LLCP transport Socket structure pointer. More... | |
| uint8_t | bSnepVersion |
| SNEP protocol version supported by Implementation. More... | |
| phnpSnep_Server_type_t | eServerType |
| Initialized Server Type. More... | |
SNEP parameter structure.
| uint16_t phnpSnep_Sw_DataParams::wId |
Layer ID for this component, NEVER MODIFY!.
| void* phnpSnep_Sw_DataParams::plnLlcpDataParams |
LLCP Data Parameters structure pointer.
| void* phnpSnep_Sw_DataParams::psSocket |
LLCP transport Socket structure pointer.
| uint8_t phnpSnep_Sw_DataParams::bSnepVersion |
SNEP protocol version supported by Implementation.
| phnpSnep_Server_type_t phnpSnep_Sw_DataParams::eServerType |
Initialized Server Type.