|
NXP NFC Reader Library
v4.040.05.011646
|
ISO14443-4 parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pHalDataParams |
| Pointer to the parameter structure of the underlying layer. More... | |
| uint8_t | bStateNow |
| Current Exchange-State. More... | |
| uint8_t | bCidEnabled |
| Card Identifier Enabler; Unequal '0' if enabled. More... | |
| uint8_t | bCid |
| Card Identifier; Ignored if *pCidSupported is equal '0'. More... | |
| uint8_t | bNadEnabled |
| Node Address Enabler; Unequal '0' if enabled. More... | |
| uint8_t | bNad |
| Node Address; Ignored if bNadEnabled is equal '0'. More... | |
| uint8_t | bFwi |
| Frame Waiting Integer. More... | |
| uint8_t | bFsdi |
| PCD Frame Size Integer; 0-8;. | |
| uint8_t | bFsci |
| PICC Frame Size Integer; 0-8;. | |
| uint8_t | bPcbBlockNum |
| Current Block-Number; 0/1;. | |
| uint8_t | bMaxRetryCount |
| Maximum Retry count for ISO/IEC 14443-4:2008(E) Rule 4 and 5. More... | |
| uint8_t | bOpeMode |
| Operation mode. More... | |
ISO14443-4 parameter structure.
| void* phpalI14443p4_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of the underlying layer.
| uint8_t phpalI14443p4_Sw_DataParams_t::bStateNow |
Current Exchange-State.
| uint8_t phpalI14443p4_Sw_DataParams_t::bCidEnabled |
Card Identifier Enabler; Unequal '0' if enabled.
| uint8_t phpalI14443p4_Sw_DataParams_t::bCid |
Card Identifier; Ignored if *pCidSupported is equal '0'.
| uint8_t phpalI14443p4_Sw_DataParams_t::bNadEnabled |
Node Address Enabler; Unequal '0' if enabled.
| uint8_t phpalI14443p4_Sw_DataParams_t::bNad |
Node Address; Ignored if bNadEnabled is equal '0'.
| uint8_t phpalI14443p4_Sw_DataParams_t::bFwi |
Frame Waiting Integer.
| uint8_t phpalI14443p4_Sw_DataParams_t::bMaxRetryCount |
Maximum Retry count for ISO/IEC 14443-4:2008(E) Rule 4 and 5.
| uint8_t phpalI14443p4_Sw_DataParams_t::bOpeMode |
Operation mode.
One of NFC, EMVCo, ISO.