|
NXP NFC Reader Library
v4.040.05.011646
|
Defines parameters that needs be provided by User to communicate with MIFare Ultralight card. More...
Data Fields | |
| phNfcLib_MFUL_Commands_t | bCommand |
| [In] Mifare Ultralight command needs to be provided. More... | |
| uint8_t | bPageNumber |
| [In] Page number on which Mifare Ultralight command to be executed. More... | |
| phNfcLib_MFUL_Commands_t phNfcLib_MFUL::bCommand |
[In] Mifare Ultralight command needs to be provided.
| uint8_t phNfcLib_MFUL::bPageNumber |
[In] Page number on which Mifare Ultralight command to be executed.