|
NXP NFC Reader Library
v4.040.05.011646
|
|
Data Structures | |
| struct | phpalI14443p4a_Sw_DataParams_t |
| Software PAL-ISO14443P4A parameter structure. More... | |
Macros | |
| #define | PHPAL_I14443P4A_SW_ID 0x01 |
| ID for Software ISO14443-4A layer. | |
Functions | |
| phStatus_t | phpalI14443p4a_Sw_Init (phpalI14443p4a_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pHalDataParams) |
| Initialize this layer. More... | |
| phStatus_t phpalI14443p4a_Sw_Init | ( | phpalI14443p4a_Sw_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| void * | pHalDataParams | ||
| ) |
Initialize this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | Specifies the size of the data parameter structure. |
| [in] | pHalDataParams | Pointer to the parameter structure of the underlying layer. |