|
NXP NFC Reader Library
v4.040.05.011646
|
Common defines used within the API of NFC library. More...
|
RF Technologies | |
Definitions used within phNfcLib_Activate and struct phNfcLib_PeerInfo_t | |
| #define | PH_NFCLIB_TECHNOLOGY_DEFAULT 0x0UL |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_14443_A (PH_NFCLIB_TECHNOLOGY_ISO_14443_A << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| ISO 14443-3A, Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_14443_B (PH_NFCLIB_TECHNOLOGY_ISO_14443_B << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| ISO 14443-3B, Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_FELICA (PH_NFCLIB_TECHNOLOGY_FELICA << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| FELICA Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_15693 (PH_NFCLIB_TECHNOLOGY_ISO_15693 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| ISO 15693, Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_18000_3_3 (PH_NFCLIB_TECHNOLOGY_ISO_18000_3_3 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| ISO 18000-3m3, Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_18092 (PH_NFCLIB_TECHNOLOGY_ISO_18092 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
| ISO 18092 active mode, Initiator mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_TARGET_ISO_14443_A (PH_NFCLIB_TECHNOLOGY_ISO_14443_A << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
| ISO 14443-3A, Target mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_TARGET_ISO_14443_B (PH_NFCLIB_TECHNOLOGY_ISO_14443_B << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
| ISO 14443-3B, Target mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_TARGET_FELICA (PH_NFCLIB_TECHNOLOGY_FELICA << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
| FELICA Target mode RF technology. More... | |
| #define | PH_NFCLIB_TECHNOLOGY_TARGET_ISO_18092 (PH_NFCLIB_TECHNOLOGY_ISO_18092 << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
| ISO 18092 active mode, Target mode RF technology. More... | |
Configuration Defaults | |
| #define | PH_NFCLIB_ACTIVATION_BLOCKINGMODE_DEFAULT PH_ON |
| #define | PH_NFCLIB_DEACTIVATION_BLOCKINGMODE_DEFAULT PH_ON |
Activation Priority | |
Definitions used as values for phNfcLib_SetConfig_Value and phNfcLib_GetConfig when using configuration tag PH_NFCLIB_CONFIG_ACTIVATION_MERGED_SAK_PRIO | |
| #define | PH_NFCLIB_ACTIVATION_MERGED_SAK_PRIO_14443 0x0U |
| Priority given to ISO 14443. | |
| #define | PH_NFCLIB_ACTIVATION_MERGED_SAK_PRIO_18092 0x1U |
| Priority given to ISO 18092. | |
Deactivation Mode | |
Definitions used within phNfcLib_DeActivate for bDeactivateMode parameter. | |
| #define | PH_NFCLIB_DEACTIVATION_MODE_RF_OFF 0x0U |
| No target deactivation procedure is performed, RF field is just switched off and wait for 5.1ms. More... | |
| #define | PH_NFCLIB_DEACTIVATION_MODE_RELEASE 0x1U |
| A target deactivation procedure is performed if applicable. More... | |
Activation Profiles | |
Definitions used as values for phNfcLib_SetConfig_Value and phNfcLib_GetConfig when using configuration tag PH_NFCLIB_CONFIG_ACTIVATION_PROFILE | |
| #define | PH_NFCLIB_ACTIVATION_PROFILE_NFC 0x0U |
| NFC Forum Activation Loop Profile and NDEF communication channel. More... | |
| #define | PH_NFCLIB_ACTIVATION_PROFILE_EMVCO 0x1U |
| EMVCo Activation Loop Profile and ISO14443-4 communication channel. | |
| #define | PH_NFCLIB_ACTIVATION_PROFILE_ISO 0x2U |
| Generic ISO Activation Loop Profile and block/frame oriented communication channel (depending on underlying protocol) | |
Common defines used within the API of NFC library.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_14443_A (PH_NFCLIB_TECHNOLOGY_ISO_14443_A << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
ISO 14443-3A, Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_14443_B (PH_NFCLIB_TECHNOLOGY_ISO_14443_B << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
ISO 14443-3B, Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_FELICA (PH_NFCLIB_TECHNOLOGY_FELICA << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
FELICA Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_15693 (PH_NFCLIB_TECHNOLOGY_ISO_15693 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
ISO 15693, Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_18000_3_3 (PH_NFCLIB_TECHNOLOGY_ISO_18000_3_3 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
ISO 18000-3m3, Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_INITIATOR_ISO_18092 (PH_NFCLIB_TECHNOLOGY_ISO_18092 << PH_NFCLIB_TECHNOLOGY_ROLE_INITIATOR_SHIFT) |
ISO 18092 active mode, Initiator mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_TARGET_ISO_14443_A (PH_NFCLIB_TECHNOLOGY_ISO_14443_A << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
ISO 14443-3A, Target mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_TARGET_ISO_14443_B (PH_NFCLIB_TECHNOLOGY_ISO_14443_B << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
ISO 14443-3B, Target mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_TARGET_FELICA (PH_NFCLIB_TECHNOLOGY_FELICA << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
FELICA Target mode RF technology.
| #define PH_NFCLIB_TECHNOLOGY_TARGET_ISO_18092 (PH_NFCLIB_TECHNOLOGY_ISO_18092 << PH_NFCLIB_TECHNOLOGY_ROLE_TARGET_SHIFT) |
ISO 18092 active mode, Target mode RF technology.
| #define PH_NFCLIB_DEACTIVATION_MODE_RF_OFF 0x0U |
No target deactivation procedure is performed, RF field is just switched off and wait for 5.1ms.
| #define PH_NFCLIB_DEACTIVATION_MODE_RELEASE 0x1U |
A target deactivation procedure is performed if applicable.
(Example, in case of activation profile PH_NFCLIB_ACTIVATION_PROFILE_EMVCO this means the removal procedure is performed. In other profiles this could imply execution of deactivation procedures like DSL_REQ.) RF field is not switched off. phNfcLib_DeActivate should be called with PH_NFCLIB_DEACTIVATION_MODE_RF_OFF to switch off RF field.
| #define PH_NFCLIB_ACTIVATION_PROFILE_NFC 0x0U |
NFC Forum Activation Loop Profile and NDEF communication channel.