These Components implement the ISO/IEC 18000-3 Mode3 support.
More...
|
| phStatus_t | phpalI18000p3m3_Exchange (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t bTxLastBits, uint8_t **ppRxBuffer, uint16_t *pRxLength, uint8_t *pRxLastBits) |
| | Perform Data Exchange with Tag. More...
|
| |
| phStatus_t | phpalI18000p3m3_CreateSelectCmd (void *pDataParams, uint8_t bTarget, uint8_t bAction, uint8_t bMemBank, uint8_t *pPointer, uint8_t bPointerLength, uint8_t *pMask, uint8_t bMaskBitLength, uint8_t bTruncate, uint8_t *pSelectCmd, uint8_t *bLen, uint8_t *bValidBits) |
| | Create the Select command frame. More...
|
| |
| phStatus_t | phpalI18000p3m3_CreateBeginRoundCmd (void *pDataParams, uint8_t bDr, uint8_t bM, uint8_t bTRext, uint8_t bSel, uint8_t bSession, uint8_t bRfu, uint8_t bQ, uint8_t *pBeginRnd) |
| | Create the BeginRound command frame. More...
|
| |
| phStatus_t | phpalI18000p3m3_Ack (void *pDataParams, uint8_t bOption, uint8_t *pHandle, uint8_t **ppRxBuffer, uint16_t *pRxBitLength) |
| | Perform a Ack for ISO18000-3 Mode3 tags. More...
|
| |
| phStatus_t | phpalI18000p3m3_Nak (void *pDataParams) |
| | Perform a Nak for ISO18000-3 Mode3 tags. More...
|
| |
| phStatus_t | phpalI18000p3m3_ActivateCard (void *pDataParams, uint8_t *pSelCmd, uint8_t bSelCmdLen, uint8_t bNumValidBitsinLastByte, uint8_t *pBeginRndCmd, uint8_t bTSprocessing, uint8_t **ppRxBuffer, uint16_t *pRxBufferLen, uint8_t *pMoreCardsAvailable) |
| | Bring the first matching tag to OPEN or SECURED state. More...
|
| |
| phStatus_t | phpalI18000p3m3_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| | Sets the configuration parameter. More...
|
| |
|
|
#define | PHPAL_I18000P3M3_MEMBANK_RESERVED 0x00U /** < Reserved Memory Bank. */ |
| |
|
#define | PHPAL_I18000P3M3_MEMBANK_UII 0x01U /** < UII Memory Bank. */ |
| |
|
#define | PHPAL_I18000P3M3_MEMBANK_TID 0x02U /** < TID Memory Bank. */ |
| |
|
#define | PHPAL_I18000P3M3_MEMBANK_USER 0x03U /** < User Memory Bank. */ |
| |
These Components implement the ISO/IEC 18000-3 Mode3 support.
§ PHPAL_I18000P3M3_TARGET_INVENTORIED_S0
| #define PHPAL_I18000P3M3_TARGET_INVENTORIED_S0 0x00U |
§ PHPAL_I18000P3M3_TARGET_INVENTORIED_S2
| #define PHPAL_I18000P3M3_TARGET_INVENTORIED_S2 0x02U |
§ PHPAL_I18000P3M3_TARGET_SL
| #define PHPAL_I18000P3M3_TARGET_SL 0x04U |
§ PHPAL_I18000P3M3_LF_423KHZ
| #define PHPAL_I18000P3M3_LF_423KHZ 0x00U |
§ PHPAL_I18000P3M3_LF_847KHZ
| #define PHPAL_I18000P3M3_LF_847KHZ 0x01U |
§ PHPAL_I18000P3M3_M_MANCHESTER_2
| #define PHPAL_I18000P3M3_M_MANCHESTER_2 0x02U |
2 sub-carrier pulse Manchester.
Equivalent to #PHHAL_HW_RF_RX_DATARATE_I18000P3M3_MAN2.
§ PHPAL_I18000P3M3_M_MANCHESTER_4
| #define PHPAL_I18000P3M3_M_MANCHESTER_4 0x03U |
4 sub-carrier pulse Manchester.
Equivalent to #PHHAL_HW_RF_RX_DATARATE_I18000P3M3_MAN4.
§ PHPAL_I18000P3M3_SEL_ALL_00
| #define PHPAL_I18000P3M3_SEL_ALL_00 0x00U |
§ PHPAL_I18000P3M3_SEL_ALL_01
| #define PHPAL_I18000P3M3_SEL_ALL_01 0x01U |
§ PHPAL_I18000P3M3_SEL_NOT_SL
| #define PHPAL_I18000P3M3_SEL_NOT_SL 0x02U |
Select only tags not matching SL.
§ PHPAL_I18000P3M3_SEL_SL
| #define PHPAL_I18000P3M3_SEL_SL 0x03U |
Select only tags matching SL.
§ PHPAL_I18000P3M3_SESSION_S0
| #define PHPAL_I18000P3M3_SESSION_S0 0x00U |
§ PHPAL_I18000P3M3_SESSION_S1
| #define PHPAL_I18000P3M3_SESSION_S1 0x01U |
§ PHPAL_I18000P3M3_SESSION_S2
| #define PHPAL_I18000P3M3_SESSION_S2 0x02U |
§ PHPAL_I18000P3M3_SESSION_S3
| #define PHPAL_I18000P3M3_SESSION_S3 0x03U |
§ PHPAL_I18000P3M3_UPDN_INCREMENT
| #define PHPAL_I18000P3M3_UPDN_INCREMENT 0x06U |
§ PHPAL_I18000P3M3_UPDN_NOCHANGE
| #define PHPAL_I18000P3M3_UPDN_NOCHANGE 0x00U |
§ PHPAL_I18000P3M3_UPDN_DECREMENT
| #define PHPAL_I18000P3M3_UPDN_DECREMENT 0x03U |
§ PHPAL_I18000P3M3_ACK_USE_CRC
| #define PHPAL_I18000P3M3_ACK_USE_CRC 0x00U |
Use StoredCrc for ACK command.
§ PHPAL_I18000P3M3_ACK_USE_HANDLE
| #define PHPAL_I18000P3M3_ACK_USE_HANDLE 0x01U |
Use given Handle for ACK command.
§ PHPAL_I18000P3M3_CONFIG_TXLASTBITS
| #define PHPAL_I18000P3M3_CONFIG_TXLASTBITS 0x0003U |
Set number of valid bits of last Tx-Byte.
§ PHPAL_I18000P3M3_CONFIG_TIMEOUT_VALUE_MS
| #define PHPAL_I18000P3M3_CONFIG_TIMEOUT_VALUE_MS 0x000EU |
Set RC Timeout (in [ms]).
§ PHPAL_I18000P3M3_TXLASTBITS_MAX
| #define PHPAL_I18000P3M3_TXLASTBITS_MAX 0x000FU |
Maximum value used for configuring TXLASTBITS.
§ PHPAL_I18000P3M3_VALID_TXLASTBITS
| #define PHPAL_I18000P3M3_VALID_TXLASTBITS 0x0007U |
Valid value of TXLASTBITS.
§ phpalI18000p3m3_Exchange()
Perform Data Exchange with Tag.
wOption can be one of:
Alternatively, the following bits can be combined:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of input data. |
| [in] | bTxLastBits | Number of valid bits of last byte (Tx). |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | Number of received data bytes including incomplete byte. |
| [out] | pRxLastBits | Number of valid bits of last byte (Rx). |
§ phpalI18000p3m3_CreateSelectCmd()
| phStatus_t phpalI18000p3m3_CreateSelectCmd |
( |
void * |
pDataParams, |
|
|
uint8_t |
bTarget, |
|
|
uint8_t |
bAction, |
|
|
uint8_t |
bMemBank, |
|
|
uint8_t * |
pPointer, |
|
|
uint8_t |
bPointerLength, |
|
|
uint8_t * |
pMask, |
|
|
uint8_t |
bMaskBitLength, |
|
|
uint8_t |
bTruncate, |
|
|
uint8_t * |
pSelectCmd, |
|
|
uint8_t * |
bLen, |
|
|
uint8_t * |
bValidBits |
|
) |
| |
Create the Select command frame.
This is a utility function to create the Select frame in the required format of ISO 18000p3m3. Parameters are validated to ensure that wrong values or wrong combinations are checked.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bTarget | Indicates whether the SL flag or the inventoried flags shall be modified. |
| [in] | bAction | Indicates the way of changing the SL flag and the inventoried flags. |
| [in] | bMemBank | Memory bank where the mask shall be applied. |
| [in] | pPointer | Memory address where the mask shall be applied. |
| [in] | bPointerLength | Length of the pointer, 0->8bits,1->16bits,2->24bits or 3->32bits. |
| [in] | pMask | Contains a bit string that a tag compares against the memory location that begins at pPointer. |
| [in] | bMaskBitLength | Length of the mask in bits. |
| [in] | bTruncate | Specifies whether a tag load modulates its entire UII (PH_OFF), or only that portion of the UII immediately following Mask (PH_ON). |
| [out] | pSelectCmd | Select Command frame. (Max 39 bytes) |
| [out] | bLen | Length of Select cmd bytes |
| [out] | bValidBits | Number of valid bits in the last byte of pSelectCmd. |
§ phpalI18000p3m3_CreateBeginRoundCmd()
Create the BeginRound command frame.
This is a utility function to create the BeginRound frame in the required format of ISO 18000p3m3. Parameters are validated to ensure that wrong values or wrong combinations are checked.
bDr can be one of
(Number of subcarrier cycles per symbol) cane be one of
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bDr | Divide ratio. |
| [in] | bM | Cycles per symbol. |
| [in] | bTRext | Indicates whether a pilot tone shall be used in the T=>R pre-amble (PH_ON) or not (PH_OFF). |
| [in] | bSel | Indicates which tags shall take part of the inventory round. |
| [in] | bSession | Indicates the session of the inventory round. |
| [in] | bRfu | RFU (1 bit). |
| [in] | bQ | Indicates the number of slots in a round (2^Q slots). |
| [out] | pBeginRnd | Begin round command frame (3 bytes) |
§ phpalI18000p3m3_Ack()
Perform a Ack for ISO18000-3 Mode3 tags.
bOption can be one of:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bOption | Option parameter. |
| [in] | pHandle | Handle value, mandatory if bOption is PHPAL_I18000P3M3_ACK_USE_HANDLE; uint8_t[2]. |
| [out] | ppRxBuffer | Pointer to Tag data and, if required, PacketCRC. |
| [out] | pRxBitLength | Tag response length in bits. |
§ phpalI18000p3m3_Nak()
| phStatus_t phpalI18000p3m3_Nak |
( |
void * |
pDataParams | ) |
|
Perform a Nak for ISO18000-3 Mode3 tags.
All tags will move to arbitrate state after receive this command.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
§ phpalI18000p3m3_ActivateCard()
Bring the first matching tag to OPEN or SECURED state.
The command performs a selection followed by an inventory round. The first responding tag is set to the OPEN or SECURED state and the tag handle is returned. If more tags are in the field, it shall resolve collision and activate one tag. The pMoreCardsAvailable value will be set to 1 if more cards are available in the field.
Issuing the Select command is optional based on the value of bSelCmdLen parameter. If bSelCmdLen parameter is zero, then ISO 18000p3m3 Select command is not issued. Only the BeginRound command is issued.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pSelCmd | ISO 18000p3m3 Select command frame. |
| [in] | bSelCmdLen | Select command length in bytes- 1 to 39 bytes. If set to zero, Select command is not sent. |
| [in] | bNumValidBitsinLastByte | Number of valid bits in last byte of pSelCmd. |
| [in] | pBeginRndCmd | ISO 18000p3m3 BeginRound command frame. This is 17bits i.e., 3 bytes are expected. CRC5 should not be provided. |
| [in] | bTSprocessing | TimeSlot processing behavior. |
| [out] | ppRxBuffer | Pointer to HAL Rx Buffer containing handle of the activated tag. |
| [out] | pRxBufferLen | Length of response in hal Rx Buffer. |
| [out] | pMoreCardsAvailable | Indicates if more tags are present in the field. |
§ phpalI18000p3m3_SetConfig()
| phStatus_t phpalI18000p3m3_SetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t |
wValue |
|
) |
| |
Sets the configuration parameter.
This function sets the values for the provided configuration parameter
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [in] | wValue | Configuration Value. |