These Components implement the ISO/IEC 14443-3 Type-A contactless protocol.
More...
|
| phStatus_t | phpalI14443p3a_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| | Set configuration parameter. More...
|
| |
| phStatus_t | phpalI14443p3a_GetConfig (void *pDataParams, uint16_t wConfig, uint16_t *pValue) |
| | Get configuration parameter. More...
|
| |
| phStatus_t | phpalI14443p3a_RequestA (void *pDataParams, uint8_t *pAtqa) |
| | Perform a ISO14443-3A Request command. More...
|
| |
| phStatus_t | phpalI14443p3a_WakeUpA (void *pDataParams, uint8_t *pAtqa) |
| | Perform a ISO14443-3A Wakeup command. More...
|
| |
| phStatus_t | phpalI14443p3a_HaltA (void *pDataParams) |
| | Perform a ISO14443-3A Halt command. More...
|
| |
| phStatus_t | phpalI14443p3a_Anticollision (void *pDataParams, uint8_t bCascadeLevel, uint8_t *pUidIn, uint8_t bNvbUidIn, uint8_t *pUidOut, uint8_t *pNvbUidOut) |
| | Perform a ISO14443-3A Anticollision or Select command. More...
|
| |
| phStatus_t | phpalI14443p3a_Select (void *pDataParams, uint8_t bCascadeLevel, uint8_t *pUidIn, uint8_t *pSak) |
| | Perform a ISO14443-3A Select command. More...
|
| |
| phStatus_t | phpalI14443p3a_ActivateCard (void *pDataParams, uint8_t *pUidIn, uint8_t bLenUidIn, uint8_t *pUidOut, uint8_t *pLenUidOut, uint8_t *pSak, uint8_t *pMoreCardsAvailable) |
| | Perform ISO14443-3A ReqA or WupA and Anticollision/Select commands for all cascade levels. More...
|
| |
| phStatus_t | phpalI14443p3a_Exchange (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| | Perform ISO14443-3A Data Exchange with Picc. More...
|
| |
| phStatus_t | phpalI14443p3a_GetSerialNo (void *pDataParams, uint8_t *pUidOut, uint8_t *pLenUidOut) |
| | Retrieve the serial number. More...
|
| |
These Components implement the ISO/IEC 14443-3 Type-A contactless protocol.
§ PHPAL_I14443P3A_CASCADE_LEVEL_1
| #define PHPAL_I14443P3A_CASCADE_LEVEL_1 0x93 |
Cascade Level 1 code for ISO14443-3A anticollision/select command.
§ PHPAL_I14443P3A_CASCADE_LEVEL_2
| #define PHPAL_I14443P3A_CASCADE_LEVEL_2 0x95 |
Cascade Level 2 code for ISO14443-3A anticollision/select command.
§ PHPAL_I14443P3A_CASCADE_LEVEL_3
| #define PHPAL_I14443P3A_CASCADE_LEVEL_3 0x97 |
Cascade Level 3 code for ISO14443-3A anticollision/select command.
§ PHPAL_I14443P3A_TIMEOUT_DEFAULT_MS
| #define PHPAL_I14443P3A_TIMEOUT_DEFAULT_MS 10 |
Timeout after card selection in milliseconds.
§ PHPAL_I14443P3A_CONFIG_OPE_MODE
| #define PHPAL_I14443P3A_CONFIG_OPE_MODE 0x001U |
§ PHPAL_I14443P3A_CONFIG_POLL_CMD
| #define PHPAL_I14443P3A_CONFIG_POLL_CMD 0x002U |
§ PHPAL_I14443P3A_CONFIG_TIMEOUT_VALUE_US
| #define PHPAL_I14443P3A_CONFIG_TIMEOUT_VALUE_US 0x003U |
Configure timeout in microseconds.
This shall be used by AL layers to set timeout for commands.
§ phpalI14443p3a_SetConfig()
| phStatus_t phpalI14443p3a_SetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t |
wValue |
|
) |
| |
Set configuration parameter.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [in] | wValue | Configuration Value. |
§ phpalI14443p3a_GetConfig()
| phStatus_t phpalI14443p3a_GetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t * |
pValue |
|
) |
| |
Get configuration parameter.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [out] | pValue | Configuration Value. |
§ phpalI14443p3a_RequestA()
| phStatus_t phpalI14443p3a_RequestA |
( |
void * |
pDataParams, |
|
|
uint8_t * |
pAtqa |
|
) |
| |
Perform a ISO14443-3A Request command.
Note: The "Request Guard Time" (see 6.2.2, ISO/IEC 14443-3:2009(E)) is mandatory and is neither implemented here nor implemented in every Hardware Abstraction Layer layer.
Make sure that either the used HAL or the used application does comply to this rule.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pAtqa | AtqA; uint8_t[2]. |
§ phpalI14443p3a_WakeUpA()
| phStatus_t phpalI14443p3a_WakeUpA |
( |
void * |
pDataParams, |
|
|
uint8_t * |
pAtqa |
|
) |
| |
Perform a ISO14443-3A Wakeup command.
Note: The "Request Guard Time" (see 6.2.2, ISO/IEC 14443-3:2009(E)) is mandatory and is neither implemented here nor implemented in every Hardware Abstraction Layer layer.
Make sure that either the used HAL or the used application does comply to this rule.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pAtqa | AtqA; uint8_t[2]. |
§ phpalI14443p3a_HaltA()
| phStatus_t phpalI14443p3a_HaltA |
( |
void * |
pDataParams | ) |
|
Perform a ISO14443-3A Halt command.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
§ phpalI14443p3a_Anticollision()
Perform a ISO14443-3A Anticollision or Select command.
bNvbUidIn != 0x40: Perform Anticollision command.
bNvbUidIn = 0x40: Perform Select command.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bCascadeLevel | cascade level code. |
| [in] | pUidIn | known Uid, can be NULL; uint8_t[0-4]. |
| [in] | bNvbUidIn | number of valid bits of UidIn. MSB codes the valid bytes, LSB codes the valid bits. |
| [out] | pUidOut | complete Uid; uint8_t[4]. |
| [out] | pNvbUidOut | number of valid bits of UidOut. MSB codes the valid bytes, LSB codes the valid bits. |
§ phpalI14443p3a_Select()
| phStatus_t phpalI14443p3a_Select |
( |
void * |
pDataParams, |
|
|
uint8_t |
bCascadeLevel, |
|
|
uint8_t * |
pUidIn, |
|
|
uint8_t * |
pSak |
|
) |
| |
Perform a ISO14443-3A Select command.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bCascadeLevel | cascade level code. |
| [in] | pUidIn | Uid; uint8_t[4]. |
| [out] | pSak | Select Acknowledge; uint8_t. |
§ phpalI14443p3a_ActivateCard()
Perform ISO14443-3A ReqA or WupA and Anticollision/Select commands for all cascade levels.
If bLenUidIn is '0' –> CardUid not given, a ReqA is performed. If CardUid is given, a WupA is performed.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUidIn | known Uid, can be NULL if bLenUidIn is 0; uint8_t[4/7/10]. |
| [in] | bLenUidIn | Length of known Uid; 0/4/7/10. |
| [out] | pUidOut | complete Uid; uint8_t[10]. |
| [out] | pLenUidOut | Length of Uid; 4/7/10. |
| [out] | pSak | Select Acknowledge; uint8_t. |
| [out] | pMoreCardsAvailable | Whether there are more cards in the field or not; uint8_t. |
§ phpalI14443p3a_Exchange()
Perform ISO14443-3A Data Exchange with Picc.
wOption can be one of:
Alternatively, the following bits can be combined:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | number of received data bytes. |
§ phpalI14443p3a_GetSerialNo()
| phStatus_t phpalI14443p3a_GetSerialNo |
( |
void * |
pDataParams, |
|
|
uint8_t * |
pUidOut, |
|
|
uint8_t * |
pLenUidOut |
|
) |
| |
Retrieve the serial number.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pUidOut | Last Uid; uint8_t[10]. |
| [out] | pLenUidOut | Length of Uid; 4/7/10. |