|
NXP NFC Reader Library
v4.040.05.011646
|
Component abstracting the functionality of LPC Open stack I2C interface. More...
|
Data Structures | |
| struct | phbalReg_LpcOpenI2c_DataParams_t |
| LPC Open I2C BAL parameter structure. More... | |
Macros | |
| #define | PHBAL_REG_LPCOPEN_I2C_ID 0x0EU |
| ID for LPC Open I2C BAL component. | |
Functions | |
| phStatus_t | phbalReg_LpcOpenI2c_Init (phbalReg_LpcOpenI2c_DataParams_t *pDataParams, uint16_t wSizeOfDataParams) |
| Initialize the LPC Open I2C BAL layer. More... | |
Component abstracting the functionality of LPC Open stack I2C interface.
| phStatus_t phbalReg_LpcOpenI2c_Init | ( | phbalReg_LpcOpenI2c_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams | ||
| ) |
Initialize the LPC Open I2C BAL layer.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_INVALID_DATA_PARAMS | Parameter structure size is invalid. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | Specifies the size of the data parameter structure. |