|
NXP NFC Reader Library
v4.040.05.011646
|
Private parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalMifareDataParams |
| Pointer to palMifare parameter structure. More... | |
| void * | pKeyStoreDataParams |
| Pointer to phKeystore parameter structure. More... | |
| void * | pCryptoDataParams |
| Pointer to phCrypto data parameters structure. More... | |
| void * | pCryptoRngDataParams |
| Pointer to the parameter structure of the CryptoRng layer. More... | |
Private parameter structure.
| void* phalMful_Sw_DataParams_t::pPalMifareDataParams |
Pointer to palMifare parameter structure.
| void* phalMful_Sw_DataParams_t::pKeyStoreDataParams |
Pointer to phKeystore parameter structure.
| void* phalMful_Sw_DataParams_t::pCryptoDataParams |
Pointer to phCrypto data parameters structure.
| void* phalMful_Sw_DataParams_t::pCryptoRngDataParams |
Pointer to the parameter structure of the CryptoRng layer.