|
NXP NFC Reader Library
v4.040.05.011646
|
ISO14443-4 card mode PAL parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY. More... | |
| uint16_t | wLastTxLen |
| Length of last I block send. More... | |
| void * | pHalDataParams |
| Pointer to the parameter structure of underlying hardware component. More... | |
| void * | pPlatform |
| Pointer to Platform layer. More... | |
| void * | pTimerHandle |
| Timer Handle (For WTX). More... | |
| uint8_t | bDisableWtx |
| WTX Disabler (i.e. More... | |
| uint8_t | bWtx |
| Frame Waiting Time Extension. More... | |
| uint8_t | bFsdi |
| FSDI parameter. More... | |
| uint8_t | bFsci |
| ATS FSCI parameter. More... | |
| uint8_t | bDr |
| ATS DR parameter. More... | |
| uint8_t | bDs |
| ATS DS parameter. More... | |
| uint8_t | bUnequalDrDs |
| DR and DS are different. More... | |
| uint8_t | bFwi |
| ATS FWI parameter. More... | |
| uint8_t | bSfgi |
| ATS SFGI parameter. More... | |
| uint8_t | bCidEnable |
| CID, Enabled = 1 or Disabled. More... | |
| uint8_t | bCidPresence |
| Flag to indicate CID presence in current command-response pair. More... | |
| uint8_t | bCid |
| CID parameter. More... | |
| uint8_t | bNadEnable |
| NAD, Enabled = 1 or Disabled. More... | |
| uint8_t | bNadPresence |
| Flag to indicate NAD presence in current command-response pair. More... | |
| uint8_t | bNad |
| NAD parameter. More... | |
| uint8_t | bStateNow |
| Current state. More... | |
| uint8_t | bBlockNr |
| Current block number. More... | |
| uint8_t | bChainingRx |
| We are chaining Rx. More... | |
| uint8_t | bChainingTx |
| We are chaining Tx. More... | |
| uint8_t | bOpMode |
| Operating mode - ISO or NFC. More... | |
| uint16_t | wWtDelta |
| Holds the configured delta time to be subtracted from the time in WTX timer. More... | |
| uint8_t | bWtPercentage |
| Percentage of actual wait time to be used in WTX timer. More... | |
| pWtxTimerCallback | pWtxTimerCallback |
| Holds WTX timer call-back function address. More... | |
ISO14443-4 card mode PAL parameter structure.
| uint16_t phpalI14443p4mC_Sw_DataParams_t::wId |
Layer ID for this component, NEVER MODIFY.
| uint16_t phpalI14443p4mC_Sw_DataParams_t::wLastTxLen |
Length of last I block send.
| void* phpalI14443p4mC_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of underlying hardware component.
| void* phpalI14443p4mC_Sw_DataParams_t::pPlatform |
Pointer to Platform layer.
| void* phpalI14443p4mC_Sw_DataParams_t::pTimerHandle |
Timer Handle (For WTX).
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bDisableWtx |
WTX Disabler (i.e.
'0' if WTX enabled).
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bWtx |
Frame Waiting Time Extension.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bFsdi |
FSDI parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bFsci |
ATS FSCI parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bDr |
ATS DR parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bDs |
ATS DS parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bUnequalDrDs |
DR and DS are different.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bFwi |
ATS FWI parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bSfgi |
ATS SFGI parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bCidEnable |
CID, Enabled = 1 or Disabled.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bCidPresence |
Flag to indicate CID presence in current command-response pair.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bCid |
CID parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bNadEnable |
NAD, Enabled = 1 or Disabled.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bNadPresence |
Flag to indicate NAD presence in current command-response pair.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bNad |
NAD parameter.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bStateNow |
Current state.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bBlockNr |
Current block number.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bChainingRx |
We are chaining Rx.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bChainingTx |
We are chaining Tx.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bOpMode |
Operating mode - ISO or NFC.
| uint16_t phpalI14443p4mC_Sw_DataParams_t::wWtDelta |
Holds the configured delta time to be subtracted from the time in WTX timer.
| uint8_t phpalI14443p4mC_Sw_DataParams_t::bWtPercentage |
Percentage of actual wait time to be used in WTX timer.
| pWtxTimerCallback phpalI14443p4mC_Sw_DataParams_t::pWtxTimerCallback |
Holds WTX timer call-back function address.