|
NXP NFC Reader Library
v4.040.05.011646
|
LLCP parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY!. More... | |
| void * | pPalI18092DataParams |
| Pointer to PAL 18092mPI/18092mT parameter structure. More... | |
| phlnLlcp_LMDataParams_t | sLocalLMParams |
| Local General Bytes. More... | |
| phlnLlcp_LMDataParams_t | sRemoteLMParams |
| Remote General Bytes. More... | |
| uint8_t | bAgreedVersion |
| Agreed Version number after Version Agreement. More... | |
| uint8_t | bCurrentClientCnt |
| Number of Registered Client count. More... | |
| uint8_t | bSdpClientSAP |
| SAP Address of the Client requested for SDP. More... | |
| uint8_t | bMacType |
| MAC type initialized either PHLN_LLCP_INITIATOR OR PHLN_LLCP_TARGET. More... | |
| phOsal_EventObj_t | LlcpEventObj |
| Event Object. More... | |
LLCP parameter structure.
| uint16_t phlnLlcp_Sw_DataParams::wId |
Layer ID for this component, NEVER MODIFY!.
| void* phlnLlcp_Sw_DataParams::pPalI18092DataParams |
Pointer to PAL 18092mPI/18092mT parameter structure.
| phlnLlcp_LMDataParams_t phlnLlcp_Sw_DataParams::sLocalLMParams |
Local General Bytes.
| phlnLlcp_LMDataParams_t phlnLlcp_Sw_DataParams::sRemoteLMParams |
Remote General Bytes.
| uint8_t phlnLlcp_Sw_DataParams::bAgreedVersion |
Agreed Version number after Version Agreement.
| uint8_t phlnLlcp_Sw_DataParams::bCurrentClientCnt |
Number of Registered Client count.
| uint8_t phlnLlcp_Sw_DataParams::bSdpClientSAP |
SAP Address of the Client requested for SDP.
| uint8_t phlnLlcp_Sw_DataParams::bMacType |
MAC type initialized either PHLN_LLCP_INITIATOR OR PHLN_LLCP_TARGET.
| phOsal_EventObj_t phlnLlcp_Sw_DataParams::LlcpEventObj |
Event Object.