|
NXP NFC Reader Library
v4.040.05.011646
|
Private parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalFelicaDataParams |
| Pointer to palFelica parameter structure. More... | |
| uint16_t | wAdditionalInfo |
| Holds the last error code sent by the VICC. More... | |
Private parameter structure.
| void* phalFelica_Sw_DataParams_t::pPalFelicaDataParams |
Pointer to palFelica parameter structure.
| uint16_t phalFelica_Sw_DataParams_t::wAdditionalInfo |
Holds the last error code sent by the VICC.