|
NXP NFC Reader Library
v4.040.05.011646
|
Peer Information. More...
Data Fields | |
| uint32_t | dwActivatedType |
| Activated type may be ORed value of phNfcLib_ActivatedType_t. More... | |
| uint32_t | dwSelectedType |
| Not used in this Beta release. More... | |
| uint16_t | wAtqa |
| To be done. More... | |
| uint8_t | bUidLength |
| Activated Type A tag UID length is provided. More... | |
| uint8_t | aUid [10] |
| Provides UID of activated Type A card. More... | |
| uint8_t | bSak |
| To be done. More... | |
| uint8_t | bAtqbLength |
| To be done. More... | |
| uint8_t | aPupi [4] |
| To be done. More... | |
| uint8_t | aApplicationData [4] |
| To be done. More... | |
| uint8_t | bIsExtendedAtqb |
| To be done. More... | |
| uint8_t | aProtocolInfo [4] |
| To be done. More... | |
| uint8_t * | pUii |
| Provides pointer to UII of ISO 18000p3m3 tags detected. More... | |
| uint16_t | wUiiLength |
| UII length in bits pointed by pUii. More... | |
| struct { | |
| } | tIso14443_4 |
| To be done. More... | |
| struct { | |
| } | tIso18092 |
| To be done. More... | |
| uint32_t phNfcLib_PeerInfo_t::dwActivatedType |
Activated type may be ORed value of phNfcLib_ActivatedType_t.
| uint32_t phNfcLib_PeerInfo_t::dwSelectedType |
Not used in this Beta release.
User has to choose from 'dwActivatedType' with any one card type phNfcLib_ActivatedType_t he is interested.
| uint16_t phNfcLib_PeerInfo_t::wAtqa |
To be done.
| uint8_t phNfcLib_PeerInfo_t::bUidLength |
Activated Type A tag UID length is provided.
| uint8_t phNfcLib_PeerInfo_t::aUid[10] |
Provides UID of activated Type A card.
| uint8_t phNfcLib_PeerInfo_t::bSak |
To be done.
| uint8_t phNfcLib_PeerInfo_t::bAtqbLength |
To be done.
| uint8_t phNfcLib_PeerInfo_t::aPupi[4] |
To be done.
| uint8_t phNfcLib_PeerInfo_t::aApplicationData[4] |
To be done.
| uint8_t phNfcLib_PeerInfo_t::bIsExtendedAtqb |
To be done.
| uint8_t phNfcLib_PeerInfo_t::aProtocolInfo[4] |
To be done.
| uint8_t* phNfcLib_PeerInfo_t::pUii |
Provides pointer to UII of ISO 18000p3m3 tags detected.
| uint16_t phNfcLib_PeerInfo_t::wUiiLength |
UII length in bits pointed by pUii.
| struct { ... } phNfcLib_PeerInfo_t::tIso14443_4 |
To be done.
| struct { ... } phNfcLib_PeerInfo_t::tIso18092 |
To be done.