Supported ReaderIC commands.
More...
|
| phStatus_t | phhalHw_Rc523_Cmd_Mem (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t *pDataIn, uint8_t bDataLength, uint8_t *pDataOut) |
| | Transfers either 25 bytes into internal buffer or returns 25 bytes from internal buffer. More...
|
| |
| phStatus_t | phhalHw_Rc523_Cmd_GenerateRandomId (phhalHw_Rc523_DataParams_t *pDataParams) |
| | Generates a 10 byte random ID. More...
|
| |
| phStatus_t | phhalHw_Rc523_Cmd_CalcCrc (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t *pData, uint16_t wDataLength, uint16_t *pCrcResult) |
| | Calculates a CRC over the input data and returns the result. More...
|
| |
| phStatus_t | phhalHw_Rc523_Cmd_SoftReset (phhalHw_Rc523_DataParams_t *pDataParams) |
| | Performs a Softreset. More...
|
| |
| phStatus_t | phhalHw_Rc523_SetListenParameters (phhalHw_Rc523_DataParams_t *pDataParams, uint8_t *pSensRes, uint8_t *pNfcId1, uint8_t SelRes, uint8_t *pPollingResp, uint8_t bNfcId3) |
| | Stores data for phhalHw_Autocoll (i.e. More...
|
| |
Supported ReaderIC commands.
§ phhalHw_Rc523_Cmd_Mem()
Transfers either 25 bytes into internal buffer or returns 25 bytes from internal buffer.
If bDataLength equals zero, 25 bytes from the internal buffer are put into pDataOut.
If bDataLength is 25, 25 bytes from pDataIn are copied into the internal buffer.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pDataIn | 25 bytes In-data or ignored if bDataLength equals zero. |
| [in] | bDataLength | Data length. Either zero or 25. |
| [out] | pDataOut | 25 bytes Out-data or ignored if bDataLength is nonzero. |
§ phhalHw_Rc523_Cmd_GenerateRandomId()
Generates a 10 byte random ID.
The generated RandomId is stored in the internal buffer (the first 10 bytes get overridden).
It can be retrieved using the function phhalHw_Rc523_Cmd_Mem.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
§ phhalHw_Rc523_Cmd_CalcCrc()
Calculates a CRC over the input data and returns the result.
Note: The CRC calculation parameters are taken from the respective registers.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pData | CRC input data. |
| [in] | wDataLength | Length of input data. |
| [out] | pCrcResult | Calculated CRC. |
§ phhalHw_Rc523_Cmd_SoftReset()
Performs a Softreset.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
§ phhalHw_Rc523_SetListenParameters()
Stores data for phhalHw_Autocoll (i.e.
phhalHw_Rc523_Autocoll) command into internal buffer.
Note: Only applicable if in Target mode.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pSensRes | 2 bytes. |
| [in] | pNfcId1 | 3 bytes; The first NfcId1 byte is fixed to 08h and the check byte is calculated automatically. |
| [in] | SelRes | 1 byte. |
| [in] | pPollingResp | 2 bytes (shall be 01h, FEh) + 6 bytes NfcId2 + 8 bytes Pad + 2 bytes SystemCode. |
| [in] | bNfcId3 | 1 byte. |