|
NXP NFC Reader Library
v4.040.05.011646
|
Software parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pCryptoDataParams |
| Data parameter structure for the AES engine. | |
| uint32_t | dwRequestCounter |
| Counts the amount of requests between two seeding procedures. More... | |
Software parameter structure.
| uint32_t phCryptoRng_Sw_DataParams_t::dwRequestCounter |
Counts the amount of requests between two seeding procedures.
Note: according to NIST SP800-90 for AES this is 2^48, for storage reasons the limit is set to 2^32 in this particular implementation.