|
NXP NFC Reader Library
v4.040.05.011646
|
Queue structure of Message Queue. More...
Data Fields | |
| void * | pSender |
| Sender of the message. More... | |
| uint8_t * | pbData |
| Content of the message, type of the content is given using bType. More... | |
| uint32_t | dwLength |
| Length of the message. More... | |
| uint8_t | bLlcpBuf [6] |
| Buffer used to store LLCP formatted PDUs that needs to be sent while processing Message Queue. More... | |
| uint8_t | bLlcpData |
| This variable is used to decide if LLCP framed data should be sent or data from application. More... | |
| struct phTools_Q * | pNext |
| Pointer to next element in the list/queue. More... | |
| uint16_t | wFrameOpt |
| Frame Option can take PH_TRANSMIT_DEFAULT, PH_TRANSMIT_BUFFER_FIRST, PH_TRANSMIT_BUFFER_CONT, or PH_TRANSMIT_BUFFER_LAST. More... | |
| uint8_t | bSenderType |
| Type of the sender, used for proper casting of pSender. More... | |
| phTools_Q_Type_t | bType |
| Message content type. More... | |
Queue structure of Message Queue.
| void* phTools_Q::pSender |
Sender of the message.
As this is void pointer pointing to the sender's context, bSenderType determines the actual type of the sender to allow proper casting.
| uint8_t* phTools_Q::pbData |
Content of the message, type of the content is given using bType.
| uint32_t phTools_Q::dwLength |
Length of the message.
| uint8_t phTools_Q::bLlcpBuf[6] |
Buffer used to store LLCP formatted PDUs that needs to be sent while processing Message Queue.
| uint8_t phTools_Q::bLlcpData |
This variable is used to decide if LLCP framed data should be sent or data from application.
| struct phTools_Q* phTools_Q::pNext |
Pointer to next element in the list/queue.
| uint16_t phTools_Q::wFrameOpt |
Frame Option can take PH_TRANSMIT_DEFAULT, PH_TRANSMIT_BUFFER_FIRST, PH_TRANSMIT_BUFFER_CONT, or PH_TRANSMIT_BUFFER_LAST.
| uint8_t phTools_Q::bSenderType |
Type of the sender, used for proper casting of pSender.
| phTools_Q_Type_t phTools_Q::bType |
Message content type.
It can be either data to be sent/received data.