|
NXP NFC Reader Library
v4.040.05.011646
|
Software PAL-I18000P3M3 parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalI18000p3m3DataParams |
| Pointer to the parameter structure of the underlying PAL layer. More... | |
| uint8_t | abHandle [2] |
| Handle retrieved by ReqRn. More... | |
| uint8_t | bHandleValid |
| Whether Handle is valid or not. More... | |
Software PAL-I18000P3M3 parameter structure.
| void* phalI18000p3m3_Sw_DataParams_t::pPalI18000p3m3DataParams |
Pointer to the parameter structure of the underlying PAL layer.
| uint8_t phalI18000p3m3_Sw_DataParams_t::abHandle[2] |
Handle retrieved by ReqRn.
| uint8_t phalI18000p3m3_Sw_DataParams_t::bHandleValid |
Whether Handle is valid or not.