Pn5180 HAL component.
More...
|
| phStatus_t | phhalHw_Pn5180_Init (phhalHw_Pn5180_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pBalDataParams, void *pKeyStoreDataParams, uint8_t *pTxBuffer, uint16_t wTxBufSize, uint8_t *pRxBuffer, uint16_t wRxBufSize) |
| | Initializes the PN5180 HAL component. More...
|
| |
| phStatus_t | phhalHw_Pn5180_SetListenParameters (phhalHw_Pn5180_DataParams_t *pDataParams, uint8_t *pSensRes, uint8_t *pNfcId1, uint8_t bSelRes, uint8_t *pPollingResp, uint8_t bNfcId3) |
| | PN5180 implementation of phhalHw_SetListenParameters. More...
|
| |
Pn5180 HAL component.
§ PHHAL_HW_PN5180_DEFAULT_TIMEOUT
| #define PHHAL_HW_PN5180_DEFAULT_TIMEOUT 150U |
Default timeout in microseconds.
§ phhalHw_Pn5180_Init()
Initializes the PN5180 HAL component.
This function has to be called as part of the initialization of the HAL layer of the application that intends to use the PN517 as the reader IC front end.
- Parameters
-
| [in] | pDataParams | Pointer to data parameter of this HAL layer |
| [in] | wSizeOfDataParams | Size of the data parameter of the structure that was passed |
| [in] | pBalDataParams | Pointer to the lower layer parameter(BAL) structure |
| [in] | pKeyStoreDataParams | Pointer to the parameter structure of the keyStore layer. |
| [in] | pTxBuffer | Pointer to global transmit buffer that will be used by Exchange() |
| [in] | wTxBufSize | size of the global transmit buffer |
| [in] | pRxBuffer | Pointer to global receive buffer that will be used by Exchange() |
| [in] | wRxBufSize | Size of the global receive buffer |
§ phhalHw_Pn5180_SetListenParameters()
PN5180 implementation of phhalHw_SetListenParameters.
- See also
- phhalHw_SetListenParameters
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pSensRes | 2 bytes. |
| [in] | pNfcId1 | 3 bytes; The first NfcId1 byte is fixed to 08h and the check byte is calculated automatically. |
| [in] | bSelRes | 1 byte. |
| [in] | pPollingResp | 2 bytes (shall be 01h, FEh) + 6 bytes NfcId2 + 8 bytes Pad + 2 bytes SystemCode. |
| [in] | bNfcId3 | 1 byte. |