|
NXP NFC Reader Library
v4.040.05.011646
|
Defines parameters that needs be provided by User to communicate with MIFare DESFire card. More...
Data Fields | |
| phNfcLib_MFDF_Commands_t | bCommand |
| [In] Mifare DESFire command needs to be provided. More... | |
| uint8_t | bOptions |
| [In] Option parameter. More... | |
| uint8_t * | pApplicationIdentifier |
| [In] Mifare DESFire AID (Application identifier), 0x000000 is reserved. More... | |
| uint8_t | bKeySettings1 |
| [In] Mifare DESFire KeySetting 1 currently can be only set to 0x0F, as authentication support is not yet provided by Simplified API. More... | |
| uint8_t | bKeySettings2 |
| [In] Mifare DESFire KeySetting 2, bits 6,7 defines the key that will be used, bit 5 indicates if application supports ISO File ID for selection, for whole application and lower nibble defines no of Keys that can be used. More... | |
| uint8_t * | pISOFileId |
| [In] Optional ISO File ID that can be used to Select application using 7816-4 command, Valid only if bit 5 of KeySetting 2 is set to '1'. More... | |
| uint8_t * | pISODFName |
| [In] Optional ISO DF name that can be used to Select application using 7816-4 command, Length of this parameter can be from 1 to 16bytes. More... | |
| uint8_t | bISODFNameLen |
| [In] ISO DF name length provided by User, can take value from 1 to 16bytes. More... | |
| uint8_t | bOption |
| [In] Option parameter. More... | |
| uint8_t | bFileNo |
| [In] File number in the range of 0x00 to 0x1F. More... | |
| uint8_t | bCommSett |
| [In] Communication settings, currently only plain comm is supported with bit 0 set to 0. More... | |
| uint8_t * | pAccessRights |
| [In] Read/Write access rights, currently only free access is supported with all nibbles set to 0xE. More... | |
| uint8_t * | pFileSize |
| [In] File size. More... | |
| uint8_t | bCommOption |
| [In] Communication settings, currently only plain comm is supported (value 0x00). More... | |
| uint8_t * | pOffset |
| [In] Offset from which write operation to be done. More... | |
| uint8_t * | pTxData |
| [In] Pointer to array of data to be written into File. More... | |
| uint8_t * | pTxDataLen |
| [In] Length of data. More... | |
| uint8_t | bSelector |
| [In] P1 field in ISO 7816-4, can take either 0x00 or 0x02 or 0x04. More... | |
| uint8_t * | pFid |
| [In] Elementary File Identifier used to select application when P1 is either 0x00 or 0x02. More... | |
| uint8_t * | pDFname |
| [In] DF name that can be used to Select ISO file. More... | |
| uint8_t | bDFnameLen |
| [In] Length of DF name provided by User, can take value from 1 to 16bytes. More... | |
| uint16_t | wOption |
| [In] Option parameter indicating PH_EXCHANGE_DEFAULT or PH_EXCHANGE_RXCHAINING. More... | |
| uint8_t | bSfid |
| [In] P1 field in ISO 7816-4, if bit 8 is set to zero then p1 indicates MSB of offset else bit5 to bit1 (5bits) indicates short ISO FID. More... | |
| uint8_t | bOffset |
| [In] P2 field in ISO 7816-4, codes offset. More... | |
| uint8_t | bBytesToRead |
| [In] Le field in ISO 7816-4, number of bytes to read from file. More... | |
| uint8_t * | pData |
| [In] Pointer to array data to be written. More... | |
| uint8_t | bDataLen |
| [In] Length of data provided by application. More... | |
| phNfcLib_MFDF_Commands_t phNfcLib_MFdf::bCommand |
[In] Mifare DESFire command needs to be provided.
| uint8_t phNfcLib_MFdf::bOptions |
[In] Option parameter.
| uint8_t* phNfcLib_MFdf::pApplicationIdentifier |
[In] Mifare DESFire AID (Application identifier), 0x000000 is reserved.
[In] Mifare DESFire AID (Application identifier) to select file.
| uint8_t phNfcLib_MFdf::bKeySettings1 |
[In] Mifare DESFire KeySetting 1 currently can be only set to 0x0F, as authentication support is not yet provided by Simplified API.
| uint8_t phNfcLib_MFdf::bKeySettings2 |
[In] Mifare DESFire KeySetting 2, bits 6,7 defines the key that will be used, bit 5 indicates if application supports ISO File ID for selection, for whole application and lower nibble defines no of Keys that can be used.
| uint8_t* phNfcLib_MFdf::pISOFileId |
[In] Optional ISO File ID that can be used to Select application using 7816-4 command, Valid only if bit 5 of KeySetting 2 is set to '1'.
[In] Optional ISO File ID that can be used to select file using 7816-4 command.
| uint8_t* phNfcLib_MFdf::pISODFName |
[In] Optional ISO DF name that can be used to Select application using 7816-4 command, Length of this parameter can be from 1 to 16bytes.
| uint8_t phNfcLib_MFdf::bISODFNameLen |
[In] ISO DF name length provided by User, can take value from 1 to 16bytes.
| uint8_t phNfcLib_MFdf::bOption |
[In] Option parameter.
[In] P2 field in ISO 7816-4, when 0x00 FCI stored in file will be returned.
when 0x0C FCI shall not be returned. Any other value is invalid.
| uint8_t phNfcLib_MFdf::bFileNo |
[In] File number in the range of 0x00 to 0x1F.
| uint8_t phNfcLib_MFdf::bCommSett |
[In] Communication settings, currently only plain comm is supported with bit 0 set to 0.
| uint8_t* phNfcLib_MFdf::pAccessRights |
[In] Read/Write access rights, currently only free access is supported with all nibbles set to 0xE.
| uint8_t* phNfcLib_MFdf::pFileSize |
[In] File size.
| uint8_t phNfcLib_MFdf::bCommOption |
[In] Communication settings, currently only plain comm is supported (value 0x00).
| uint8_t* phNfcLib_MFdf::pOffset |
[In] Offset from which write operation to be done.
| uint8_t* phNfcLib_MFdf::pTxData |
[In] Pointer to array of data to be written into File.
| uint8_t* phNfcLib_MFdf::pTxDataLen |
[In] Length of data.
| uint8_t phNfcLib_MFdf::bSelector |
[In] P1 field in ISO 7816-4, can take either 0x00 or 0x02 or 0x04.
| uint8_t* phNfcLib_MFdf::pFid |
[In] Elementary File Identifier used to select application when P1 is either 0x00 or 0x02.
| uint8_t* phNfcLib_MFdf::pDFname |
[In] DF name that can be used to Select ISO file.
| uint8_t phNfcLib_MFdf::bDFnameLen |
[In] Length of DF name provided by User, can take value from 1 to 16bytes.
| uint16_t phNfcLib_MFdf::wOption |
[In] Option parameter indicating PH_EXCHANGE_DEFAULT or PH_EXCHANGE_RXCHAINING.
| uint8_t phNfcLib_MFdf::bSfid |
[In] P1 field in ISO 7816-4, if bit 8 is set to zero then p1 indicates MSB of offset else bit5 to bit1 (5bits) indicates short ISO FID.
| uint8_t phNfcLib_MFdf::bOffset |
[In] P2 field in ISO 7816-4, codes offset.
| uint8_t phNfcLib_MFdf::bBytesToRead |
[In] Le field in ISO 7816-4, number of bytes to read from file.
| uint8_t* phNfcLib_MFdf::pData |
[In] Pointer to array data to be written.
| uint8_t phNfcLib_MFdf::bDataLen |
[In] Length of data provided by application.