|
NXP NFC Reader Library
v4.040.05.011646
|
Defines parameters that needs be provided by User to communicate with ISO 18000p3m3 card. More...
Data Fields | |
| phNfcLib_I18000_Commands_t | bCommand |
| [In] ISO-IEC 18000-p3m3 command needs to be provided. More... | |
| uint8_t | bOption |
| [In] Options that can provided for Write, Kill and Access. More... | |
| uint8_t | bMemBank |
| [In] Memory bank being addressed. More... | |
| uint8_t | bReadLock |
| [In] Indicates if BlockPermaLock should read (bit 0) or lock (bit 1) the block. More... | |
| uint8_t * | pWordPtr |
| [In] Pointer to starting address for Read. More... | |
| uint8_t | bWordPtrLength |
| [In] Should indicate length of pWordPtr provided by User. More... | |
| uint8_t | bWordCount |
| [In] Number of 16-bit words to be Read or BlockWrite. More... | |
| uint8_t * | pPassword |
| [In] Pointer to 4 bytes of password used by Kill and Access command to put the Tag into killed or secured state respectively. More... | |
| uint8_t | bRecom |
| [In] Recommission Option - 3 bit significant, Option 0x04 is mandatory implementation rest is optional . More... | |
| uint8_t * | pMask |
| [In] Mask specifies which memory blocks a tag PermaLocks. More... | |
| uint8_t * | pAction |
| [In] Action specifies teh action to be perfomed for Lock on the given Mask. More... | |
| uint8_t * | pBlockPtr |
| [In] Pointer to starting address for BlockPermaLock. More... | |
| uint8_t | bBlockPtrLength |
| [In] Should indicate length of pBlockPtr provided by User. More... | |
| uint8_t | bBlockRange |
| [In] Specifies range of Mask, starting at BlockPtr and ending (16�BlockRange)�1 blocks later to starting address for BlockPermaLock. More... | |
| uint8_t * | pHandle |
| [In] Pointer to the 2 byte handle of the tag. More... | |
| uint8_t * | pUii |
| [In] Pointer to the UII Mem bank of the tag, could be at max 58 bytes data . More... | |
| uint8_t | wUiiMaskLength |
| [In] Length of the UII Membank data received . More... | |
| uint8_t * | pBuffer |
| [In] Pointer to 16bit or multiple of 16bit data that needs to be written on Tag. More... | |
| phNfcLib_I18000_Commands_t phNfcLib_I18000p3m3::bCommand |
[In] ISO-IEC 18000-p3m3 command needs to be provided.
| uint8_t phNfcLib_I18000p3m3::bOption |
[In] Options that can provided for Write, Kill and Access.
Refer nfc_lib_18000p3m3_options Options
| uint8_t phNfcLib_I18000p3m3::bMemBank |
[In] Memory bank being addressed.
Valid memory bank are 0, 1, 2 and 3.
| uint8_t phNfcLib_I18000p3m3::bReadLock |
[In] Indicates if BlockPermaLock should read (bit 0) or lock (bit 1) the block.
| uint8_t* phNfcLib_I18000p3m3::pWordPtr |
[In] Pointer to starting address for Read.
Shall be of 8, 16, 24, 32 bit length.
| uint8_t phNfcLib_I18000p3m3::bWordPtrLength |
[In] Should indicate length of pWordPtr provided by User.
Valid values are 0, 1, 2 and 3.
| uint8_t phNfcLib_I18000p3m3::bWordCount |
[In] Number of 16-bit words to be Read or BlockWrite.
| uint8_t* phNfcLib_I18000p3m3::pPassword |
[In] Pointer to 4 bytes of password used by Kill and Access command to put the Tag into killed or secured state respectively.
| uint8_t phNfcLib_I18000p3m3::bRecom |
[In] Recommission Option - 3 bit significant, Option 0x04 is mandatory implementation rest is optional .
| uint8_t* phNfcLib_I18000p3m3::pMask |
[In] Mask specifies which memory blocks a tag PermaLocks.
| uint8_t* phNfcLib_I18000p3m3::pAction |
[In] Action specifies teh action to be perfomed for Lock on the given Mask.
| uint8_t* phNfcLib_I18000p3m3::pBlockPtr |
[In] Pointer to starting address for BlockPermaLock.
Shall be of 8, 16, 24, 32 bit length.
| uint8_t phNfcLib_I18000p3m3::bBlockPtrLength |
[In] Should indicate length of pBlockPtr provided by User.
Valid values are 0, 1, 2 and 3.
| uint8_t phNfcLib_I18000p3m3::bBlockRange |
[In] Specifies range of Mask, starting at BlockPtr and ending (16�BlockRange)�1 blocks later to starting address for BlockPermaLock.
If 0x00 then tag ignore the BlockPermalock command.
| uint8_t* phNfcLib_I18000p3m3::pHandle |
[In] Pointer to the 2 byte handle of the tag.
| uint8_t* phNfcLib_I18000p3m3::pUii |
[In] Pointer to the UII Mem bank of the tag, could be at max 58 bytes data .
| uint8_t phNfcLib_I18000p3m3::wUiiMaskLength |
[In] Length of the UII Membank data received .
| uint8_t* phNfcLib_I18000p3m3::pBuffer |
[In] Pointer to 16bit or multiple of 16bit data that needs to be written on Tag.