|
NXP NFC Reader Library
v4.040.05.011646
|
T5T parameter structure. More...
Data Fields | |
| void * | pAlI15693DataParams |
| Pointer to T5T data parameters. | |
| uint8_t | bRwa |
| Tag read/write size. | |
| uint8_t | bTerminatorTlvPresence |
| Terminator TLV presence; 1 -present, 0 - not present. | |
| uint8_t | bMbRead |
| Flag Bit for Multiple Read support. | |
| uint8_t | bLockBlock |
| Flag Bit for Lock Command support. | |
| uint8_t | bSplFrm |
| Flag Bit for special frame support. | |
| uint8_t | bExtendedCommandSupport |
| Flag Bit for Extended Command Support support. | |
| uint8_t | bOptionFlag |
| Option Flag PH_ON = Enable, PH_OFF = Disable. | |
| uint16_t | wMlen |
| Tag Memory size. | |
| uint16_t | wNdefHeaderAddr |
| Header offset of first NDEF message. | |
| uint16_t | wNdefMsgAddr |
| NDEF message start address. | |
| uint16_t | bBlockSize |
| T5T Block Size supported by card. | |
| uint16_t | bMaxBlockNum |
| Maximum Block number supported by Card. | |
T5T parameter structure.