|
NXP NFC Reader Library
v4.040.05.011646
|
|
Data Structures | |
| struct | phalT1T_Sw_DataParams_t |
| Private parameter structure. More... | |
Macros | |
| #define | PHAL_T1T_SW_ID 0x01U |
| ID for Software T1T layer. | |
Functions | |
| phStatus_t | phalT1T_Sw_Init (phalT1T_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pPalI14443p3aDataParams) |
| Initialise this layer. More... | |
| phStatus_t phalT1T_Sw_Init | ( | phalT1T_Sw_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| void * | pPalI14443p3aDataParams | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | Specifies the size of the data parameter structure. |
| [in] | pPalI14443p3aDataParams | Pointer to the parameter structure of the underlying ISO14443-3 layer. |