Contains definitions for types defined within NxpRdLib.
More...
|
|
typedef unsigned char | uint8_t |
| | 8 bit unsigned integer
|
| |
|
typedef unsigned short | uint16_t |
| | 16 bit unsigned integer
|
| |
|
typedef unsigned int | uint32_t |
| | 32 bit and 64 bit unsigned integers
|
| |
|
typedef unsigned long long | uint64_t |
| |
|
#define | __uint8_t_defined |
| |
|
#define | __uint16_t_defined |
| |
|
#define | __uint32_t_defined |
| |
|
|
typedef signed char | int8_t |
| | 8 bit signed integer
|
| |
|
typedef short | int16_t |
| | 16 bit signed integer
|
| |
|
typedef int | int32_t |
| | 32 bit signed integer
|
| |
|
#define | __int8_t_defined |
| |
|
#define | __int16_t_defined |
| |
|
#define | __int32_t_defined |
| |
|
|
typedef float | float32_t |
| | 32 bit floating point
|
| |
|
#define | __float32_t_defined |
| |
Contains definitions for types defined within NxpRdLib.