|
NXP NFC Reader Library
v4.040.05.011646
|
NFC Type 4A Tag card emulation parameter structure. More...
Data Fields | |
| uint16_t | wId |
| ID for this component, not to be modified by user. More... | |
| uint16_t | wStatusWord |
| Status Word (SW1 and SW2) as per ISO 7816-4 (Example: 0x9000 indicates SUCCESS). More... | |
| uint16_t | wLc |
| Lc field of received C-APDU (Command Application Protocol Data Unit). More... | |
| uint16_t | wAppBufferSize |
| Size of application buffer. More... | |
| uint8_t * | pAppBuffer |
| Application buffer. More... | |
| uint8_t * | pNdefFile |
| NDEF file pointer. More... | |
| uint32_t | dwNdefFileSize |
| NDEF file size. More... | |
| uint8_t * | pCcFile |
| CC (Capability Container) file pointer. More... | |
| uint16_t | wCcFileSize |
| CC (Capability Container) file size. More... | |
| uint16_t | wCcContentLen |
| CC (Capability Container) file content length. More... | |
| uint8_t * | pSelectedFile |
| Pointer to currently selected file. More... | |
| uint32_t | dwFileSize |
| Size of currently selected file. More... | |
| uint32_t | dwFileOffset |
| Offset for selected file. More... | |
| uint16_t | wSelectedFileId |
| ID of currently selected file. More... | |
| uint8_t | bFileWriteAccess |
| Write access of currently selected file. More... | |
| uint8_t | bTagState |
| Current state of tag. More... | |
| void * | pPalI14443p4mCDataParams |
| Pointer to ISO 14443p4mC PAL data parameter structure. More... | |
| uint8_t * | pSharedData |
| Shared data buffer. More... | |
| uint16_t | wSharedDataLen |
| Length of shared data in phceT4T_Sw_DataParams::pSharedData. More... | |
| uint8_t | bRxOption |
| Indicates the data received option. More... | |
| uint8_t | bSupportProprietaryCmd |
| Indicates support for proprietary commands. More... | |
| uint8_t | bHandleUpdateCmd |
| Indicates handling of UPDATE BINARY command by phceT4T_Activate and phceT4T_ProcessCmd. More... | |
| uint16_t | wExitStatus |
| Used to share the exit status (error code) between reader library thread and application thread in multi-threaded environment. More... | |
| phOsal_EventObj_t | T4TEventObj |
| Event Object. More... | |
NFC Type 4A Tag card emulation parameter structure.
| uint16_t phceT4T_Sw_DataParams::wId |
ID for this component, not to be modified by user.
This is initialized with PHCE_T4T_SW_ID in the initialization function phceT4T_Sw_Init. This is used for validating the data parameter structure and to make sure that APIs are called after initialization.
| uint16_t phceT4T_Sw_DataParams::wStatusWord |
Status Word (SW1 and SW2) as per ISO 7816-4 (Example: 0x9000 indicates SUCCESS).
This will be updated after successful processing of received C-APDU (Command Application Protocol Data Unit). This Status Word is send as the last 2 bytes of Response Application Protocol Data Unit (R-APDU).
| uint16_t phceT4T_Sw_DataParams::wLc |
Lc field of received C-APDU (Command Application Protocol Data Unit).
This indicates the length of command data field. This parameter is updated and used only for UPDATE BINARY command.
| uint16_t phceT4T_Sw_DataParams::wAppBufferSize |
Size of application buffer.
Holds the size of application buffer (phceT4T_Sw_DataParams::pAppBuffer) provided in the initialization function phceT4T_Sw_Init. Application buffer size should be at least equal to the HAL receive buffer.
| uint8_t* phceT4T_Sw_DataParams::pAppBuffer |
Application buffer.
Holds the application buffer provided in the initialization function phceT4T_Sw_Init. This buffer is used to copy and keep the received data to avoid data loss in case of WTX (Waiting Time eXtension).
| uint8_t* phceT4T_Sw_DataParams::pNdefFile |
NDEF file pointer.
Holds the pointer to application provided NDEF file. Application can set the NDEF file using phceT4T_SetElementaryFile with file type as PHCE_T4T_FILE_NDEF.
| uint32_t phceT4T_Sw_DataParams::dwNdefFileSize |
NDEF file size.
Holds the size of application provided NDEF file. Application can set the NDEF file and file size using phceT4T_SetElementaryFile with file type as PHCE_T4T_FILE_NDEF.
| uint8_t* phceT4T_Sw_DataParams::pCcFile |
CC (Capability Container) file pointer.
Holds the pointer to application provided CC file. Application can set the CC file using phceT4T_SetElementaryFile with file type as PHCE_T4T_FILE_CC.
| uint16_t phceT4T_Sw_DataParams::wCcFileSize |
CC (Capability Container) file size.
Holds the size of application provided CC file. Application can set the CC file and file size using phceT4T_SetElementaryFile with file type as PHCE_T4T_FILE_CC.
| uint16_t phceT4T_Sw_DataParams::wCcContentLen |
CC (Capability Container) file content length.
Holds the content length of application provided CC file. Application can set the CC file and content length using phceT4T_SetElementaryFile with file type as PHCE_T4T_FILE_CC. Content length specifies the length of valid content inside file. For CC file the valid content length values supported by phceT4T_SetElementaryFile are:
| uint8_t* phceT4T_Sw_DataParams::pSelectedFile |
Pointer to currently selected file.
Holds the pointer to the currently selected file. This will be updated after processing a valid FILE SELECT command. The pointer to the file selected by the SELECT command is updated here.
| uint32_t phceT4T_Sw_DataParams::dwFileSize |
Size of currently selected file.
Holds the size of currently selected file. This will be updated after processing a valid FILE SELECT command. The size of file selected by the SELECT command is updated here.
| uint32_t phceT4T_Sw_DataParams::dwFileOffset |
Offset for selected file.
Holds the offset of currently selected file. This will be updated after processing a valid UPDATE BINARY command. The offset of file specified in the UPDATE BINARY command is updated here. After updating the file this will be updated with the file offset till where update happened successfully.
| uint16_t phceT4T_Sw_DataParams::wSelectedFileId |
ID of currently selected file.
Holds the ID of the currently selected file. This will be updated after processing a valid FILE SELECT command. The ID of file selected by the SELECT command is updated here.
| uint8_t phceT4T_Sw_DataParams::bFileWriteAccess |
Write access of currently selected file.
Holds the write access of the currently selected file. This will be updated after processing a valid FILE SELECT command. The write access of file selected by the SELECT command is updated here.
| uint8_t phceT4T_Sw_DataParams::bTagState |
Current state of tag.
The supported values of tag state are:
| void* phceT4T_Sw_DataParams::pPalI14443p4mCDataParams |
Pointer to ISO 14443p4mC PAL data parameter structure.
Holds the pointer to ISO 14443p4mC PAL data parameter structure specified by application in the initialization function phceT4T_Sw_Init.
| uint8_t* phceT4T_Sw_DataParams::pSharedData |
Shared data buffer.
Used to share data between reader library thread and application thread in multi-threaded environment. Pointer to the data to be send to another thread is copied to this variable and shared.
| uint16_t phceT4T_Sw_DataParams::wSharedDataLen |
Length of shared data in phceT4T_Sw_DataParams::pSharedData.
Used to share data between reader library thread and application thread in multi-threaded environment. Length of data to be send to another thread is copied to this variable and shared.
| uint8_t phceT4T_Sw_DataParams::bRxOption |
Indicates the data received option.
This specifies if the received data is complete or chaining. The supported options are:
If UPDATE BINARY and/or proprietary commands are handled by application callback, then value of this option is send to application callback through wRxOption parameter of phceT4T_AppCallback_t.
| uint8_t phceT4T_Sw_DataParams::bSupportProprietaryCmd |
Indicates support for proprietary commands.
By default the proprietary command support is disabled. If proprietary command support is disabled then unsupported command status word is send back to reader.
Use phceT4T_SetConfig with PHCE_T4T_CONFIG_RECEIVE_PROPRIETARY option to enable/disable (PH_ON or PH_OFF) support for proprietary commands.
| uint8_t phceT4T_Sw_DataParams::bHandleUpdateCmd |
Indicates handling of UPDATE BINARY command by phceT4T_Activate and phceT4T_ProcessCmd.
By default the handling of UPDATE BINARY by phceT4T_Activate and phceT4T_ProcessCmd is disabled (PH_OFF). If UPDATE BINARY is handled, WTX can not be handled. If application don't want handling of UPDATE BINARY using a separate application thread (like in single threaded environment with no RTOS), application can enable (PH_ON) this option.
Use phceT4T_SetConfig with PHCE_T4T_CONFIG_HANDLE_UPDATEBINARY option to enable/disable (PH_ON or PH_OFF) this option.
| uint16_t phceT4T_Sw_DataParams::wExitStatus |
Used to share the exit status (error code) between reader library thread and application thread in multi-threaded environment.
This contains the return status from lower layers or error occurred in this layer when phceT4T_Activate exits.
| phOsal_EventObj_t phceT4T_Sw_DataParams::T4TEventObj |
Event Object.