|
NXP NFC Reader Library
v4.040.05.011646
|
ISO18092 mode passive target parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY. | |
| void * | pHalDataParams |
| Pointer to the parameter structure of underlying hardware component. | |
| void * | pPlatform |
| Pointer to OSAL layer. More... | |
| void * | ovrTask |
| Task context. More... | |
| void * | pTimerHandle |
| Timer Handle (For RTOX). More... | |
| pRtoxTimerCallback | pRtoxCallback |
| Holds RTOX Callback function address. | |
| uint16_t | wLastTxLen |
| Last successful DEP send length. More... | |
| uint8_t | aNfcid3i [PHPAL_I18092MT_NFCID3_LENGTH] |
| Array holding 10 bytes long NFCID3. More... | |
| uint8_t | aNfcid3t [PHPAL_I18092MT_NFCID3_LENGTH] |
| Array holding 10 bytes long NFCID3 of the PCD. More... | |
| uint8_t | bStateNow |
| Current Exchange-State. More... | |
| uint8_t | bDid |
| Device Identifier; '0' to disable usage else 1-14. More... | |
| uint8_t | bNadEnabled |
| Indicates presence of Node Address. More... | |
| uint8_t | bNadVal |
| Node Address; Ignored if bNadEnabled is equal '0'. More... | |
| uint8_t | bFsl |
| Frame Length Byte; 0-3. More... | |
| uint8_t | bPni |
| Current Packet Number (Packet number information); 0-3. More... | |
| uint8_t | bDst |
| Divisor Send Integer; 0-2. More... | |
| uint8_t | bDrt |
| Divisor Receive Integer; 0-2. More... | |
| uint8_t | bBsi |
| Send bit-rate supported by the PCD. More... | |
| uint8_t | bBri |
| Receive bit-rate supported by the PCD. More... | |
| uint8_t | bLri |
| Length reduction value is stored here. More... | |
| uint8_t | bBst |
| Send bit-rate supported by the PCD. More... | |
| uint8_t | bBrt |
| Receive bit-rate supported by the PCD. More... | |
| uint8_t | bLrt |
| Length reduction value is stored here. More... | |
| uint8_t | bTo |
| Hold the time out value. More... | |
| uint8_t | bRtoxDisabled |
| RTOX Disabler (i.e. More... | |
| uint8_t | bRtoxExtnVal |
| Response timeout extension value. More... | |
| uint8_t | bCmdtype |
| Holds the type of Command send by target. More... | |
| phOsal_EventObj_t | Pal18092mTEventObj |
| Handle for Event. More... | |
ISO18092 mode passive target parameter structure.
| void* phpalI18092mT_Sw_DataParams_t::pPlatform |
Pointer to OSAL layer.
| void* phpalI18092mT_Sw_DataParams_t::ovrTask |
Task context.
| void* phpalI18092mT_Sw_DataParams_t::pTimerHandle |
Timer Handle (For RTOX).
| uint16_t phpalI18092mT_Sw_DataParams_t::wLastTxLen |
Last successful DEP send length.
| uint8_t phpalI18092mT_Sw_DataParams_t::aNfcid3i[PHPAL_I18092MT_NFCID3_LENGTH] |
Array holding 10 bytes long NFCID3.
| uint8_t phpalI18092mT_Sw_DataParams_t::aNfcid3t[PHPAL_I18092MT_NFCID3_LENGTH] |
Array holding 10 bytes long NFCID3 of the PCD.
| uint8_t phpalI18092mT_Sw_DataParams_t::bStateNow |
Current Exchange-State.
| uint8_t phpalI18092mT_Sw_DataParams_t::bDid |
Device Identifier; '0' to disable usage else 1-14.
| uint8_t phpalI18092mT_Sw_DataParams_t::bNadEnabled |
Indicates presence of Node Address.
1 = present.
| uint8_t phpalI18092mT_Sw_DataParams_t::bNadVal |
Node Address; Ignored if bNadEnabled is equal '0'.
| uint8_t phpalI18092mT_Sw_DataParams_t::bFsl |
Frame Length Byte; 0-3.
| uint8_t phpalI18092mT_Sw_DataParams_t::bPni |
Current Packet Number (Packet number information); 0-3.
| uint8_t phpalI18092mT_Sw_DataParams_t::bDst |
Divisor Send Integer; 0-2.
| uint8_t phpalI18092mT_Sw_DataParams_t::bDrt |
Divisor Receive Integer; 0-2.
| uint8_t phpalI18092mT_Sw_DataParams_t::bBsi |
Send bit-rate supported by the PCD.
| uint8_t phpalI18092mT_Sw_DataParams_t::bBri |
Receive bit-rate supported by the PCD.
| uint8_t phpalI18092mT_Sw_DataParams_t::bLri |
Length reduction value is stored here.
| uint8_t phpalI18092mT_Sw_DataParams_t::bBst |
Send bit-rate supported by the PCD.
| uint8_t phpalI18092mT_Sw_DataParams_t::bBrt |
Receive bit-rate supported by the PCD.
| uint8_t phpalI18092mT_Sw_DataParams_t::bLrt |
Length reduction value is stored here.
| uint8_t phpalI18092mT_Sw_DataParams_t::bTo |
Hold the time out value.
| uint8_t phpalI18092mT_Sw_DataParams_t::bRtoxDisabled |
RTOX Disabler (i.e.
'0' if RTOX enabled).
| uint8_t phpalI18092mT_Sw_DataParams_t::bRtoxExtnVal |
Response timeout extension value.
| uint8_t phpalI18092mT_Sw_DataParams_t::bCmdtype |
Holds the type of Command send by target.
| phOsal_EventObj_t phpalI18092mT_Sw_DataParams_t::Pal18092mTEventObj |
Handle for Event.