|
NXP NFC Reader Library
v4.040.05.011646
|
Controls build behaviour of components. More...
|
Macros | |
| #define | NXPBUILD__PHBAL_REG |
| < DEBUG build definition More... | |
| #define | NXPBUILD__PHHAL_HW |
| Generic HAL definition. | |
| #define | NXPBUILD__PHPAL_I14443P3A |
| Generic PAL ISO 14443-3A definition. | |
| #define | NXPBUILD__PHPAL_I14443P3B |
| Generic PAL ISO 14443-3B definition. | |
| #define | NXPBUILD__PHPAL_I14443P4A |
| Generic PAL ISO 14443-4A definition. | |
| #define | NXPBUILD__PHPAL_I14443P4 |
| Generic PAL ISO 14443-4 definition. | |
| #define | NXPBUILD__PHPAL_I14443P4MC |
| Generic PAL ISO 18092 target definition. | |
| #define | NXPBUILD__PHPAL_MIFARE |
| Generic PAL MIFARE definition. | |
| #define | NXPBUILD__PHPAL_SLI15693 |
| Generic PAL Sli 15693 definition. | |
| #define | NXPBUILD__PHPAL_FELICA |
| < Enable handling of multiple Felica card response More... | |
| #define | NXPBUILD__PHPAL_EPCUID |
| Generic PAL ICode EPC/UID definition. | |
| #define | NXPBUILD__PHPAL_I18000P3M3 |
| Generic PAL I18000p3m3 definition. | |
| #define | NXPBUILD__PHPAL_I18092MPI |
| Generic PAL ISO 18092 definition. | |
| #define | NXPBUILD__PHPAL_I18092MT |
| Generic PAL ISO 18092 target definition. | |
| #define | NXPBUILD__PHAC_DISCLOOP |
| Generic dicovery loop component. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TAGS |
| Detect Passive TypeA Tags/Peers. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_TAGS |
| Detect TypeB Tags. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TARGET |
| Configure Target Mode. | |
| #define | NXPBUILD__PH_OSAL |
| Generic OSAL definition. | |
| #define | NXPBUILD__PHAL_FELICA |
| Generic AL Felica definition. | |
| #define | NXPBUILD__PHAL_MFC |
| Generic AL MIFARE Classic definition. | |
| #define | NXPBUILD__PHAL_MFDF |
| Generic AL MIFARE Desfire definition. | |
| #define | NXPBUILD__PHAL_MFUL |
| Generic AL MIFARE Ultralight definition. | |
| #define | NXPBUILD__PHAL_T1T |
| Generic AL Type 1 Tag definition. | |
| #define | NXPBUILD__PHAL_TOP |
| Generic AL Tag Operations. | |
| #define | NXPBUILD__PHCE_T4T |
| Generic HCE. | |
| #define | NXPBUILD__PHAL_I15693 |
| Generic AL I15693 definition. | |
| #define | NXPBUILD__PHAL_SLI |
| Generic AL Sli definition. | |
| #define | NXPBUILD__PHAL_I18000P3M3 |
| Generic AL I18000p3m3 definition. | |
| #define | NXPBUILD__PH_CIDMANAGER |
| Generic CID Manager definition. | |
| #define | NXPBUILD__PH_CRYPTOSYM |
| Generic Crypto Sym definition. | |
| #define | NXPBUILD__PH_CRYPTORNG |
| Generic CryptoRng definition. | |
| #define | NXPBUILD__PH_KEYSTORE |
| Generic KeyStore definition. | |
| #define | NXPBUILD__PHLN_LLCP |
| Generic Link layer definition. | |
| #define | NXPBUILD__PHNP_SNEP |
| Generic HAL definition. | |
| #define | NXPBUILD__PH_KINETIS |
| Kinetis. | |
| #define | NXPBUILD__PH_PLATFORM |
| < DEBUG build definition More... | |
| #define | NXPBUILD__PH_PLATFORM |
| < DEBUG build definition More... | |
| #define | NXPBUILD__PH_KINETIS_K82 |
| K82 Freedom Board. | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PH_LPC1769 |
| Host Controller LPC1769. More... | |
| #define | NXPBUILD__PH_LPC1769 |
| Host Controller LPC1769. More... | |
| #define | NXPBUILD__PH_LPC11U68 |
| Host Controller LPC11U68. More... | |
| #define | NXPBUILD__PH_LPC11U68 |
| Host Controller LPC11U68. More... | |
| #define | NXPBUILD__PH_RASPBERRY_PI |
| Host Controller RaspBerry Pi. More... | |
| #define | NXPBUILD__PH_RASPBERRY_PI |
| Host Controller RaspBerry Pi. More... | |
| #define | NXPBUILD__PH_UDOO_NEO |
| Host Controller udoo-neo. | |
| #define | NXPBUILD__PH_OSAL_LINUX |
| OSAL Implementation of POSIX is included. More... | |
| #define | NXPBUILD__PH_OSAL_LINUX |
| OSAL Implementation of POSIX is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_FREERTOS |
| OSAL Implementation of Free RTOS is included. More... | |
| #define | NXPBUILD__PH_OSAL_FREERTOS |
| OSAL Implementation of Free RTOS is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
| LPCOpenStack SPI BAL Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
| LPCOpenStack SPI BAL Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
| LPCOpenStack SPI I2C Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
| LPCOpenStack SPI I2C Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_PI_SPI |
| Raspberry Linux UM/KM SPI BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_SPI |
| Raspberry Linux UM/KM SPI BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_I2C |
| Raspberry Linux UM I2C BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_I2C |
| Raspberry Linux UM I2C BAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_RC523 |
| RC523 HAL Component is included. More... | |
| #define | NXPBUILD__PHHAL_HW_RC523 |
| RC523 HAL Component is included. More... | |
| #define | NXPBUILD__PHHAL_HW_RC663 |
| RC663 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_RC663 |
| RC663 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_PN5180 |
| PN5180 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_PN5180 |
| PN5180 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_TARGET |
| Dependency checking if target mode macros should be enabled. | |
| #define | NXPBUILD__PHHAL_HW_TARGET |
| Dependency checking if target mode macros should be enabled. | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_SLI15693_SW |
| PAL SLI 15693 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18000P3M3_SW |
| PAL ISO 18000p3m3 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18000P3M3_SW |
| PAL ISO 18000p3m3 Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_LPCD |
| SRC to enable LPCD is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_LPCD |
| SRC to enable LPCD is included. More... | |
| #define | NXPBUILD__PHAL_I18000P3M3_SW |
| AL ISO18000p3m3 SW Component is included. | |
| #define | NXPBUILD__PHAL_I18000P3M3_SW |
| AL ISO18000p3m3 SW Component is included. | |
| #define | NXPBUILD__PHCE_T4T_SW |
| AL HCE T2AT SW Component is included. | |
| #define | NXPBUILD__PHPAL_I18092MPI_SW |
| PAL ISO18092 (P2P) SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MPI_SW |
| PAL ISO18092 (P2P) SW Component is included. More... | |
| #define | NXPBUILD__PHLN_LLCP_SW |
| Link LLCP SW Component is included. | |
| #define | NXPBUILD__PHPAL_I14443P3A_SW |
| PAL ISO 14443-3A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P3B_SW |
| PAL ISO 14443-3B SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4A_SW |
| PAL ISO 14443-4A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4_SW |
| PAL ISO 14443-4 SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_MIFARE_SW |
| PAL MIFARE SW Component is included. | |
| #define | NXPBUILD__PHPAL_FELICA_SW |
| PAL Felica SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_EPCUID_SW |
| < If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_SW |
| Discovery Loop Activity SW Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
| SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
| SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
| SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
| SRC/DATA to Detect FeliCa Cards is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P3B_TAGS |
| SRC/DATA to Detect Type B Cards that operate at Layer3 level is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P4B_TAGS |
| SRC/DATA to Detect Type B Cards such as NFC Forum Type 4 Tags, EMVCo Type B Cards etc is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS |
| SRC/DATA to Detect Type V Cards such as ICODE SLI/SLIX/SLI2/Tesa Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS |
| SRC/DATA to Detect ICODE ILT Cards such as SMARTRAC StackIt Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
| SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
| SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
| SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
| SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
| SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
| SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHNFCLIB |
| Simplified API Interface, If enabling this the entry point should be this component in the application. | |
| #define | NXPBUILD__PH_CIDMANAGER_SW |
| CID Manager SW Component is included. More... | |
| #define | NXPBUILD__PH_KEYSTORE_SW |
| SW KeyStore Component is included. More... | |
| #define | NXPBUILD__PH_CRYPTOSYM_SW |
| Crypto Symbols SW Component is included. More... | |
| #define | NXPBUILD__PH_CRYPTORNG_SW |
| Crypto RNG SW Component is included. More... | |
| #define | NXPBUILD__PHAL_FELICA_SW |
| AL FeliCa SW Component is included. | |
| #define | NXPBUILD__PHAL_MFC_SW |
| AL Mifare Classic SW Component is included. | |
| #define | NXPBUILD__PHAL_MFUL_SW |
| AL Mifare Ultrlight SW Component is included. | |
| #define | NXPBUILD__PHAL_MFDF_SW |
| AL Mifare DesFire SW Component is included. | |
| #define | NXPBUILD__PHAL_T1T_SW |
| AL Type T1 Tag SW Component is included. | |
| #define | NXPBUILD__PHAL_I15693_SW |
| AL ISO 15693 SW Component is included. | |
| #define | NXPBUILD__PHAL_SLI_SW |
| AL SLI SW Component is included. | |
| #define | NXPBUILD__PHAL_TOP_SW |
| AL for TagOps Mapping SW Component is included.Required for NDEF operations. | |
| #define | NXPBUILD__PHNP_SNEP_SW |
| Protocol SNEP SW Component is included. | |
| #define | NXPBUILD__PH_PLATFORM |
| < DEBUG build definition More... | |
| #define | NXPBUILD__PH_PLATFORM |
| < DEBUG build definition More... | |
| #define | NXPBUILD__PH_KINETIS_K82 |
| K82 Freedom Board. | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PHHAL_HW_PN7462AU |
| NFC Controller PN7462AU HAL. More... | |
| #define | NXPBUILD__PH_LPC1769 |
| Host Controller LPC1769. More... | |
| #define | NXPBUILD__PH_LPC1769 |
| Host Controller LPC1769. More... | |
| #define | NXPBUILD__PH_LPC11U68 |
| Host Controller LPC11U68. More... | |
| #define | NXPBUILD__PH_LPC11U68 |
| Host Controller LPC11U68. More... | |
| #define | NXPBUILD__PH_RASPBERRY_PI |
| Host Controller RaspBerry Pi. More... | |
| #define | NXPBUILD__PH_RASPBERRY_PI |
| Host Controller RaspBerry Pi. More... | |
| #define | NXPBUILD__PH_UDOO_NEO |
| Host Controller udoo-neo. | |
| #define | NXPBUILD__PH_OSAL_LINUX |
| OSAL Implementation of POSIX is included. More... | |
| #define | NXPBUILD__PH_OSAL_LINUX |
| OSAL Implementation of POSIX is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_NULLOS |
| OSAL Implementation of NULL OS is included. More... | |
| #define | NXPBUILD__PH_OSAL_FREERTOS |
| OSAL Implementation of Free RTOS is included. More... | |
| #define | NXPBUILD__PH_OSAL_FREERTOS |
| OSAL Implementation of Free RTOS is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
| LPCOpenStack SPI BAL Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
| LPCOpenStack SPI BAL Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
| LPCOpenStack SPI I2C Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
| LPCOpenStack SPI I2C Component is included. More... | |
| #define | NXPBUILD__PHBAL_REG_PI_SPI |
| Raspberry Linux UM/KM SPI BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_SPI |
| Raspberry Linux UM/KM SPI BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_I2C |
| Raspberry Linux UM I2C BAL Component is included. | |
| #define | NXPBUILD__PHBAL_REG_PI_I2C |
| Raspberry Linux UM I2C BAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_RC523 |
| RC523 HAL Component is included. More... | |
| #define | NXPBUILD__PHHAL_HW_RC523 |
| RC523 HAL Component is included. More... | |
| #define | NXPBUILD__PHHAL_HW_RC663 |
| RC663 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_RC663 |
| RC663 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_PN5180 |
| PN5180 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_PN5180 |
| PN5180 HAL Component is included. | |
| #define | NXPBUILD__PHHAL_HW_TARGET |
| Dependency checking if target mode macros should be enabled. | |
| #define | NXPBUILD__PHHAL_HW_TARGET |
| Dependency checking if target mode macros should be enabled. | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_SLI15693_SW |
| PAL SLI 15693 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18000P3M3_SW |
| PAL ISO 18000p3m3 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18000P3M3_SW |
| PAL ISO 18000p3m3 Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_LPCD |
| SRC to enable LPCD is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_LPCD |
| SRC to enable LPCD is included. More... | |
| #define | NXPBUILD__PHAL_I18000P3M3_SW |
| AL ISO18000p3m3 SW Component is included. | |
| #define | NXPBUILD__PHAL_I18000P3M3_SW |
| AL ISO18000p3m3 SW Component is included. | |
| #define | NXPBUILD__PHCE_T4T_SW |
| AL HCE T2AT SW Component is included. | |
| #define | NXPBUILD__PHPAL_I18092MPI_SW |
| PAL ISO18092 (P2P) SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MPI_SW |
| PAL ISO18092 (P2P) SW Component is included. More... | |
| #define | NXPBUILD__PHLN_LLCP_SW |
| Link LLCP SW Component is included. | |
| #define | NXPBUILD__PHPAL_I14443P3A_SW |
| PAL ISO 14443-3A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P3B_SW |
| PAL ISO 14443-3B SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4A_SW |
| PAL ISO 14443-4A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4_SW |
| PAL ISO 14443-4 SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_MIFARE_SW |
| PAL MIFARE SW Component is included. | |
| #define | NXPBUILD__PHPAL_FELICA_SW |
| PAL Felica SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_EPCUID_SW |
| < If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_SW |
| Discovery Loop Activity SW Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
| SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
| SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
| SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
| SRC/DATA to Detect FeliCa Cards is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P3B_TAGS |
| SRC/DATA to Detect Type B Cards that operate at Layer3 level is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P4B_TAGS |
| SRC/DATA to Detect Type B Cards such as NFC Forum Type 4 Tags, EMVCo Type B Cards etc is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS |
| SRC/DATA to Detect Type V Cards such as ICODE SLI/SLIX/SLI2/Tesa Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS |
| SRC/DATA to Detect ICODE ILT Cards such as SMARTRAC StackIt Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
| SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
| SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
| SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
| SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
| SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
| SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHNFCLIB |
| Simplified API Interface, If enabling this the entry point should be this component in the application. | |
| #define | NXPBUILD__PH_CIDMANAGER_SW |
| CID Manager SW Component is included. More... | |
| #define | NXPBUILD__PH_KEYSTORE_SW |
| SW KeyStore Component is included. More... | |
| #define | NXPBUILD__PH_CRYPTOSYM_SW |
| Crypto Symbols SW Component is included. More... | |
| #define | NXPBUILD__PH_CRYPTORNG_SW |
| Crypto RNG SW Component is included. More... | |
| #define | NXPBUILD__PHAL_FELICA_SW |
| AL FeliCa SW Component is included. | |
| #define | NXPBUILD__PHAL_MFC_SW |
| AL Mifare Classic SW Component is included. | |
| #define | NXPBUILD__PHAL_MFUL_SW |
| AL Mifare Ultrlight SW Component is included. | |
| #define | NXPBUILD__PHAL_MFDF_SW |
| AL Mifare DesFire SW Component is included. | |
| #define | NXPBUILD__PHAL_T1T_SW |
| AL Type T1 Tag SW Component is included. | |
| #define | NXPBUILD__PHAL_I15693_SW |
| AL ISO 15693 SW Component is included. | |
| #define | NXPBUILD__PHAL_SLI_SW |
| AL SLI SW Component is included. | |
| #define | NXPBUILD__PHAL_TOP_SW |
| AL for TagOps Mapping SW Component is included.Required for NDEF operations. | |
| #define | NXPBUILD__PHNP_SNEP_SW |
| Protocol SNEP SW Component is included. | |
| #define | NXPRDLIB_REM_GEN_INTFS |
| < DEBUG build definition | |
| #define | NXPBUILD__PH_PLATFORM |
| Embedded Platform Porting and Abstraction Component included. More... | |
| #define | NXPBUILD__PH_OSAL_FREERTOS |
| OSAL Implementation of Free RTOS is included. More... | |
| #define | NXPBUILD__PHHAL_HW_PN5180 |
| < If the used NFC HW is not NFC Controller like PN7462AU, then include one of the front end HAL More... | |
| #define | NXPBUILD__PHHAL_HW_TARGET |
| Dependency checking if target mode macros should be enabled. | |
| #define | NXPBUILD__PHPAL_I14443P3A_SW |
| PAL ISO 14443-3A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P3B_SW |
| PAL ISO 14443-3B SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4A_SW |
| PAL ISO 14443-4A SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I14443P4_SW |
| PAL ISO 14443-4 SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_MIFARE_SW |
| PAL MIFARE SW Component is included. | |
| #define | NXPBUILD__PHPAL_FELICA_SW |
| PAL Felica SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_SLI15693_SW |
| PAL SLI 15693 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18000P3M3_SW |
| PAL ISO 18000p3m3 Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MPI_SW |
| < If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude. More... | |
| #define | NXPBUILD__PHPAL_I14443P4MC_SW |
| PAL ISO 14443-4 Card Mode SW Component is included. More... | |
| #define | NXPBUILD__PHPAL_I18092MT_SW |
| PAL ISO 18092 Target Mode SW Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_SW |
| Discovery Loop Activity SW Component is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_LPCD |
| SRC to enable LPCD is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
| SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
| SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
| SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
| SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
| SRC/DATA to Detect FeliCa Cards is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
| SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P3B_TAGS |
| SRC/DATA to Detect Type B Cards that operate at Layer3 level is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEB_I3P4B_TAGS |
| SRC/DATA to Detect Type B Cards such as NFC Forum Type 4 Tags, EMVCo Type B Cards etc is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEV_TAGS |
| SRC/DATA to Detect Type V Cards such as ICODE SLI/SLIX/SLI2/Tesa Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_I18000P3M3_TAGS |
| SRC/DATA to Detect ICODE ILT Cards such as SMARTRAC StackIt Cards is included. | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
| < If FE HAL is RC663, target mode is not supported at all, hence exclude those SRC, otherwise include as required More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
| SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
| SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
| SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
| SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
| SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included. More... | |
| #define | NXPBUILD__PHNFCLIB |
| Simplified API Interface, If enabling this the entry point should be this component in the application. More... | |
| #define | NXPBUILD__PHNFCLIB |
| Simplified API Interface, If enabling this the entry point should be this component in the application. More... | |
| #define | NXPBUILD__PH_KEYSTORE_SW |
| SW KeyStore Component is included. More... | |
| #define | NXPBUILD__PH_NDA_MFDF |
| Mifare DESFire implementation under NDA. | |
| #define | NXPBUILD__PH_CRYPTOSYM_SW |
| Crypto Symbols SW Component is included. More... | |
| #define | NXPBUILD__PH_CRYPTORNG_SW |
| Crypto RNG SW Component is included. More... | |
| #define | NXPBUILD__PHAL_FELICA_SW |
| AL FeliCa SW Component is included. | |
| #define | NXPBUILD__PHAL_MFC_SW |
| AL Mifare Classic SW Component is included. | |
| #define | NXPBUILD__PHAL_MFUL_SW |
| AL Mifare Ultrlight SW Component is included. | |
| #define | NXPBUILD__PHAL_MFDF_SW |
| AL Mifare DesFire SW Component is included. | |
| #define | NXPBUILD__PHAL_T1T_SW |
| AL Type T1 Tag SW Component is included. | |
| #define | NXPBUILD__PHAL_I15693_SW |
| AL ISO 15693 SW Component is included. | |
| #define | NXPBUILD__PHAL_SLI_SW |
| AL SLI SW Component is included. | |
| #define | NXPBUILD__PHAL_TOP_SW |
| AL for TagOps Mapping SW Component is included.Required for NDEF operations. | |
| #define | NXPBUILD__PHAL_I18000P3M3_SW |
| AL ISO18000p3m3 SW Component is included. | |
| #define | NXPBUILD__PHCE_T4T_SW |
| AL HCE T2AT SW Component is included. | |
| #define | NXPBUILD__PHLN_LLCP_SW |
| < SRC to handle Extended NDEF Support as per T4T spec 3.0 is included More... | |
| #define | NXPBUILD__PHNP_SNEP_SW |
| Protocol SNEP SW Component is included. | |
Controls build behaviour of components.
Controls the Inclusion of required components, Inclusion SRC/DATA within components and the Build Dependencies between the components.
| #define NXPBUILD__PHBAL_REG |
< DEBUG build definition
Generic BAL definition
| #define NXPBUILD__PHPAL_FELICA |
< Enable handling of multiple Felica card response
Generic PAL Felica definition
| #define NXPBUILD__PH_PLATFORM |
< DEBUG build definition
Embedded Platform Porting and Abstraction Component included. Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required.
| #define NXPBUILD__PH_PLATFORM |
< DEBUG build definition
Embedded Platform Porting and Abstraction Component included. Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PH_LPC1769 |
Host Controller LPC1769.
Host Controller LPC1769 Porting Component is included.RdLib is linked to LPC1769 Driver from LPCOpenStack.
| #define NXPBUILD__PH_LPC1769 |
Host Controller LPC1769.
Host Controller LPC1769 Porting Component is included.RdLib is linked to LPC1769 Driver from LPCOpenStack.
| #define NXPBUILD__PH_LPC11U68 |
Host Controller LPC11U68.
Host Controller LPC11U68 Porting Component is included.
| #define NXPBUILD__PH_LPC11U68 |
Host Controller LPC11U68.
Host Controller LPC11U68 Porting Component is included.
| #define NXPBUILD__PH_RASPBERRY_PI |
Host Controller RaspBerry Pi.
Host Controller RaspBerry Pi Porting Component is included.
| #define NXPBUILD__PH_RASPBERRY_PI |
Host Controller RaspBerry Pi.
Host Controller RaspBerry Pi Porting Component is included.
| #define NXPBUILD__PH_OSAL_LINUX |
OSAL Implementation of POSIX is included.
RdLib is executed as UM application in Linux
| #define NXPBUILD__PH_OSAL_LINUX |
OSAL Implementation of POSIX is included.
RdLib is executed as UM application in Linux
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_FREERTOS |
OSAL Implementation of Free RTOS is included.
RdLib is linked to Free RTOS Library
| #define NXPBUILD__PH_OSAL_FREERTOS |
OSAL Implementation of Free RTOS is included.
RdLib is linked to Free RTOS Library
| #define NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
LPCOpenStack SPI BAL Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
LPCOpenStack SPI BAL Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
LPCOpenStack SPI I2C Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
LPCOpenStack SPI I2C Component is included.
| #define NXPBUILD__PHHAL_HW_RC523 |
RC523 HAL Component is included.
| #define NXPBUILD__PHHAL_HW_RC523 |
RC523 HAL Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_SLI15693_SW |
PAL SLI 15693 Component is included.
| #define NXPBUILD__PHPAL_I18000P3M3_SW |
PAL ISO 18000p3m3 Component is included.
| #define NXPBUILD__PHPAL_I18000P3M3_SW |
PAL ISO 18000p3m3 Component is included.
| #define NXPBUILD__PHAC_DISCLOOP_LPCD |
SRC to enable LPCD is included.
| #define NXPBUILD__PHAC_DISCLOOP_LPCD |
SRC to enable LPCD is included.
| #define NXPBUILD__PHPAL_I18092MPI_SW |
PAL ISO18092 (P2P) SW Component is included.
| #define NXPBUILD__PHPAL_I18092MPI_SW |
PAL ISO18092 (P2P) SW Component is included.
| #define NXPBUILD__PHPAL_I14443P3A_SW |
PAL ISO 14443-3A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P3B_SW |
PAL ISO 14443-3B SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4A_SW |
PAL ISO 14443-4A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4_SW |
PAL ISO 14443-4 SW Component is included.
| #define NXPBUILD__PHPAL_FELICA_SW |
PAL Felica SW Component is included.
If FE HAL is RC523, then exclude ISO15693 & ISO18000p3m3 PAL, otherwise include as required.
| #define NXPBUILD__PHPAL_EPCUID_SW |
< If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude.
PAL EPC UID SW Component is included.
| #define NXPBUILD__PHAC_DISCLOOP_SW |
Discovery Loop Activity SW Component is included.
If DiscLoop SW Component is included, macros( & it's dependencies) to include/exclude SRC/DATA within Discloop is defined.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
SRC/DATA to Detect FeliCa Cards is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PH_CIDMANAGER_SW |
CID Manager SW Component is included.
| #define NXPBUILD__PH_KEYSTORE_SW |
SW KeyStore Component is included.
| #define NXPBUILD__PH_CRYPTOSYM_SW |
Crypto Symbols SW Component is included.
| #define NXPBUILD__PH_CRYPTORNG_SW |
Crypto RNG SW Component is included.
| #define NXPBUILD__PH_PLATFORM |
< DEBUG build definition
Embedded Platform Porting and Abstraction Component included. Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required.
| #define NXPBUILD__PH_PLATFORM |
< DEBUG build definition
Embedded Platform Porting and Abstraction Component included. Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PHHAL_HW_PN7462AU |
NFC Controller PN7462AU HAL.
NFC Controller PN7462AU HAL and Porting Component is included.
| #define NXPBUILD__PH_LPC1769 |
Host Controller LPC1769.
Host Controller LPC1769 Porting Component is included.RdLib is linked to LPC1769 Driver from LPCOpenStack.
| #define NXPBUILD__PH_LPC1769 |
Host Controller LPC1769.
Host Controller LPC1769 Porting Component is included.RdLib is linked to LPC1769 Driver from LPCOpenStack.
| #define NXPBUILD__PH_LPC11U68 |
Host Controller LPC11U68.
Host Controller LPC11U68 Porting Component is included.
| #define NXPBUILD__PH_LPC11U68 |
Host Controller LPC11U68.
Host Controller LPC11U68 Porting Component is included.
| #define NXPBUILD__PH_RASPBERRY_PI |
Host Controller RaspBerry Pi.
Host Controller RaspBerry Pi Porting Component is included.
| #define NXPBUILD__PH_RASPBERRY_PI |
Host Controller RaspBerry Pi.
Host Controller RaspBerry Pi Porting Component is included.
| #define NXPBUILD__PH_OSAL_LINUX |
OSAL Implementation of POSIX is included.
RdLib is executed as UM application in Linux
| #define NXPBUILD__PH_OSAL_LINUX |
OSAL Implementation of POSIX is included.
RdLib is executed as UM application in Linux
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_NULLOS |
OSAL Implementation of NULL OS is included.
RdLib executed in Executive Loop.
| #define NXPBUILD__PH_OSAL_FREERTOS |
OSAL Implementation of Free RTOS is included.
RdLib is linked to Free RTOS Library
| #define NXPBUILD__PH_OSAL_FREERTOS |
OSAL Implementation of Free RTOS is included.
RdLib is linked to Free RTOS Library
| #define NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
LPCOpenStack SPI BAL Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_SPI |
LPCOpenStack SPI BAL Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
LPCOpenStack SPI I2C Component is included.
| #define NXPBUILD__PHBAL_REG_LPCOPEN_I2C |
LPCOpenStack SPI I2C Component is included.
| #define NXPBUILD__PHHAL_HW_RC523 |
RC523 HAL Component is included.
| #define NXPBUILD__PHHAL_HW_RC523 |
RC523 HAL Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
< ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHPAL_SLI15693_SW |
PAL SLI 15693 Component is included.
| #define NXPBUILD__PHPAL_I18000P3M3_SW |
PAL ISO 18000p3m3 Component is included.
| #define NXPBUILD__PHPAL_I18000P3M3_SW |
PAL ISO 18000p3m3 Component is included.
| #define NXPBUILD__PHAC_DISCLOOP_LPCD |
SRC to enable LPCD is included.
| #define NXPBUILD__PHAC_DISCLOOP_LPCD |
SRC to enable LPCD is included.
| #define NXPBUILD__PHPAL_I18092MPI_SW |
PAL ISO18092 (P2P) SW Component is included.
| #define NXPBUILD__PHPAL_I18092MPI_SW |
PAL ISO18092 (P2P) SW Component is included.
| #define NXPBUILD__PHPAL_I14443P3A_SW |
PAL ISO 14443-3A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P3B_SW |
PAL ISO 14443-3B SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4A_SW |
PAL ISO 14443-4A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4_SW |
PAL ISO 14443-4 SW Component is included.
| #define NXPBUILD__PHPAL_FELICA_SW |
PAL Felica SW Component is included.
If FE HAL is RC523, then exclude ISO15693 & ISO18000p3m3 PAL, otherwise include as required.
| #define NXPBUILD__PHPAL_EPCUID_SW |
< If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude.
PAL EPC UID SW Component is included.
| #define NXPBUILD__PHAC_DISCLOOP_SW |
Discovery Loop Activity SW Component is included.
If DiscLoop SW Component is included, macros( & it's dependencies) to include/exclude SRC/DATA within Discloop is defined.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
SRC/DATA to Detect FeliCa Cards is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PH_CIDMANAGER_SW |
CID Manager SW Component is included.
| #define NXPBUILD__PH_KEYSTORE_SW |
SW KeyStore Component is included.
| #define NXPBUILD__PH_CRYPTOSYM_SW |
Crypto Symbols SW Component is included.
| #define NXPBUILD__PH_CRYPTORNG_SW |
Crypto RNG SW Component is included.
| #define NXPBUILD__PH_PLATFORM |
Embedded Platform Porting and Abstraction Component included.
Used for LPC_XXX, Kinetis_XXX,Raspberry_XXX,iMX_XXX etc. If RdLib executing on embedded platform, then include one of the below embedded platform and one of the OS used as required.
| #define NXPBUILD__PH_OSAL_FREERTOS |
OSAL Implementation of Free RTOS is included.
RdLib is linked to Free RTOS Library
| #define NXPBUILD__PHHAL_HW_PN5180 |
< If the used NFC HW is not NFC Controller like PN7462AU, then include one of the front end HAL
PN5180 HAL Component is included
| #define NXPBUILD__PHPAL_I14443P3A_SW |
PAL ISO 14443-3A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P3B_SW |
PAL ISO 14443-3B SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4A_SW |
PAL ISO 14443-4A SW Component is included.
| #define NXPBUILD__PHPAL_I14443P4_SW |
PAL ISO 14443-4 SW Component is included.
| #define NXPBUILD__PHPAL_FELICA_SW |
PAL Felica SW Component is included.
If FE HAL is RC523, then exclude ISO15693 & ISO18000p3m3 PAL, otherwise include as required.
| #define NXPBUILD__PHPAL_SLI15693_SW |
PAL SLI 15693 Component is included.
| #define NXPBUILD__PHPAL_I18000P3M3_SW |
PAL ISO 18000p3m3 Component is included.
| #define NXPBUILD__PHPAL_I18092MPI_SW |
< If FE HAL is RC663, then include EPC UID PAL as required, otherwise exclude.
PAL ISO18092 (P2P) SW Component is included. If FE HAL is RC663, then exclude ISO14443 Card Mode PAL & ISO18092 Target Mode PAL, otherwise include as required. ISO14443 Card Mode PAL & ISO18092 Target Mode PAL will execute only in an embedded platform and not in PC platform.
| #define NXPBUILD__PHPAL_I14443P4MC_SW |
PAL ISO 14443-4 Card Mode SW Component is included.
| #define NXPBUILD__PHPAL_I18092MT_SW |
PAL ISO 18092 Target Mode SW Component is included.
| #define NXPBUILD__PHAC_DISCLOOP_SW |
Discovery Loop Activity SW Component is included.
If DiscLoop SW Component is included, macros( & it's dependencies) to include/exclude SRC/DATA within Discloop is defined.
| #define NXPBUILD__PHAC_DISCLOOP_LPCD |
SRC to enable LPCD is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P3_TAGS |
SRC/DATA to Detect/CollRes/Activate cards such as MFC, MFUL, MFP SL1 etc is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_JEWEL_TAGS |
SRC/DATA to Detect cards such as NFC Forum T1T, Topaz/Jewel is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_I3P4_TAGS |
SRC/DATA to Detect cards such as MFDF, MFP, T4AT NFC Forum Tag or Type A EMVCo is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type A P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F212 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_P2P_ACTIVE |
SRC/DATA to Detect Peer Active Type F424 P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_FELICA_TAGS |
SRC/DATA to Detect FeliCa Cards is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF_P2P_TAGS |
SRC/DATA to Detect Peer Passive Type F P2P Target mode devices is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_PASSIVE |
< If FE HAL is RC663, target mode is not supported at all, hence exclude those SRC, otherwise include as required
SRC to Initialize Type A passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEA_TARGET_ACTIVE |
SRC to Initialize Type A active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_PASSIVE |
SRC to Initialize Type F212 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF212_TARGET_ACTIVE |
SRC to Initialize Type F212 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_PASSIVE |
SRC to Initialize Type F424 passive listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHAC_DISCLOOP_TYPEF424_TARGET_ACTIVE |
SRC to Initialize Type F424 active listen config and subsequently call HAL AutoColl is included.
| #define NXPBUILD__PHNFCLIB |
Simplified API Interface, If enabling this the entry point should be this component in the application.
Simplified layer Component.
| #define NXPBUILD__PHNFCLIB |
Simplified API Interface, If enabling this the entry point should be this component in the application.
Simplified layer Component.
| #define NXPBUILD__PH_KEYSTORE_SW |
SW KeyStore Component is included.
| #define NXPBUILD__PH_CRYPTOSYM_SW |
Crypto Symbols SW Component is included.
| #define NXPBUILD__PH_CRYPTORNG_SW |
Crypto RNG SW Component is included.
| #define NXPBUILD__PHLN_LLCP_SW |
< SRC to handle Extended NDEF Support as per T4T spec 3.0 is included
Link LLCP SW Component is included