These Components implement the Felica (contactless) protocol.
More...
|
| phStatus_t | phpalFelica_ReqC (void *pDataParams, uint8_t *pSystemCode, uint8_t bNumTimeSlots, uint8_t **ppRxBuffer, uint16_t *wLen) |
| | Perform the Felica ReqC command. More...
|
| |
| phStatus_t | phpalFelica_ActivateCard (void *pDataParams, uint8_t *pIDmPMm, uint8_t bIDmPMmLength, uint8_t *pSystemCode, uint8_t bNumTimeSlots, uint8_t *pRxBuffer, uint8_t *pRxLength, uint8_t *pMoreCardsAvailable) |
| | This command activates a Felica card. More...
|
| |
| phStatus_t | phpalFelica_Exchange (void *pDataParams, uint16_t wOption, uint16_t wN, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| | Exchange data with the Picc. More...
|
| |
| phStatus_t | phpalFelica_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| | Set configuration parameter. More...
|
| |
| phStatus_t | phpalFelica_GetConfig (void *pDataParams, uint16_t wConfig, uint16_t *pValue) |
| | Get configuration parameter. More...
|
| |
| phStatus_t | phpalFelica_GetSerialNo (void *pDataParams, uint8_t *pUidOut, uint8_t *pLenUidOut) |
| | As the card receives the Get Serial Number command, it shall respond with that one. More...
|
| |
| phStatus_t | phpalFelica_GetFrameInfo (void *pDataParams, uint8_t bFrameNum, uint8_t *pResponseBuffer, uint16_t *pwStatus, uint8_t **pID, uint8_t *pLen) |
| | This function will provide information of given frame number(1 to N). More...
|
| |
| phStatus_t | phpalFelica_SetSerialNo (void *pDataParams, uint8_t *pIDmPMm) |
| | This function will update IDmPMm in this layer's parameter structure. More...
|
| |
|
|
#define | PHPAL_FELICA_SYSTEM_CODE_BYTE_0 0xFFU |
| |
|
#define | PHPAL_FELICA_SYSTEM_CODE_BYTE_1 0xFFU |
| |
These Components implement the Felica (contactless) protocol.
§ PHPAL_FELICA_IDM_LENGTH
| #define PHPAL_FELICA_IDM_LENGTH 8U |
§ PHPAL_FELICA_PMM_LENGTH
| #define PHPAL_FELICA_PMM_LENGTH 8U |
§ PHPAL_FELICA_BLOCK_LENGTH
| #define PHPAL_FELICA_BLOCK_LENGTH 4U |
§ PHPAL_FELICA_PAGE_LENGTH
| #define PHPAL_FELICA_PAGE_LENGTH 16U |
Number of bytes per page.
§ PHPAL_FELICA_ATQC_LENGTH
| #define PHPAL_FELICA_ATQC_LENGTH 17U |
§ PHPAL_FELICA_RD_LENGTH
| #define PHPAL_FELICA_RD_LENGTH 2U |
Length of Request Data (RD) in ATQC.
§ PHPAL_FELICA_TXLENGTH_MAX
| #define PHPAL_FELICA_TXLENGTH_MAX 254U |
Maximum length of a transmission package.
§ PHPAL_FELICA_NUMSLOTS_1
| #define PHPAL_FELICA_NUMSLOTS_1 0x00 |
§ PHPAL_FELICA_NUMSLOTS_2
| #define PHPAL_FELICA_NUMSLOTS_2 0x01 |
§ PHPAL_FELICA_NUMSLOTS_4
| #define PHPAL_FELICA_NUMSLOTS_4 0x03 |
§ PHPAL_FELICA_NUMSLOTS_8
| #define PHPAL_FELICA_NUMSLOTS_8 0x07 |
§ PHPAL_FELICA_NUMSLOTS_16
| #define PHPAL_FELICA_NUMSLOTS_16 0x0F |
Value for bNumSlots = 16.
§ PHPAL_FELICA_PREAMBLE_LEN_48BITS
| #define PHPAL_FELICA_PREAMBLE_LEN_48BITS 0x00 |
Lengths
Preamble of 48 Bits.
§ PHPAL_FELICA_PREAMBLE_LEN_56BITS
| #define PHPAL_FELICA_PREAMBLE_LEN_56BITS 0x02 |
§ PHPAL_FELICA_PREAMBLE_LEN_64BITS
| #define PHPAL_FELICA_PREAMBLE_LEN_64BITS 0x03 |
§ PHPAL_FELICA_PREAMBLE_LEN_72BITS
| #define PHPAL_FELICA_PREAMBLE_LEN_72BITS 0x04 |
§ PH_PALFELICA_CONFIG_NUM_RESPONSE_FRAMES
| #define PH_PALFELICA_CONFIG_NUM_RESPONSE_FRAMES 0x0001U |
§ phpalFelica_ReqC()
Perform the Felica ReqC command.
Note: This function waits until all cards in all time slots have had time to reply even though only the first response is returned.
The formula used is 1208us * (n-1) according to JIS X 6319-4:2005.
Response format when bNumTimeSlots greater than PHPAL_FELICA_NUMSLOTS_1
0 28 31
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
| LEN | PAYLOAD(MAX 19 BYTES) | PAD | STATUS |
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
Format of Status Byte.
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
| | | |L| | | | | |
| | | |e|Co|Pr|Da|CL| |
| RFU | LEN | RFU |n|ll|ot|ta|Er| RFU |
| [7:5]| [4:0] | [7:5]|E|De|Er|Er|ro| |
| | | |r|t |r |r |r | |
| | | |r| | | | | |
+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
|<-------Byte 28----->|<------Byte 29----->|<------Byte 30----->|<------Byte 31------>|
Response format when bNumTimeSlots is PHPAL_FELICA_NUMSLOTS_1
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
| IDmPMm[16] | RD[Optional] |
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pSystemCode | System-Code; uint8_t[2]. |
| [in] | bNumTimeSlots | Number of time slots to use. Refer to e.g. PHPAL_FELICA_NUMSLOTS_1 for valid values. |
| [out] | ppRxBuffer | Pointer to the HAL Rx buffer. 32bytes / slot information in case of multiple slots or else a single response containing IDmPMm. |
| [out] | wLen | Length of the content in the buffer. |
§ phpalFelica_ActivateCard()
This command activates a Felica card.
Note: If an IDm is passed to this function, it is stored as the current IDm and no real activation is done.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pIDmPMm | IDm followed by PMm; If supplied it is stored and no real activation is done. |
| [in] | bIDmPMmLength | IDm length; 0 or 16. |
| [in] | pSystemCode | System-Code; uint8_t[2]. |
| [in] | bNumTimeSlots | Number of timeslots to use. Refer to e.g. PHPAL_FELICA_NUMSLOTS_1 for valid values. |
| [out] | pRxBuffer | 8 bytes NFCID2 + 8 bytes PAD; uint8_t[16]. |
| [out] | pRxLength | Length of received data. 0 or 16. |
| [out] | pMoreCardsAvailable | Whether there are more cards in the field or not; uint8_t. |
§ phpalFelica_Exchange()
Exchange data with the Picc.
wOption can be one of:
Alternatively, the following bits can be combined:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | wN | N to calculate the response timeout. |
| [in] | pTxBuffer | Data to transmit; Length and IDm is added automatically. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data; Length, response code and IDm are removed automatically. |
| [out] | pRxLength | number of received data bytes. |
§ phpalFelica_SetConfig()
| phStatus_t phpalFelica_SetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t |
wValue |
|
) |
| |
Set configuration parameter.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [in] | wValue | Configuration Value. |
§ phpalFelica_GetConfig()
| phStatus_t phpalFelica_GetConfig |
( |
void * |
pDataParams, |
|
|
uint16_t |
wConfig, |
|
|
uint16_t * |
pValue |
|
) |
| |
Get configuration parameter.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [out] | pValue | Configuration Value. |
§ phpalFelica_GetSerialNo()
| phStatus_t phpalFelica_GetSerialNo |
( |
void * |
pDataParams, |
|
|
uint8_t * |
pUidOut, |
|
|
uint8_t * |
pLenUidOut |
|
) |
| |
As the card receives the Get Serial Number command, it shall respond with that one.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pUidOut | Last Uid (IDm + PMm); uint8_t[16]. |
| [out] | pLenUidOut | Length of Uid; 0 or 16. |
§ phpalFelica_GetFrameInfo()
This function will provide information of given frame number(1 to N).
It will provide pointer to IDmPMm if frame status is PH_ERR_SUCCESS. pwStatus can be one of:
Note: This function is only valid when function phpalFelica_ReqC is called with slot number greater than PHPAL_FELICA_NUMSLOTS_1.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bFrameNum | Frame number. Frame number 0 is invalid. |
| [in] | pResponseBuffer | The pointer to the entire Felica response as obtained from ReqC API. |
| [out] | pwStatus | Frame status. Status will be Success, or one of collision, length, integrity, protocol errors. |
| [out] | pID | Pointer to IDmPMm in case of wStatus being success. |
| [out] | pLen | Length of IDmPMm data. 2 Request Data (RD) bytes are optional. This will indicate exact length. |
§ phpalFelica_SetSerialNo()
| phStatus_t phpalFelica_SetSerialNo |
( |
void * |
pDataParams, |
|
|
uint8_t * |
pIDmPMm |
|
) |
| |
This function will update IDmPMm in this layer's parameter structure.
This function must be call after card or device is activated.
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pIDmPMm | 16 byte IDmPMm. |