|
NXP NFC Reader Library
v4.040.05.011646
|
These Components implement the ISO/IEC 14443-3 Type-B contactless protocol. More...
|
Modules | |
| Component : Software | |
Functions | |
| phStatus_t | phpalI14443p3b_SetConfig (void *pDataParams, uint16_t wConfig, uint16_t wValue) |
| Set configuration value. More... | |
| phStatus_t | phpalI14443p3b_GetConfig (void *pDataParams, uint16_t wConfig, uint16_t *pValue) |
| Get configuration value. More... | |
| phStatus_t | phpalI14443p3b_RequestB (void *pDataParams, uint8_t bNumSlots, uint8_t bAfi, uint8_t bExtAtqb, uint8_t *pAtqb, uint8_t *pAtqbLen) |
| Perform a ISO14443-3B Request command. More... | |
| phStatus_t | phpalI14443p3b_WakeUpB (void *pDataParams, uint8_t bNumSlots, uint8_t bAfi, uint8_t bExtAtqb, uint8_t *pAtqb, uint8_t *pAtqbLen) |
| Perform a ISO14443-3B Wakeup command. More... | |
| phStatus_t | phpalI14443p3b_SlotMarker (void *pDataParams, uint8_t bSlotNumber, uint8_t *pAtqb, uint8_t *pAtqbLen) |
| Perform a ISO14443-3B Slot-MARKER command. More... | |
| phStatus_t | phpalI14443p3b_HaltB (void *pDataParams) |
| Perform a ISO14443-3B Halt command. More... | |
| phStatus_t | phpalI14443p3b_Attrib (void *pDataParams, uint8_t *pAtqb, uint8_t bAtqbLen, uint8_t bFsdi, uint8_t bCid, uint8_t bDri, uint8_t bDsi, uint8_t *pMbli) |
| Perform a ISO14443-3B Attrib command. More... | |
| phStatus_t | phpalI14443p3b_ActivateCard (void *pDataParams, uint8_t *pPupi, uint8_t bPupiLength, uint8_t bNumSlots, uint8_t bAfi, uint8_t bExtAtqb, uint8_t bFsdi, uint8_t bCid, uint8_t bDri, uint8_t bDsi, uint8_t *pAtqb, uint8_t *pAtqbLen, uint8_t *pMbli, uint8_t *pMoreCardsAvailable) |
| Perform ISO14443-3B ReqB or WupB and Anticollision/Select commands for all cascade levels. More... | |
| phStatus_t | phpalI14443p3b_Exchange (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| Perform ISO14443-3B Data Exchange with Picc. More... | |
| phStatus_t | phpalI14443p3b_GetSerialNo (void *pDataParams, uint8_t *pPupi) |
| Retrieve the serial number. More... | |
| phStatus_t | phpalI14443p3b_SetSerialNo (void *pDataParams, uint8_t *pPupi) |
| This function will update PUPI in this layer's parameter structure. More... | |
| phStatus_t | phpalI14443p3b_SetHigherLayerInf (void *pDataParams, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t *pRxBuffer, uint16_t wRxBufSize) |
| Set higher layer information. More... | |
| phStatus_t | phpalI14443p3b_GetHigherLayerResp (void *pDataParams, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| Get higher layer response. More... | |
| phStatus_t | phpalI14443p3b_GetProtocolParams (void *pDataParams, uint8_t *pCidEnabled, uint8_t *pCid, uint8_t *pNadSupported, uint8_t *pFwi, uint8_t *pFsdi, uint8_t *pFsci) |
| Retrieve the ISO14443-3B protocol parameters. More... | |
14443-3B constant definitions | |
| #define | PHPAL_I14443P3B_CONFIG_ATTRIB_PARAM1 0x0000U |
| Set or get the AttribB param1 byte. More... | |
Configuration | |
| #define | PHPAL_I14443P3B_CONFIG_OPE_MODE 0x0001U |
| Configure Operation Mode for this Layer. More... | |
| #define | PHPAL_I14443P3B_CONFIG_POLL_CMD 0x0002U |
| Configure which command to be used for Type B Polling. More... | |
| #define | PHPAL_I14443P3B_CONFIG_ATTRIB_RETRY_COUNT 0x0003U |
| Configure retry count for ATTRIB command. More... | |
Poll Command | |
| #define | PHPAL_I14443P3B_USE_REQB 0x00U |
| Indicate REQB command to be used for Type B Polling. | |
| #define | PHPAL_I14443P3B_USE_WUPB 0x01U |
| Indicate WakeupB command to be used for Type B Polling. | |
DRI/DSI Values | |
| #define | PHPAL_I14443P3B_DATARATE_106 0x00U |
| DRI/DSI value for 106 kBit/s. | |
| #define | PHPAL_I14443P3B_DATARATE_212 0x01U |
| DRI/DSI value for 212 kBit/s. | |
| #define | PHPAL_I14443P3B_DATARATE_424 0x02U |
| DRI/DSI value for 424 kBit/s. | |
| #define | PHPAL_I14443P3B_DATARATE_848 0x03U |
| DRI/DSI value for 848 kBit/s. | |
| #define | PHPAL_I14443P3B_DATARATE_FORCE 0x80U |
| Flag that forces the use of the given baud rates. | |
Attrib Command Retry Values | |
| #define | PHPAL_I14443P3B_ATTRIB_RETRY_MAX 1 |
| Maximum retry value of ATTRIB during transmission and timeout error. More... | |
| #define | PHPAL_I14443P3B_ATTRIB_RETRY_MIN 0 |
| Minimum retry value of ATTRIB during transmission and timeout error. More... | |
These Components implement the ISO/IEC 14443-3 Type-B contactless protocol.
Note: The "Timing before the PCD SOF" (see 7.1.7, ISO/IEC 14443-3:2009(E)) is mandatory and is neither implemented here nor implemented in every Hardware Abstraction Layer layer.
Make sure that either the used HAL or the used application does comply to this rule.
| #define PHPAL_I14443P3B_CONFIG_ATTRIB_PARAM1 0x0000U |
Set or get the AttribB param1 byte.
| #define PHPAL_I14443P3B_CONFIG_OPE_MODE 0x0001U |
Configure Operation Mode for this Layer.
Possible values are
RD_LIB_MODE_EMVCO,
RD_LIB_MODE_NFC,
RD_LIB_MODE_ISO,
Default value is RD_LIB_MODE_NFC.
| #define PHPAL_I14443P3B_CONFIG_POLL_CMD 0x0002U |
Configure which command to be used for Type B Polling.
Possible values are
PHPAL_I14443P3B_USE_WUPB,
PHPAL_I14443P3B_USE_REQB,
Default value is PHPAL_I14443P3B_USE_REQB.
| #define PHPAL_I14443P3B_CONFIG_ATTRIB_RETRY_COUNT 0x0003U |
Configure retry count for ATTRIB command.
Possible values are
PHPAL_I14443P3B_ATTRIB_RETRY_MIN,
PHPAL_I14443P3B_ATTRIB_RETRY_MAX,
Default value is PHPAL_I14443P3B_ATTRIB_RETRY_MAX.
For mode RD_LIB_MODE_EMVCO retry count should be 1.
| #define PHPAL_I14443P3B_ATTRIB_RETRY_MAX 1 |
Maximum retry value of ATTRIB during transmission and timeout error.
| #define PHPAL_I14443P3B_ATTRIB_RETRY_MIN 0 |
Minimum retry value of ATTRIB during transmission and timeout error.
Set configuration value.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [in] | wValue | Configuration Value. |
Get configuration value.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wConfig | Configuration Identifier. |
| [out] | pValue | Configuration Value. |
| phStatus_t phpalI14443p3b_RequestB | ( | void * | pDataParams, |
| uint8_t | bNumSlots, | ||
| uint8_t | bAfi, | ||
| uint8_t | bExtAtqb, | ||
| uint8_t * | pAtqb, | ||
| uint8_t * | pAtqbLen | ||
| ) |
Perform a ISO14443-3B Request command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | bNumSlots | Number of slots. |
| [in] | bAfi | AFI; Application Family Indentifier. |
| [in] | bExtAtqb | Enable Extended AtqB. |
| [out] | pAtqb | AtqB; uint8_t[13]. |
| [out] | pAtqbLen | length of ATQB (12/13 bytes). |
| phStatus_t phpalI14443p3b_WakeUpB | ( | void * | pDataParams, |
| uint8_t | bNumSlots, | ||
| uint8_t | bAfi, | ||
| uint8_t | bExtAtqb, | ||
| uint8_t * | pAtqb, | ||
| uint8_t * | pAtqbLen | ||
| ) |
Perform a ISO14443-3B Wakeup command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | bNumSlots | Number of slots. |
| [in] | bAfi | AFI; Application Family Indentifier. |
| [in] | bExtAtqb | Enable Extended AtqB. |
| [out] | pAtqb | AtqB; uint8_t[12/13]. |
| [out] | pAtqbLen | length of ATQB (12/13 bytes). |
| phStatus_t phpalI14443p3b_SlotMarker | ( | void * | pDataParams, |
| uint8_t | bSlotNumber, | ||
| uint8_t * | pAtqb, | ||
| uint8_t * | pAtqbLen | ||
| ) |
Perform a ISO14443-3B Slot-MARKER command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | bSlotNumber | Slot Number. |
| [out] | pAtqb | AtqB; uint8_t[12/13]. |
| [out] | pAtqbLen | length of ATQB (12/13 bytes). |
| phStatus_t phpalI14443p3b_HaltB | ( | void * | pDataParams | ) |
Perform a ISO14443-3B Halt command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| phStatus_t phpalI14443p3b_Attrib | ( | void * | pDataParams, |
| uint8_t * | pAtqb, | ||
| uint8_t | bAtqbLen, | ||
| uint8_t | bFsdi, | ||
| uint8_t | bCid, | ||
| uint8_t | bDri, | ||
| uint8_t | bDsi, | ||
| uint8_t * | pMbli | ||
| ) |
Perform a ISO14443-3B Attrib command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | pAtqb | Atqb from ReqB/WupB; uint8_t[12/13]. |
| [in] | bAtqbLen | Length of Atqb. |
| [in] | bFsdi | Frame Size Integer; 0-8. |
| [in] | bCid | Card Identifier; 0-14. |
| [in] | bDri | Divisor Receive (PCD to PICC) Integer; 0-3. |
| [in] | bDsi | Divisor Send (PICC to PCD) Integer; 0-3. |
| [out] | pMbli | MBLI byte; uint8_t. |
| phStatus_t phpalI14443p3b_ActivateCard | ( | void * | pDataParams, |
| uint8_t * | pPupi, | ||
| uint8_t | bPupiLength, | ||
| uint8_t | bNumSlots, | ||
| uint8_t | bAfi, | ||
| uint8_t | bExtAtqb, | ||
| uint8_t | bFsdi, | ||
| uint8_t | bCid, | ||
| uint8_t | bDri, | ||
| uint8_t | bDsi, | ||
| uint8_t * | pAtqb, | ||
| uint8_t * | pAtqbLen, | ||
| uint8_t * | pMbli, | ||
| uint8_t * | pMoreCardsAvailable | ||
| ) |
Perform ISO14443-3B ReqB or WupB and Anticollision/Select commands for all cascade levels.
If bLenUidIn is '0' –> CardUid not given, a ReqB is performed. If CardUid is given, a WupB is performed.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | pPupi | Pointer to the known PUPI; uint8_t[4]. |
| [in] | bPupiLength | Length of given PUPI, only a value of 0 or 4 is allowed. |
| [in] | bNumSlots | Number of slots. |
| [in] | bAfi | AFI; Application Family Indentifier. |
| [in] | bExtAtqb | Enable Extended AtqB. |
| [in] | bFsdi | Frame Size Integer; 0-8. |
| [in] | bCid | Card Identifier; 0-14. |
| [in] | bDri | Divisor Receive (PCD to PICC) Integer; 0-3. |
| [in] | bDsi | Divisor Send (PICC to PCD) Integer; 0-3. |
| [out] | pAtqb | AtqB; uint8_t[13]. |
| [out] | pAtqbLen | length of ATQB (12/13 bytes). |
| [out] | pMbli | MBLI byte; uint8_t. |
| [out] | pMoreCardsAvailable | Whether there are more cards in the field or not; uint8_t. |
| phStatus_t phpalI14443p3b_Exchange | ( | void * | pDataParams, |
| uint16_t | wOption, | ||
| uint8_t * | pTxBuffer, | ||
| uint16_t | wTxLength, | ||
| uint8_t ** | ppRxBuffer, | ||
| uint16_t * | pRxLength | ||
| ) |
Perform ISO14443-3B Data Exchange with Picc.
wOption can be one of:
Alternatively, the following bits can be combined:
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | number of received data bytes. |
| phStatus_t phpalI14443p3b_GetSerialNo | ( | void * | pDataParams, |
| uint8_t * | pPupi | ||
| ) |
Retrieve the serial number.
This function will provide 4 byte PUPI.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_USE_CONDITION | No PUPI available. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [out] | pPupi | Most recent PUPI. |
| phStatus_t phpalI14443p3b_SetSerialNo | ( | void * | pDataParams, |
| uint8_t * | pPupi | ||
| ) |
This function will update PUPI in this layer's parameter structure.
This function must be called with valid PUPI. Once set the subsequent type B commands use this PUPI.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | pPupi | 4 byte PUPI. |
| phStatus_t phpalI14443p3b_SetHigherLayerInf | ( | void * | pDataParams, |
| uint8_t * | pTxBuffer, | ||
| uint16_t | wTxLength, | ||
| uint8_t * | pRxBuffer, | ||
| uint16_t | wRxBufSize | ||
| ) |
Set higher layer information.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_USE_CONDITION | Feature not available. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [in] | pTxBuffer | Higher layer Information; Can be NULL if /c wTxLength is 0. |
| [in] | wTxLength | Length of the Higher layer Information. Can be 0. |
| [in] | pRxBuffer | Higher layer response buffer. |
| [in] | wRxBufSize | Size of Higher layer response buffer. |
| phStatus_t phpalI14443p3b_GetHigherLayerResp | ( | void * | pDataParams, |
| uint8_t ** | ppRxBuffer, | ||
| uint16_t * | pRxLength | ||
| ) |
Get higher layer response.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_USE_CONDITION | Feature not available. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [out] | ppRxBuffer | Higher layer response. |
| [out] | pRxLength | Length of Higher layer response. |
| phStatus_t phpalI14443p3b_GetProtocolParams | ( | void * | pDataParams, |
| uint8_t * | pCidEnabled, | ||
| uint8_t * | pCid, | ||
| uint8_t * | pNadSupported, | ||
| uint8_t * | pFwi, | ||
| uint8_t * | pFsdi, | ||
| uint8_t * | pFsci | ||
| ) |
Retrieve the ISO14443-3B protocol parameters.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | Pointer to this layers parameter structure. |
| [out] | pCidEnabled | Unequal '0' if Card Identifier is enabled. |
| [out] | pCid | Card Identifier. |
| [out] | pNadSupported | Node Address Support; Unequal '0' if supported. |
| [out] | pFwi | Frame Waiting Integer. |
| [out] | pFsdi | PCD Frame Size Integer; 0-8. |
| [out] | pFsci | PICC Frame Size Integer; 0-8. |