|
NXP NFC Reader Library
v4.040.05.011646
|
Keystore implementation in Software. More...
|
Data Structures | |
| struct | phKeyStore_Sw_KeyVersionPair_t |
| Sw KeyVersionPair structure. More... | |
| struct | phKeyStore_Sw_KeyEntry_t |
| Sw KeyEntry structure. More... | |
| struct | phKeyStore_Sw_KUCEntry_t |
| Sw KeyUsageCounter structure. More... | |
| struct | phKeyStore_Sw_DataParams_t |
| Sw parameter structure. More... | |
Macros | |
| #define | PH_KEYSTORE_SW_ID 0x01 |
| ID for Software KeyStore component. More... | |
| #define | PH_KEYSTORE_SW_MAX_KEY_SIZE 32U |
| Maximum size of a Key. More... | |
Functions | |
| phStatus_t | phKeyStore_Sw_Init (phKeyStore_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phKeyStore_Sw_KeyEntry_t *pKeyEntries, uint16_t wNoOfKeyEntries, phKeyStore_Sw_KeyVersionPair_t *pKeyVersionPairs, uint16_t wNoOfVersionPairs, phKeyStore_Sw_KUCEntry_t *pKUCEntries, uint16_t wNoOfKUCEntries) |
| Initialise this layer. More... | |
Keystore implementation in Software.
| #define PH_KEYSTORE_SW_ID 0x01 |
ID for Software KeyStore component.
| #define PH_KEYSTORE_SW_MAX_KEY_SIZE 32U |
Maximum size of a Key.
| phStatus_t phKeyStore_Sw_Init | ( | phKeyStore_Sw_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phKeyStore_Sw_KeyEntry_t * | pKeyEntries, | ||
| uint16_t | wNoOfKeyEntries, | ||
| phKeyStore_Sw_KeyVersionPair_t * | pKeyVersionPairs, | ||
| uint16_t | wNoOfVersionPairs, | ||
| phKeyStore_Sw_KUCEntry_t * | pKUCEntries, | ||
| uint16_t | wNoOfKUCEntries | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | Specifies the size of the data parameter structure. |
| [in] | pKeyEntries | Pointer to a storage containing the key entries. |
| [in] | wNoOfKeyEntries | size of pKeyEntries. |
| [in] | pKeyVersionPairs | Pointer to a storage containing the key version pairs. |
| [in] | wNoOfVersionPairs | amount of key versions available in each key entry. |
| [in] | pKUCEntries | Key usage counter entry storage, size = sizeof(phKeyStore_Sw_KUCEntry_t) * wNumKUCEntries |
| [in] | wNoOfKUCEntries | Number of Key usage counter entries. |