|
NXP NFC Reader Library
v4.040.05.011646
|
Software PAL-MIFARE parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pHalDataParams |
| Pointer to the parameter structure of the underlying HAL layer. More... | |
| void * | pPalI14443p4DataParams |
| Pointer to the parameter structure of the underlying ISO14443-4 layer. More... | |
Software PAL-MIFARE parameter structure.
| void* phpalMifare_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of the underlying HAL layer.
| void* phpalMifare_Sw_DataParams_t::pPalI14443p4DataParams |
Pointer to the parameter structure of the underlying ISO14443-4 layer.