|
NXP NFC Reader Library
v4.040.05.011646
|
Target parameter structure. More...
Data Fields | |
| uint8_t * | pRxBuffer |
| Pointer to the Receive Buffer. More... | |
| uint16_t | wRxBufferLen |
| Length of Data Present in Receive Buffer. More... | |
| uint16_t | wProtParams |
| Frame mode and RX speed information. More... | |
| uint8_t | bRetryCount |
| Retry count for AUTOCOLL in case of failure. More... | |
Target parameter structure.
| uint8_t* phacDiscLoop_TargetParams::pRxBuffer |
Pointer to the Receive Buffer.
| uint16_t phacDiscLoop_TargetParams::wRxBufferLen |
Length of Data Present in Receive Buffer.
| uint16_t phacDiscLoop_TargetParams::wProtParams |
Frame mode and RX speed information.
| uint8_t phacDiscLoop_TargetParams::bRetryCount |
Retry count for AUTOCOLL in case of failure.
Default is 0.