These Components implement the MIFARE(R) Classic, MIFARE(R) Ultralight, MIFARE(R) DESFire and MIFARE(R) Plus products.
More...
|
| phStatus_t | phpalMifare_ExchangeL3 (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| | Perform ISO14443-3 Data Exchange with MIFARE Picc. More...
|
| |
| phStatus_t | phpalMifare_ExchangeL4 (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| | Perform ISO14443-4 Data Exchange with MIFARE Picc. More...
|
| |
| phStatus_t | phpalMifare_ExchangePc (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t **ppRxBuffer, uint16_t *pRxLength) |
| | Perform Proximity-Check Data Exchange with MIFARE Picc. More...
|
| |
| phStatus_t | phpalMifare_ExchangeRaw (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxLength, uint8_t bTxLastBits, uint8_t **ppRxBuffer, uint16_t *pRxLength, uint8_t *pRxLastBits) |
| | Perform Raw (No CRC, No Parity) Data Exchange with MIFARE Picc. More...
|
| |
| phStatus_t | phpalMifare_MfcAuthenticateKeyNo (void *pDataParams, uint8_t bBlockNo, uint8_t bKeyType, uint16_t wKeyNo, uint16_t wKeyVersion, uint8_t *pUid) |
| | Perform MIFARE(R) Authenticate command with Picc using a key number. More...
|
| |
| phStatus_t | phpalMifare_MfcAuthenticate (void *pDataParams, uint8_t bBlockNo, uint8_t bKeyType, uint8_t *pKey, uint8_t *pUid) |
| | Perform MIFARE(R) Authenticate command with Picc using a key. More...
|
| |
| phStatus_t | phpalMifare_SetMinFdtPc (void *pDataParams, uint16_t wValue) |
| | Perform Setting min FDT for Proximity check. More...
|
| |
These Components implement the MIFARE(R) Classic, MIFARE(R) Ultralight, MIFARE(R) DESFire and MIFARE(R) Plus products.
§ PHPAL_MIFARE_KEYA
| #define PHPAL_MIFARE_KEYA 0x0AU |
MIFARE Classic Key Type A.
§ PHPAL_MIFARE_KEYB
| #define PHPAL_MIFARE_KEYB 0x0BU |
MIFARE Classic Key Type B.
§ PHPAL_MIFARE_KEY_LENGTH
| #define PHPAL_MIFARE_KEY_LENGTH 0x06U |
Length of a MIFARE Classic key (for completeness).
§ phpalMifare_ExchangeL3()
Perform ISO14443-3 Data Exchange with MIFARE Picc.
wOption can be one of:
Alternatively, the following bits can be combined:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | number of received data bytes. |
§ phpalMifare_ExchangeL4()
Perform ISO14443-4 Data Exchange with MIFARE Picc.
wOption can be one of:
Additionally, the following options are also available:
Alternatively to the FIRST/CONT/LAST options, the following bits can be combined:
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | number of received data bytes. |
§ phpalMifare_ExchangePc()
Perform Proximity-Check Data Exchange with MIFARE Picc.
Note: The wOption parameter is currently RFU.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of data to transmit. |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | number of received data bytes. |
§ phpalMifare_ExchangeRaw()
Perform Raw (No CRC, No Parity) Data Exchange with MIFARE Picc.
wOption can be one of:
Alternatively, the following bits can be combined:
In Sam non X configuration, wOption can be combined with the following options to instruct Sam to not do enciphering and/or deciphering.
- #PHHAL_HW_SAMAV2_EXCHANGE_NO_ENCIPHERING_BIT
- #PHHAL_HW_SAMAV2_EXCHANGE_NO_DECIPHERING_BIT
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wOption | Option parameter. |
| [in] | pTxBuffer | Data to transmit. |
| [in] | wTxLength | Length of input data. |
| [in] | bTxLastBits | Number of valid bits of last byte (Tx). |
| [out] | ppRxBuffer | Pointer to received data. |
| [out] | pRxLength | Number of received data bytes including incomplete byte. |
| [out] | pRxLastBits | Number of valid bits of last byte (Rx). |
§ phpalMifare_MfcAuthenticateKeyNo()
Perform MIFARE(R) Authenticate command with Picc using a key number.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bBlockNo | Block-Number on card to authenticate to. |
| [in] | bKeyType | Either PHPAL_MIFARE_KEYA or PHPAL_MIFARE_KEYB |
| [in] | wKeyNo | Key number to be used in authentication. |
| [in] | wKeyVersion | Key version to be used in authentication. |
| [in] | pUid | Serial number of current cascade level; uint8_t[4]. |
§ phpalMifare_MfcAuthenticate()
Perform MIFARE(R) Authenticate command with Picc using a key.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | bBlockNo | Block-Number on card to authenticate to. |
| [in] | bKeyType | Either PHPAL_MIFARE_KEYA or PHPAL_MIFARE_KEYB |
| [in] | pKey | Key to be used in authentication. |
| [in] | pUid | Serial number of current cascade level; uint8_t[4]. |
§ phpalMifare_SetMinFdtPc()
| phStatus_t phpalMifare_SetMinFdtPc |
( |
void * |
pDataParams, |
|
|
uint16_t |
wValue |
|
) |
| |
Perform Setting min FDT for Proximity check.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | wValue | Option parameter. '1' for setting '0' for resetting |