|
NXP NFC Reader Library
v4.040.05.011646
|
Private parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pPalI14443p3aDataParams |
| Pointer to pal parameter structure. More... | |
| uint8_t | abHR [2] |
| Header Rom bytes. More... | |
| uint8_t | abUid [4] |
| UID of selected tag. More... | |
Private parameter structure.
| void* phalT1T_Sw_DataParams_t::pPalI14443p3aDataParams |
Pointer to pal parameter structure.
| uint8_t phalT1T_Sw_DataParams_t::abHR[2] |
Header Rom bytes.
| uint8_t phalT1T_Sw_DataParams_t::abUid[4] |
UID of selected tag.