|
NXP NFC Reader Library
v4.040.05.011646
|
Structure info required for ISO/IEC 14443-4 communication. More...
Data Fields | |
| uint8_t | bFsdi |
| Frame size integer. More... | |
| uint8_t | bCid |
| Card identifier. More... | |
| uint8_t | bNad |
| Node ADdress. More... | |
| uint8_t | bDri |
| Data Rate received by Initiator. More... | |
| uint8_t | bDsi |
| Data Rate send by Initiator. More... | |
| uint8_t * | pAts |
| Holds the answer to select response. More... | |
Structure info required for ISO/IEC 14443-4 communication.
| uint8_t phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::bFsdi |
Frame size integer.
| uint8_t phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::bCid |
Card identifier.
| uint8_t phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::bNad |
Node ADdress.
| uint8_t phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::bDri |
Data Rate received by Initiator.
| uint8_t phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::bDsi |
Data Rate send by Initiator.
| uint8_t* phacDiscLoop_Sw_TypeA_Info::phascDiscLoop_TypeA_I3P4::pAts |
Holds the answer to select response.