|
NXP NFC Reader Library
v4.040.05.011646
|
T3T parameter structure. More...
Data Fields | |
| void * | pAlT3TDataParams |
| Pointer to Felica data parameters. | |
| uint8_t | bRwa |
| Tag read/write access; 1 - Read/Write, 0 - Read Only. | |
| uint8_t | bNbr |
| Number of Blocks that can be read at one time. | |
| uint8_t | bNbw |
| Number of Blocks that can be written at one time. | |
| uint16_t | bNmaxb |
| Maximum number of 'Blocks * 16' available for NDEF data. | |
| uint8_t | bUid [16] |
| UID to address T3T. | |
| uint8_t | bAttributeBlock [16] |
| Contains the attribute block of the Ndef Type 3 tag. | |
T3T parameter structure.