|
NXP NFC Reader Library
v4.040.05.011646
|
Felica parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pHalDataParams |
| Pointer to the parameter structure of the underlying layer. More... | |
| uint8_t | aIDmPMm [PHPAL_FELICA_IDM_LENGTH+PHPAL_FELICA_PMM_LENGTH+PHPAL_FELICA_RD_LENGTH] |
| The Cards Manufacture ID (IDm), Manufacture Parameters (PMm) and Request Data length. More... | |
| uint8_t | bIDmPMmValid |
Whether the stored IDm and PMm are valid (1) or not (0). More... | |
| uint8_t | bLength |
| Current data length, used internally for Exchange function. More... | |
| uint8_t | bRequestCode |
| Request code (RC) field of ReqC, default value is '0'. More... | |
| uint8_t | bTotalFrames |
| Holds total number of response frame received. More... | |
| uint8_t | bPreambleLen |
| Preamble length used for reception from tag. More... | |
Felica parameter structure.
| void* phpalFelica_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of the underlying layer.
| uint8_t phpalFelica_Sw_DataParams_t::aIDmPMm[PHPAL_FELICA_IDM_LENGTH+PHPAL_FELICA_PMM_LENGTH+PHPAL_FELICA_RD_LENGTH] |
The Cards Manufacture ID (IDm), Manufacture Parameters (PMm) and Request Data length.
| uint8_t phpalFelica_Sw_DataParams_t::bIDmPMmValid |
Whether the stored IDm and PMm are valid (1) or not (0).
| uint8_t phpalFelica_Sw_DataParams_t::bLength |
Current data length, used internally for Exchange function.
| uint8_t phpalFelica_Sw_DataParams_t::bRequestCode |
Request code (RC) field of ReqC, default value is '0'.
| uint8_t phpalFelica_Sw_DataParams_t::bTotalFrames |
Holds total number of response frame received.
Value ranges from 1 to N
Ignored if phpalFelica_ReqC function called with slot number PHPAL_FELICA_NUMSLOTS_1.
| uint8_t phpalFelica_Sw_DataParams_t::bPreambleLen |
Preamble length used for reception from tag.