|
NXP NFC Reader Library
v4.040.05.011646
|
Software PAL-ISO14443P3B parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pHalDataParams |
| Pointer to the parameter structure of the underlying layer. More... | |
| uint8_t | bExtAtqb |
| Stores whether last request used extended ATQB. More... | |
| uint8_t | pPupi [4] |
| Array holding the activated PUPI. More... | |
| uint8_t | bPupiValid |
Whether the stored Pupi is valid (1) or not (0). More... | |
| uint8_t | bCidSupported |
| Cid Support indicator; Unequal '0' if supported. More... | |
| uint8_t | bNadSupported |
| Nad Support indicator; Unequal '0' if supported. More... | |
| uint8_t | bCid |
| Card Identifier; Ignored if bCidSupported is equal '0'. More... | |
| uint8_t | bFwi |
| Frame Waiting Integer. More... | |
| uint8_t | bFsci |
| PICC Frame Size Integer; 0-8;. | |
| uint8_t | bFsdi |
| (Current) PCD Frame Size Integer; 0-8; | |
| uint8_t | bDri |
| (Current) Divisor Receive (PCD to PICC) Integer; 0-3; | |
| uint8_t | bDsi |
| (Current) Divisor Send (PICC to PCD) Integer; 0-3; | |
| uint8_t | bAttribParam1 |
| Param1 parameter for attrib command. More... | |
| uint8_t * | pHigherLayerInf |
| Pointer to higher layer information buffer. More... | |
| uint16_t | wHigherLayerInfLen |
| Length higher layer information. More... | |
| uint8_t * | pHigherLayerResp |
| Pointer to higher layer response buffer. More... | |
| uint16_t | wHigherLayerRespSize |
| Size of higher layer response buffer. More... | |
| uint16_t | wHigherLayerRespLen |
| Length of higher layer response. More... | |
| uint8_t | bOpeMode |
| Operation mode. More... | |
| uint8_t | bPollCmd |
| Used to differentiate which command to send REQA or WakeUpA command for polling. | |
| uint8_t | bRetryCount |
| Retry count for ATTRIB command as per NFC Digital Protocol Version 1.1 For mode RD_LIB_MODE_EMVCO retry count should be 1. More... | |
Software PAL-ISO14443P3B parameter structure.
| void* phpalI14443p3b_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of the underlying layer.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bExtAtqb |
Stores whether last request used extended ATQB.
| uint8_t phpalI14443p3b_Sw_DataParams_t::pPupi[4] |
Array holding the activated PUPI.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bPupiValid |
Whether the stored Pupi is valid (1) or not (0).
| uint8_t phpalI14443p3b_Sw_DataParams_t::bCidSupported |
Cid Support indicator; Unequal '0' if supported.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bNadSupported |
Nad Support indicator; Unequal '0' if supported.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bCid |
Card Identifier; Ignored if bCidSupported is equal '0'.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bFwi |
Frame Waiting Integer.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bAttribParam1 |
Param1 parameter for attrib command.
| uint8_t* phpalI14443p3b_Sw_DataParams_t::pHigherLayerInf |
Pointer to higher layer information buffer.
| uint16_t phpalI14443p3b_Sw_DataParams_t::wHigherLayerInfLen |
Length higher layer information.
| uint8_t* phpalI14443p3b_Sw_DataParams_t::pHigherLayerResp |
Pointer to higher layer response buffer.
| uint16_t phpalI14443p3b_Sw_DataParams_t::wHigherLayerRespSize |
Size of higher layer response buffer.
| uint16_t phpalI14443p3b_Sw_DataParams_t::wHigherLayerRespLen |
Length of higher layer response.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bOpeMode |
Operation mode.
One of NFC, EMVCo, ISO.
| uint8_t phpalI14443p3b_Sw_DataParams_t::bRetryCount |
Retry count for ATTRIB command as per NFC Digital Protocol Version 1.1
For mode RD_LIB_MODE_EMVCO retry count should be 1.