These Components implement the Platform HOST porting abstraction layer.
More...
|
| enum | phPlatform_Port_Host_config {
PHPLATFORM_PORT_PIN_RESET = 0x1U,
PHPLATFORM_PORT_PIN_IRQ = 0x2U,
PHPLATFORM_PORT_PIN_SPI = 0x3U,
PHPLATFORM_PORT_PIN_I2C = 0x4U,
PHPLATFORM_PORT_PIN_BUSY = 0x5U,
PHPLATFORM_PORT_PIN_DWL = 0x6U,
PHPLATFORM_PORT_PIN_IFSEL0 = 0x7U,
PHPLATFORM_PORT_PIN_IFSEL1 = 0x8U,
PHPLATFORM_PORT_PIN_AD0 = 0x9U,
PHPLATFORM_PORT_PIN_AD1 = 0xAU,
PHPLATFORM_PORT_PIN_AD2 = 0xBU
} |
| | Functional Abstraction of various PINs between Host and Frontend. More...
|
| |
| enum | phPlatform_Port_Host_Interrupt { PHPLATFORM_PORT_INT_DISABLED = 0x0U,
PHPLATFORM_PORT_INT_RISING_EDGE = 0x1U,
PHPLATFORM_PORT_INT_FALLING_EDGE = 0x2U
} |
| | Configures the interrupt generation condition. More...
|
| |
|
| phStatus_t | phPlatform_Port_Host_SetPinConfig (phPlatform_Port_Host_config_t bConfig) |
| | This API is used to configure and initialize the HOST pins (ex : Reset, IRQ, AD etc) which are connected to respective front-ends. More...
|
| |
| void | phPlatform_Port_Host_SetPinValue (phPlatform_Port_Host_config_t bConfig, uint8_t bVal) |
| | This API is used to set the state of HOST pin. More...
|
| |
| bool | phPlatform_Port_Host_GetPinValue (phPlatform_Port_Host_config_t bConfig) |
| | Get a GPIO pin state via the GPIO byte register. More...
|
| |
| void | phPlatform_Port_Host_ClearInt (void) |
| | Clear interrupt status. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Init (void) |
| | Initialize the Host Timer module. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Create (uint32_t dwUnits, uint8_t bTimerId, void **ppTimerHandle) |
| | Allocates a free Host timer. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Configure (void *pTimerHandle, uint32_t dwUnits, uint32_t dwTimePeriod) |
| | This API configures the acquired timer with timeout duration. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Start (void *pTimerHandle, uint16_t wOption) |
| | Start the Host timer, upon timer expire phPlatform_Timer_IsrHandler API will be called with timer ID. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_GetElapsedDelay (void *pTimerHandle, uint32_t dwUnits, uint32_t *pdwGetElapsedDelay) |
| | Get Elapsed Delay from host timer which is created and started before calling this API. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Stop (void *pTimerHandle) |
| | Stop the host timer. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Reset (void *pTimerHandle) |
| | Reset the host timer. More...
|
| |
| phStatus_t | phPlatform_Port_Host_HwTimer_Delete (void *pTimerHandle) |
| | Delete the host timer. More...
|
| |
| void | phPlatform_Port_Host_HwTimer_DeInit (void) |
| | DeInitializes the Timer component. More...
|
| |
These Components implement the Platform HOST porting abstraction layer.
These API provide easy to port NfcRdLib on different Host platform.
§ phPlatform_Port_Host_config
Functional Abstraction of various PINs between Host and Frontend.
| Enumerator |
|---|
| PHPLATFORM_PORT_PIN_RESET | Reset the Frontend.
|
| PHPLATFORM_PORT_PIN_IRQ | Interrupt from the Frontend to Host.
|
| PHPLATFORM_PORT_PIN_SPI | SPI Pins of the Host.
|
| PHPLATFORM_PORT_PIN_I2C | I2C Pins of the Host.
|
| PHPLATFORM_PORT_PIN_BUSY | Frontend's Busy Status, if Applicable.
|
| PHPLATFORM_PORT_PIN_DWL | Assert Download mode of Frontend, if Applicable.
|
| PHPLATFORM_PORT_PIN_IFSEL0 | IFSEL0 of the Frontend, if Applicable.
|
| PHPLATFORM_PORT_PIN_IFSEL1 | IFSEL1 of the Frontend, if Applicable.
|
| PHPLATFORM_PORT_PIN_AD0 | Address Select Pin of Frontend, if Applicable.
|
| PHPLATFORM_PORT_PIN_AD1 | Address Select Pin of Frontend, if Applicable.
|
| PHPLATFORM_PORT_PIN_AD2 | Address Select Pin of Frontend, if Applicable.
|
§ phPlatform_Port_Host_Interrupt
Configures the interrupt generation condition.
| Enumerator |
|---|
| PHPLATFORM_PORT_INT_DISABLED | Interrupt request is disabled.
|
| PHPLATFORM_PORT_INT_RISING_EDGE | Interrupt on rising edge.
|
| PHPLATFORM_PORT_INT_FALLING_EDGE | Interrupt on falling edge.
|
§ phPlatform_Port_Host_SetPinConfig()
This API is used to configure and initialize the HOST pins (ex : Reset, IRQ, AD etc) which are connected to respective front-ends.
Port and Pin number are abstracted in specific Platform configuration header file. For any new combination of Host and Front-end, new configuration header file can be added to easy the porting.
- Parameters
-
| [in] | bConfig | : HOST pin that needs to be configured. |
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_SetPinValue()
This API is used to set the state of HOST pin.
Port and Pin number are abstracted in specific Platform configuration header file. For any new combination of Host and Front-end, new configuration header file can be added to easy the porting.
- Parameters
-
| [in] | bConfig | : HOST pin needs to be set. |
| [in] | bVal | : PH_PLATFORM_SET_HIGH for high, PH_PLATFORM_SET_LOW for low. |
- Returns
- Nothing
§ phPlatform_Port_Host_GetPinValue()
Get a GPIO pin state via the GPIO byte register.
Port and Pin number are abstracted in specific Platform configuration header file. For any new combination of Host and Front-end, new configuration header file can be added to easy the porting.
- Parameters
-
| [in] | bConfig | : Get the state of HOST pin. |
- Returns
- Status of the API
-
true if HOST pin is in high state else false.
§ phPlatform_Port_Host_ClearInt()
| void phPlatform_Port_Host_ClearInt |
( |
void |
| ) |
|
Clear interrupt status.
Port and Pin number are abstracted in specific Platform configuration header file. For any new combination of Host and Front-end, new configuration header file can be added to easy the porting.
- Returns
- Nothing
§ phPlatform_Port_Host_HwTimer_Init()
| phStatus_t phPlatform_Port_Host_HwTimer_Init |
( |
void |
| ) |
|
Initialize the Host Timer module.
- Note
- This API will be called by phPlatform_Timer_Init API.
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Create()
| phStatus_t phPlatform_Port_Host_HwTimer_Create |
( |
uint32_t |
dwUnits, |
|
|
uint8_t |
bTimerId, |
|
|
void ** |
ppTimerHandle |
|
) |
| |
Allocates a free Host timer.
- Note
- This API will be called by phPlatform_Timer_Create API.
- Parameters
-
| [in] | dwUnits | Timer Resolution (e.g. PH_PLATFORM_TIMER_UNIT_S) |
| [in] | bTimerId | Timer Number |
| [out] | ppTimerHandle | Handle to the timer in case of success else NULL. |
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Configure()
| phStatus_t phPlatform_Port_Host_HwTimer_Configure |
( |
void * |
pTimerHandle, |
|
|
uint32_t |
dwUnits, |
|
|
uint32_t |
dwTimePeriod |
|
) |
| |
This API configures the acquired timer with timeout duration.
- Note
- This API will be called by phPlatform_Timer_Configure API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Start()
| phStatus_t phPlatform_Port_Host_HwTimer_Start |
( |
void * |
pTimerHandle, |
|
|
uint16_t |
wOption |
|
) |
| |
Start the Host timer, upon timer expire phPlatform_Timer_IsrHandler API will be called with timer ID.
- Note
- This API will be called by phPlatform_Timer_Start API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_GetElapsedDelay()
| phStatus_t phPlatform_Port_Host_HwTimer_GetElapsedDelay |
( |
void * |
pTimerHandle, |
|
|
uint32_t |
dwUnits, |
|
|
uint32_t * |
pdwGetElapsedDelay |
|
) |
| |
Get Elapsed Delay from host timer which is created and started before calling this API.
- Note
- This API will be called by phPlatform_Timer_GetElapsedDelay API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Stop()
| phStatus_t phPlatform_Port_Host_HwTimer_Stop |
( |
void * |
pTimerHandle | ) |
|
Stop the host timer.
- Note
- This API will be called by phPlatform_Timer_Stop API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Reset()
| phStatus_t phPlatform_Port_Host_HwTimer_Reset |
( |
void * |
pTimerHandle | ) |
|
Reset the host timer.
- Note
- This API will be called by phPlatform_Timer_Reset API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_Delete()
| phStatus_t phPlatform_Port_Host_HwTimer_Delete |
( |
void * |
pTimerHandle | ) |
|
Delete the host timer.
- Note
- This API will be called by phPlatform_Timer_Delete API.
- Parameters
-
- Returns
- Status of the API
- Return values
-
§ phPlatform_Port_Host_HwTimer_DeInit()
| void phPlatform_Port_Host_HwTimer_DeInit |
( |
void |
| ) |
|
DeInitializes the Timer component.
- Note
- This API will be called by phPlatform_Timer_DeInit API.
- Returns
- Status of the API
- Return values
-