|
NXP NFC Reader Library
v4.040.05.011646
|
Software PAL-ISO14443P3A parameter structure. More...
Data Fields | |
| uint16_t | wId |
| Layer ID for this component, NEVER MODIFY! | |
| void * | pHalDataParams |
| Pointer to the parameter structure of the underlying layer. More... | |
| uint8_t | abUid [10] |
| Array holding the activated UID. More... | |
| uint8_t | bUidLength |
Length of UID stored in abUid. More... | |
| uint8_t | bUidComplete |
Whether the UID is complete (1) or not (0). More... | |
| uint8_t | bOpeMode |
| Operation mode. More... | |
| uint8_t | bPollCmd |
| Used to differentiate which command to send REQA or WakeUpA command for polling. | |
Software PAL-ISO14443P3A parameter structure.
| void* phpalI14443p3a_Sw_DataParams_t::pHalDataParams |
Pointer to the parameter structure of the underlying layer.
| uint8_t phpalI14443p3a_Sw_DataParams_t::abUid[10] |
Array holding the activated UID.
| uint8_t phpalI14443p3a_Sw_DataParams_t::bUidLength |
Length of UID stored in abUid.
| uint8_t phpalI14443p3a_Sw_DataParams_t::bUidComplete |
Whether the UID is complete (1) or not (0).
| uint8_t phpalI14443p3a_Sw_DataParams_t::bOpeMode |
Operation mode.
One of NFC, EMVCo, ISO.