|
NXP NFC Reader Library
v4.040.05.011646
|
These Components implement the Type 1 Tag commands. More...
|
Modules | |
| Component : Software | |
Functions | |
| phStatus_t | phalT1T_ReadUID (void *pDataParams, uint8_t *pUid, uint16_t *pLength) |
| Perform Jewel/Topaz Read UID command. More... | |
| phStatus_t | phalT1T_ReadAll (void *pDataParams, uint8_t *pUid, uint8_t **pData, uint16_t *pLength) |
| Perform Jewel/Topaz Read All command. More... | |
| phStatus_t | phalT1T_ReadByte (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t *pData, uint16_t *pLength) |
| Perform Jewel/Topaz Read Byte command. More... | |
| phStatus_t | phalT1T_WriteEraseByte (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t bTxData, uint8_t *pRxData, uint16_t *pLength) |
| Perform Jewel/Topaz Write Erase Byte command. More... | |
| phStatus_t | phalT1T_WriteNoEraseByte (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t bTxData, uint8_t *pRxData, uint16_t *pLength) |
| Perform Jewel/Topaz Write No Erase Byte command. More... | |
| phStatus_t | phalT1T_ReadSegment (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t **pData, uint16_t *pLength) |
| Perform Jewel/Topaz Read Segment command. More... | |
| phStatus_t | phalT1T_ReadBlock (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t *pData, uint16_t *pLength) |
| Perform Jewel/Topaz Read Block command. More... | |
| phStatus_t | phalT1T_WriteEraseBlock (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t *pTxData, uint8_t *pRxData, uint16_t *pLength) |
| Perform Jewel/Topaz Write Erase Block command. More... | |
| phStatus_t | phalT1T_WriteNoEraseBlock (void *pDataParams, uint8_t *pUid, uint8_t bAddress, uint8_t *pTxData, uint8_t *pRxData, uint16_t *pLength) |
| Perform Jewel/Topaz Write No Erase Block command. More... | |
These Components implement the Type 1 Tag commands.
Perform Jewel/Topaz Read UID command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [out] | pUid | Uid of Card, 4 bytes. |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_ReadAll | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t ** | pData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Read All command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [out] | pData | pData containing 122 data bytes returned from the PICC. [HR0][HR1][Data from blocks 0 to 0xE] |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_ReadByte | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t * | pData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Read Byte command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a byte on Picc to read from. |
| [out] | pData | pData containing one data byte returned from the PICC. |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_WriteEraseByte | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t | bTxData, | ||
| uint8_t * | pRxData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Write Erase Byte command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid, 4 bytes. |
| [in] | bAddress | Address of a byte on Picc to write to. |
| [in] | bTxData | pData containing data to be written to the Picc. |
| [out] | pRxData | pRxData containing 2 data bytes returned from the Picc. [ADD][Byte] |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_WriteNoEraseByte | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t | bTxData, | ||
| uint8_t * | pRxData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Write No Erase Byte command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a byte on PICC to write to. |
| [in] | bTxData | pData containing data to be written to the PICC. |
| [out] | pRxData | pRxData containing 2 data bytes returned from the PICC. |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_ReadSegment | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t ** | pData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Read Segment command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a segment on Picc to read from. |
| [out] | pData | pData containing 128 bytes of data returned from the PICC. |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_ReadBlock | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t * | pData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Read Block command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a block on Picc to read from. |
| [out] | pData | pData containing 8 data bytes returned from the Picc. At least 8 bytes must be provided by the user |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_WriteEraseBlock | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t * | pTxData, | ||
| uint8_t * | pRxData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Write Erase Block command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a block on Picc to write to. |
| [in] | pTxData | pTxData containing data to be written to the Picc. |
| [out] | pRxData | pRxData containing 8 data bytes returned from the Picc. At least 8 bytes buffer must be provided by the user. |
| [out] | pLength | Number of received data bytes. |
| phStatus_t phalT1T_WriteNoEraseBlock | ( | void * | pDataParams, |
| uint8_t * | pUid, | ||
| uint8_t | bAddress, | ||
| uint8_t * | pTxData, | ||
| uint8_t * | pRxData, | ||
| uint16_t * | pLength | ||
| ) |
Perform Jewel/Topaz Write No Erase Block command.
| PH_ERR_SUCCESS | Operation successful. |
| PH_ERR_PROTOCOL_ERROR | Invalid response received. |
| PH_ERR_FRAMING_ERROR | Bcc invalid. |
| Other | Depending on implementation and underlying component. |
| [in] | pDataParams | Pointer to this layer's parameter structure. |
| [in] | pUid | Known Uid , 4 bytes. |
| [in] | bAddress | Address of a block on Picc to write to. |
| [in] | pTxData | pTxData containing data to be written to the Picc. |
| [out] | pRxData | pRxData containing 8 data bytes returned from the Picc. At least 8 bytes buffer must be provided by the user. |
| [out] | pLength | Number of received data bytes. |